Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help with Making a RPM tacho Shift Light circuit open a 12v Relay
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 341 subscribers
  • Views 5269 views
  • Users 0 members are here
  • ask_an_expert
  • led
  • rpm
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help with Making a RPM tacho Shift Light circuit open a 12v Relay

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone, i have a few adjustable Tachometer Shift light Circuits that i want to use to turn on a relay when the led turns on.

The way they are set up now:
You can adjust the desired rpm Shift light value with a pot then when that rpm is reached the led turns on.

 

My problem is tracing it back to the IC or to the nearest transistor.
I'm trying to turn on a 12v relay when the desired rpm is reached.

 

So there are 2 ways i am thinking of doing this...


1: is to use a transistor to allow a higher current to run through the relay's solenoid to then allow me to run a separate 12v circuit to turn on more than 1 led light. i cant find where to run the transistor off or which pin on the ic is actually the "remote wire" for the led.


2: If i can't use a transistor is it possible to use a phototransistor and just use the built in led to then turn on a second circuit with a phototransitor linked to the relay's solenoid>


Any help would be greatly appreciated please find some pictures attached of the circuitimage







image

  • Sign in to reply
  • Cancel
Parents
  • mudz
    0 mudz over 11 years ago

    Greetings,
    I have figured out little info about the circuit check the following images.

    image

    If I am guessing it right, looking at the led the internal right side(near capacitor) is larger which is negative part of led. So that pin is connected with resistor which is connected with 5th pin of IC. Now, the positive pin is connected with three resistor and the 1st pin of IC which I guess is the input to the led(this pins voltage is driving the led). Also if you look at the capacitor, you will find that the capacitor's positive pin is connected to the 1st pin of IC which also confirms that it is the input to the led. This part, I guess, you already knew.
    Consider this circuit :

    image

    As you have mentioned that even when LED is off it is getting some voltage, I suggest you to add a Diode which will give a voltage drop of around ~0.7v (as shown in image). If again transistor stays on try adding another diode in series, total voltage drop will be around ~1.4v. I guess it will do the job. Don't forget to add resistor in between v+ and collector of transistor. For transistor consider TIP120, TIP31 ...
    If this does not works, Please mention few things like:
    1. IC number/Name
    2. voltage across led when it is off.
    3. Few more Images(without reflection, shadow).
    4. Voltages across red & black wire, red & green wire.
    5. Mention Circuit driving voltage(as I can see 1 watt or 2 watt resistors)

     

    Good Luck image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to mudz

    In the circuit you depict here I would have guessed the orange line is the positive power rail and therefore would not change much, the green line through the resistor I would have guessed to be the control line for the LED and the resistor between it and the pin on the IC is to limit the current through the LED.

     

    The additional transistor in this case would not work as the supply rail for the chip is unlightly to be 12V, the transistor would have to be PNP and turn on then the base is pulled low, if it is NPN then the base would have to exced 12V in order to deliver 12V to the relay, if the chip is a 5V device then you will get about 4V only to the relay (Standard emitter follow). You indicate the transistor is NPN based on the description and the direction of the included DIODE. You have no current limiting in the circuit to the base so this could be an issue

     

    I would suggest putting the transistor on the other side of the relay (12V to the relay, relay to the collector of the transistor and the emitter of the transistor to ground. put a few hundred ohms resistor between the base and the control signal

     

    I would actually suggest measuring what is happening on the chip where you indicate the resistor is connected, this would be pin 5 by convention with the assumption the dot on the chip is pin 1 (Normal convention)

     

    this pin I would expect to go from high volts when the LED is off, to close to ground when the LED is on, if this is the case you can use a NPN transistor to hold of a PNP transistor that in turn drives the relay (This provides a level of isolation from the 12 V to the chip which can not be avoided with only one transistor

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to mudz

    In the circuit you depict here I would have guessed the orange line is the positive power rail and therefore would not change much, the green line through the resistor I would have guessed to be the control line for the LED and the resistor between it and the pin on the IC is to limit the current through the LED.

     

    The additional transistor in this case would not work as the supply rail for the chip is unlightly to be 12V, the transistor would have to be PNP and turn on then the base is pulled low, if it is NPN then the base would have to exced 12V in order to deliver 12V to the relay, if the chip is a 5V device then you will get about 4V only to the relay (Standard emitter follow). You indicate the transistor is NPN based on the description and the direction of the included DIODE. You have no current limiting in the circuit to the base so this could be an issue

     

    I would suggest putting the transistor on the other side of the relay (12V to the relay, relay to the collector of the transistor and the emitter of the transistor to ground. put a few hundred ohms resistor between the base and the control signal

     

    I would actually suggest measuring what is happening on the chip where you indicate the resistor is connected, this would be pin 5 by convention with the assumption the dot on the chip is pin 1 (Normal convention)

     

    this pin I would expect to go from high volts when the LED is off, to close to ground when the LED is on, if this is the case you can use a NPN transistor to hold of a PNP transistor that in turn drives the relay (This provides a level of isolation from the 12 V to the chip which can not be avoided with only one transistor

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mudz
    0 mudz over 11 years ago in reply to Robert Peter Oakes
    In the circuit you depict here I would have guessed the orange line is the positive power rail and therefore would not change much,

    You might be right because this is another way that this led is powered, but conventional way to power a led is by giving voltage to the positive pin while keeping negative pin at ground. Your case is true too.

    the green line through the resistor I would have guessed to be the control line for the LED and the resistor between it and the pin on the IC is to limit the current through the LED.

    This might be also true, but current limiting resistor can be connected both ways i.e on positive pin as well as on negative pin of led to limit the current.

    The additional transistor in this case would not work as the supply rail for the chip is unlightly to be 12V, the transistor would have to be PNP and turn on then the base is pulled low, if it is NPN then the base would have to exced 12V in order to deliver 12V to the relay, if the chip is a 5V device then you will get about 4V only to the relay (Standard emitter follow). You indicate the transistor is NPN based on the description and the direction of the included DIODE. You have no current limiting in the circuit to the base so this could be an issue

    I have mentioned that the transistor is supplied with v+ but i forgot to mention it should be 12v as we can drive the 12v load directly, but this is the option 1(without relay). Transistors i have mentioned are of 3A/5A rating.

    Current limiting resistor can be added to the base, The idea was to get the circuit up early and then do the minor corrections.

    I would suggest putting the transistor on the other side of the relay (12V to the relay, relay to the collector of the transistor and the emitter of the transistor to ground. put a few hundred ohms resistor between the base and the control signal

    Again another case and true but whenever there is a relay in the circuit I prefer to go with optocoupler/optoisolator. So this circuit can be used for this case too. You can use system supply at v+ and the where I have connected load that can be used to drive optocoupler which in turns drive the relay(connected with external 12v supply).