Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help with Making a RPM tacho Shift Light circuit open a 12v Relay
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 341 subscribers
  • Views 5323 views
  • Users 0 members are here
  • ask_an_expert
  • led
  • rpm
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help with Making a RPM tacho Shift Light circuit open a 12v Relay

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone, i have a few adjustable Tachometer Shift light Circuits that i want to use to turn on a relay when the led turns on.

The way they are set up now:
You can adjust the desired rpm Shift light value with a pot then when that rpm is reached the led turns on.

 

My problem is tracing it back to the IC or to the nearest transistor.
I'm trying to turn on a 12v relay when the desired rpm is reached.

 

So there are 2 ways i am thinking of doing this...


1: is to use a transistor to allow a higher current to run through the relay's solenoid to then allow me to run a separate 12v circuit to turn on more than 1 led light. i cant find where to run the transistor off or which pin on the ic is actually the "remote wire" for the led.


2: If i can't use a transistor is it possible to use a phototransistor and just use the built in led to then turn on a second circuit with a phototransitor linked to the relay's solenoid>


Any help would be greatly appreciated please find some pictures attached of the circuitimage







image

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to supper_slash

    Ah yes so where i have the +ve leg on the led coming off the relay i need to put the cathode on the diode and bridge it straight across the relay solenoid in parallel if that makes sense?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to e14 Contributor

    you got it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to supper_slash

    Although i cant remember if i have the relay coming off the negative pin on the led or the positive... i have a feeling it may be switched negative and constant pos.... cant remember in that case would i flip the diode around?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to e14 Contributor

    nope. here is what happens in a relay, that requires the diode.:

     

    Since an inductor (the relay coil) cannot change it's current instantly, the fly-back diode provides a path for the current when the coil is switched off. Otherwise, a voltage spike will occur causing arcing on switch contacts or possibly destroying switching transistors.


    But, if you place the diode the wrong way, it will act like a short, and there will not be enough voltage to the relay to activate it.


    Done properly, When the current through a coil is switched off, the coil (being an inductor) will try to maintain the current. When there is no path for this current the voltage across the coil will increase rapidly, and the current will find a path, right through the isolation of a chip or transistor, destroying that component. The diode provides a path for this current, so the energy stored in the coil can be dissipated safely.



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to supper_slash

    Yes i understand that but what i mean is that the switch (SW1) in your diagram is actually negative on mine from memory (will clarify later) so in that case my positive lead is constant so then if i didnt switch the diode around wouldnt it just short and create high current to run and not activate the relay?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    DIODE will always point to the positive supply side, no matter where you place the switch, it is to protect against back EMF when the switch opens as stated

     

    the switch does not dictate the current flow or the polarity of the supply, thats all about how the battery is wired up in the circuit

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Yeah thats what i thought so If mine is a switched negative then i need to face the diode in the opposing way to the diagram. I will draw up a bit of a circuit later to confirm and also see if mine is switched negative like i think cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago

    The diode will point to the positive, no matter where the switch is.

    (cathode, on the positive NO MATTER WHAT.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Sharing what the numbers are on the chip (Part number of the Chip) would help immensely

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<