Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How can I DIY 230VAC E27 lamp from a 41W 35V 1,17A COB LED? I can't find parts for it.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 9 answers
  • Subscribers 339 subscribers
  • Views 2890 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How can I DIY 230VAC E27 lamp from a 41W 35V 1,17A COB LED? I can't find parts for it.

gyulánk
gyulánk over 5 years ago

BXRC-30H4000-C-73

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago in reply to dougw +5 suggested
    That's a really nice module. I used MeanWell constant voltage modules (LPF) that for home lighting in my office. The voltage is dead-accurate (the one I tested was within 0.05V!) for long LED life, and…
  • robogary
    robogary over 5 years ago +5 suggested
    I have dissected a couple LED bulbs. They have a buck switching power supply in the base to convert 120 V or 230V to DC. The ones I checked are 5V.dc You can get a buck switching power supply with an adjustable…
  • jw0752
    jw0752 over 5 years ago in reply to gyulánk +5 suggested
    Hi Gyula, Everyone here is on their own time and giving you the best ideas that they have to offer. Sometimes an idea even a bad one can help a person to look at a problem from a new perspective. It is…
Parents
  • robogary
    0 robogary over 5 years ago

    I have dissected a couple LED bulbs.

    They have a buck switching power supply in the base to convert 120 V or 230V to DC.

    The ones I checked are 5V.dc

    You can get a buck switching power supply with an adjustable voltage and current output, adjust voltage and current. Commercial light bulbs buck power supplies are preset to volts and amps when they are designed.

     

    I have a LED kitchen light that has 2 banks of ~ 100 smaller LEDs around the edge. The buck power supply inside was set higher, it was failed so I dont have the DC voltage output available to share.

     

    For another example I took 115 VAC  LED floodlights that had a failed motion detector, and removed the LED floodlights.

    I installed them on a robot that used a 12V battery.  The LEDs turned on at about 1.6 V   and varied brightness based on the current limit adjust.

    The LEDs were rated for 2A, I adjusted the buck supply output voltage to .25V above turn on voltage, and current limit to 1 A  because the lights got hot to touch at higher current levels. 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • robogary
    0 robogary over 5 years ago

    I have dissected a couple LED bulbs.

    They have a buck switching power supply in the base to convert 120 V or 230V to DC.

    The ones I checked are 5V.dc

    You can get a buck switching power supply with an adjustable voltage and current output, adjust voltage and current. Commercial light bulbs buck power supplies are preset to volts and amps when they are designed.

     

    I have a LED kitchen light that has 2 banks of ~ 100 smaller LEDs around the edge. The buck power supply inside was set higher, it was failed so I dont have the DC voltage output available to share.

     

    For another example I took 115 VAC  LED floodlights that had a failed motion detector, and removed the LED floodlights.

    I installed them on a robot that used a 12V battery.  The LEDs turned on at about 1.6 V   and varied brightness based on the current limit adjust.

    The LEDs were rated for 2A, I adjusted the buck supply output voltage to .25V above turn on voltage, and current limit to 1 A  because the lights got hot to touch at higher current levels. 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer