Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Rise time measurements counter/timer vs Oscope?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 303 subscribers
  • Views 2546 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Rise time measurements counter/timer vs Oscope?

dc2daylight
dc2daylight over 3 years ago

Hi,

I am trying to measure the rise time of a 10 MHz square wave with a Keysight 53220A universal counter.  The source has a specified rise time at 10 MHz of <3 nS.  This is confirmed to be about 3 nS when measured on a scope.

However, when measured on the counter I am seeing a rise time of around 40 nS (10-90%).

I suspect that either I am not measuring the same thing or I may be setting up the measurement incorrectly on the counter.  (the user manual has very little on this).

Any help or suggestions would be appreciated.

Thanks,

Mark

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +3
    The 53220A isn't a time-stamping or zero-dead-time counter. So there is a minimum delay needed between start and stop triggers on time interval measurements. The rise time of a fast edge wouldn't satisfy…
  • Jan Cumps
    Jan Cumps over 3 years ago +2
    Is the 10/90% on the counter rise time or duty cycle? A sking because the UOM is %, and that's more common for the duty cycle. 2nd check: input impedance of scope vs counter. Are they both 50 Ohm, both…
  • dc2daylight
    dc2daylight over 3 years ago in reply to Jan Cumps +1
    Ok, yes, It's a time interval parameter, not a duty cycle. My understanding is the 10-90% is the time interval it takes the signal to go from 10% to it's final value of 90% of it's final value. It…
Parents
  • shabaz
    0 shabaz over 3 years ago

    I suppose one other thing to rule in or out, could be, has it ever worked, or is it in some lab and no-one knows if it works. I only say this because people do end up damaging anything RF related, I've seen several destroyed spectrum analyzers, and my counter came destroyed too, fortunately, that was an easy fix. I think people like plugging in transmitters.

    If there's another way to verify it works (on all channels if it is a multi-channel instrument, or run diagnostics) could be good to confirm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dc2daylight
    0 dc2daylight over 3 years ago in reply to shabaz

    So, both inputs are behaving similarly.  Instrument passes all self tests and has no other problems.

    Interestingly,  I tried it again with a sine wave and it seems to work perfectly and confirms results seen on the oscilloscope. 

    I tested up to 140 MHz and it is +/- 0.2 nS . 

    Makes me wonder if the square wave harmonics are culpable. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dc2daylight
    0 dc2daylight over 3 years ago in reply to shabaz

    So, both inputs are behaving similarly.  Instrument passes all self tests and has no other problems.

    Interestingly,  I tried it again with a sine wave and it seems to work perfectly and confirms results seen on the oscilloscope. 

    I tested up to 140 MHz and it is +/- 0.2 nS . 

    Makes me wonder if the square wave harmonics are culpable.