Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How do you start up an untested circuit board?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 337 subscribers
  • Views 10149 views
  • Users 0 members are here
  • testing
  • start-up
  • circuit board
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How do you start up an untested circuit board?

fmilburn
fmilburn over 4 years ago

I've been known to throw a circuit together, apply power to it, and fry something.  Or the circuit just doesn't work and the problem could be anywhere in that mess of wiring.  But I used to work on complex and potentially hazardous projects where we couldn't afford those types of mistakes. There were mechanical, electrical, civil, chemical processing, and instrumentation disciplines, and towards the middle of the design specialists in commissioning and start-up were brought in.

I recently sent out a PCB design for manufacture without prototyping it first.  The schematic is shown below but it is just an example.  My question is more general to starting up any untested circuits.

Schematic

Time for me to get my act together.  I put together a plan with the following approach:

  • Break the circuit into logical sections that can be tested sequentially
  • Describe the test plan for each section with the expected outcome
  • Solder it up a section at a time and test the section before moving on

The actual plan used is shown below.

Commissioning and Startup Plan

One lesson from this was that the test plan should have been made before the PCB was sent out which would have allowed for dedicated test points.  Not shown in the plan (but they should have been) are the bench power over-voltage and over-current settings.

Fortunately, this board went together and started up without a problem but it got me thinking.  What did I leave out?  What tips do you have for planning and starting up an untested circuit?  Do you know of any good resources on the web?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +5
    For production designs of products which will be small and use 0402 parts I often start with a development or prototype board based on 0603 minimum sizes. I use lots of test points for power and key…
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago +4
    With the small footprints on ICs, one can often measure correct solder joints on digital IOs or generally all pins that have protection diodes built in. With the DMM set to diode forward voltage mode,…
  • fmilburn
    fmilburn over 4 years ago in reply to BigG +3
    I had the same questions on test points, although it isn't clearly stated. How many, where to put them, and what to measure is the main reason I developed the test plan. I did some internet searching before…
  • shabaz
    shabaz over 4 years ago

    Hi Frank,

    Interesting topic : ) A proper test plan for bring-up is an excellent idea, and the table looks very good. It is sometimes very easy to design oneself into a hole, with a board that is not easily testable : ) so thinking it through like this makes a lot of sense.

    Prior to PCB testing, I try (although admittedly not always) to test all the bits I'm unsure of (either real or use a dev-board, or simulate), before creating the PCB, i.e. I end up with a lot of scraps of stripboard/perfboard etc. But I also scavenge the parts off them once the PCBs arrive.
    Sometimes I can't do this, especially recently, where I'm waiting a month or longer for parts to arrive from China, and I sonetimes have to just take the leap, sometimes even just going by measurements of pixels from photos of the parts, to get the dimensioning approximately right. This is only for hobby stuff of course.
    For the PCB, in terms of test points, zero-ohm resistors can also be handy for isolating circuits on a board (in third place to 100k and 10k resistors, they are the next most-used resistor for me. I try not to connect inputs/outputs from subsystems on a circuit board together without a resistor in-between, for allowing the isolation, unless I'm certain the circuit portion will work. For digital circuits, I might use a resistor instead of tying pins high or low, in case something else needs to be patched. I don't always do that, but sometimes it's handy. Also I'll sometimes add a resistor in-line, it is usually benign (might help with matching impedances a bit occasionally) but saves too much damage if things get shorted, or if two outputs are accidentally connected together, e.g. RX/TX lines, since sometimes it's easy to get that wrong in a design. Ferrite bead chips are also handy for isolating power to portions of circuitry on a board too, i.e. there's usually no harm to add that in on supply lines to chips. That way, even if a lot of the board is assembled, it is still possible to power off portions for testing (provided inputs/outputs do not cause an issue), or to current-limit using a resistor.
    It is also good to stick a polyfuse on each board, especially if it's expensive, I don't do that much on cheap hobby projects, but for the small cost it's worth it for a bit more peace of mind on more expensive boards. With test wires or metal chassis everywhere, it's too easy to accidentally short things, so that bit of extra protection from the polyfuse could help.

    EDIT: Also test code helps : ) It is handy to have debug code, extra print statements with a debug flag, to troubleshoot the code and hardware.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to shabaz

    Hi Shabaz,

    Those are all great suggestions.  I especially like the concept of modeling/testing things beforehand and isolating circuits with zero-ohm resistors.  Can you give an example of a case where you would consider adding a resistor in-line and how you would size it?  I've thought about adding a polyfuse but haven't done that to date.  Ferrite beads are another thing I haven't tried.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago

    The few boards I have built don't give me the experience to provide a detailed test plan.

    A few suggestions are all I have:

    • I measure resistance between the input power terminal before the board is assembled. NO SHORT!
    • I make the same measurement when the board is populated. NO SHORT!
    • I try to power staging for populating the board. If it involves Arduino or Pi, they are not installed on first power-up.
    • In this staging exercise, I look at what I can populate in stages. Establish the power supply, test, then passive components and test, then active and test and finally processor.

    Like I said my experience is limited so is my knowledge.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to colporteur

    Good suggestions, using the multimeter to buzz for shorts is the first thing I do too.  Learned from experience :-)  I mentioned it in the test plan but the other thing I do now is a detailed visual between each stage.  Not only have I inadvertently added shorts, but I've also left pins completely unconnected or poorly soldered and then wondered why it wasn't working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to fmilburn

    I've done something similar except on the final PCB.

    I now print the PCB etching and hand trace the layout against the schematic. It is a mind-numbing task especially after working with the schematic for so long. It really takes a lot of concentration and focus. I save this wonderful task for last to preserve my sanity.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago

    I always build in test points now that can take either a test terminal soldered in - I have around 100 of these that cost a couple of quid from CPC and are reusable - or can take a probe tip and pigtail.  When I was designing my Instrument Control Board I spent a lot of time breadboarding sections first which also allowed me to create some test Arduino code; I then went on to prototyping the power section with a PCB to do a comparison test between various approaches.  That's not as expensive as it sounds: the parts can be desoldered afterwards and reused and the PCB manufacturer is dirt cheap from China.

    That doesn't help for shorts across pins though  I never used to give a second thought about continuity or resistance testing pins on SMD ICs to make sure no shorts across pins existed and a good connection to the pad had been made as a visual inspection is often awkward.  More recently I've wondered about this approach: a multimeter does this by providing a voltage and in some cases that might be more than the IC is designed for.  It's not often clear from the DMM manual what the voltage is.  On the other hand, I don't know if this is ever likely to be a problem, e.g. continuity testing with a 9V DMM signal across an IC designed for 5V.

    For the ICB when I first received the actual boards, I did like Shabaz and measured continuity across points to ensure that there were no shorts where there shouldn't be.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 4 years ago

    Hmm interesting.

    fmilburn said:
    What did I leave out? 

    I suppose this is side question... as in what's best practice for including test points on a PCB... I see shabaz has already touched on this in one of his comments.

    In particular I am curious to understand the following... What size should a test point be? How many to include? Where to place them? What to avoid? What do you measure etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to Andrew J

    That is an interesting concern about measuring continuity where ICs are in place and I've never given it consideration.  Does anyone know the answer to that?  I've not experienced a problem with it to my knowledge.

    The detailed design process and documentation you create for your projects would be helpful in developing a test plan and selecting test points. I'm more apt to do that with software/firmware than hardware.  Maybe that is part of the reason I have problems with even simple circuits at times?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 4 years ago in reply to BigG

    A lot depends on how much space you have. A test point could be a small surface pad or a though hole big enough to fit a DVM probe or it could be an actual component like a wire loop or connector jack. They should be on all power rails, and all signals of interest.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to BigG

    I had the same questions on test points, although it isn't clearly stated.  How many, where to put them, and what to measure is the main reason I developed the test plan.  I did some internet searching before making this post and what I found wasn't that enlightening.

    KiCad has a number of footprints in the library.  A couple of them are shown below.

    Test Point Footprints

    I have tested a few PCBs in the RoadTest program with the loops and really like them for their ease of use.  Farnell / Newark carry them.  For example, there is Buy Now in different colors.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
>