Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How do you start up an untested circuit board?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 337 subscribers
  • Views 10177 views
  • Users 0 members are here
  • testing
  • start-up
  • circuit board
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How do you start up an untested circuit board?

fmilburn
fmilburn over 4 years ago

I've been known to throw a circuit together, apply power to it, and fry something.  Or the circuit just doesn't work and the problem could be anywhere in that mess of wiring.  But I used to work on complex and potentially hazardous projects where we couldn't afford those types of mistakes. There were mechanical, electrical, civil, chemical processing, and instrumentation disciplines, and towards the middle of the design specialists in commissioning and start-up were brought in.

I recently sent out a PCB design for manufacture without prototyping it first.  The schematic is shown below but it is just an example.  My question is more general to starting up any untested circuits.

Schematic

Time for me to get my act together.  I put together a plan with the following approach:

  • Break the circuit into logical sections that can be tested sequentially
  • Describe the test plan for each section with the expected outcome
  • Solder it up a section at a time and test the section before moving on

The actual plan used is shown below.

Commissioning and Startup Plan

One lesson from this was that the test plan should have been made before the PCB was sent out which would have allowed for dedicated test points.  Not shown in the plan (but they should have been) are the bench power over-voltage and over-current settings.

Fortunately, this board went together and started up without a problem but it got me thinking.  What did I leave out?  What tips do you have for planning and starting up an untested circuit?  Do you know of any good resources on the web?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +5
    For production designs of products which will be small and use 0402 parts I often start with a development or prototype board based on 0603 minimum sizes. I use lots of test points for power and key…
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago +4
    With the small footprints on ICs, one can often measure correct solder joints on digital IOs or generally all pins that have protection diodes built in. With the DMM set to diode forward voltage mode,…
  • fmilburn
    fmilburn over 4 years ago in reply to BigG +3
    I had the same questions on test points, although it isn't clearly stated. How many, where to put them, and what to measure is the main reason I developed the test plan. I did some internet searching before…
Parents
  • BigG
    BigG over 4 years ago

    Hmm interesting.

    fmilburn said:
    What did I leave out? 

    I suppose this is side question... as in what's best practice for including test points on a PCB... I see shabaz has already touched on this in one of his comments.

    In particular I am curious to understand the following... What size should a test point be? How many to include? Where to place them? What to avoid? What do you measure etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to BigG

    I had the same questions on test points, although it isn't clearly stated.  How many, where to put them, and what to measure is the main reason I developed the test plan.  I did some internet searching before making this post and what I found wasn't that enlightening.

    KiCad has a number of footprints in the library.  A couple of them are shown below.

    Test Point Footprints

    I have tested a few PCBs in the RoadTest program with the loops and really like them for their ease of use.  Farnell / Newark carry them.  For example, there is Buy Now in different colors.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to fmilburn

    Those are the ones I'm talking about as well.  The link you provide errors for me: incorrect link or not available in your country.  It may be worth posting the full URL.

    I always position them in pairs with one connected to ground and the other to the signal of interest.  The spacing I set as sufficient to allow me to use a probe and pigtail inserted into the loops, useful for minimising loops if checking for, e.g. ripple.  The through holes are sized to take those test points but are also just big enough to take the probe tip of my Siglent probes.  I've also found they are big enough to take a bootlace ferrule which is stopped by the ferrule 'flare' and makes a good connection without soldering.  The advantage is that the probe and pigtail insert into the ferrule and are held in place, even when placed vertically.  Ferrules are also dirt cheap.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to fmilburn

    I had the same questions on test points, although it isn't clearly stated.  How many, where to put them, and what to measure is the main reason I developed the test plan.  I did some internet searching before making this post and what I found wasn't that enlightening.

    KiCad has a number of footprints in the library.  A couple of them are shown below.

    Test Point Footprints

    I have tested a few PCBs in the RoadTest program with the loops and really like them for their ease of use.  Farnell / Newark carry them.  For example, there is Buy Now  in different colors.

    Here is another link if the one above doesn't work for you: TEST-1(BK) - Multicomp - PCB Test Point, Pin, Black (newark.com)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fmilburn
    fmilburn over 4 years ago in reply to fmilburn

    I had the same questions on test points, although it isn't clearly stated.  How many, where to put them, and what to measure is the main reason I developed the test plan.  I did some internet searching before making this post and what I found wasn't that enlightening.

    KiCad has a number of footprints in the library.  A couple of them are shown below.

    Test Point Footprints

    I have tested a few PCBs in the RoadTest program with the loops and really like them for their ease of use.  Farnell / Newark carry them.  For example, there is Buy Now  in different colors.

    Here is another link if the one above doesn't work for you: TEST-1(BK) - Multicomp - PCB Test Point, Pin, Black (newark.com)