Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Miller DX200 welder SEMIKRON SkiiP 33NEC125T2 Power IGBT Module
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 97 replies
  • Subscribers 343 subscribers
  • Views 24663 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Miller DX200 welder SEMIKRON SkiiP 33NEC125T2 Power IGBT Module

mb443
mb443 over 4 years ago

imageThe hot topic for those who owns DX200 welder and willing to participate in re-implementing of the original PowerModule on discrete elements.

This is continuation of the discussion and efforts already put into at other forum:  Miller Boost Circuit Board Assembly NO. 200841

This is a restoration project attempt of reproducing using discreet components an obsolete  power module  which SkiiP 33NEC125T2 no longer produced by SEMIKRON.

DISCLAIMER: This is a high voltage project DANGER. Anyone who joins this experimental project need to be aware of high voltage (up to 1000v) and high currents (up to 100A) which is a high risk and requires to be qualified to work with such circuits and can be done only at your own risk.

  • Sign in to reply
  • Cancel

Top Replies

  • lanuser
    lanuser over 4 years ago in reply to mb443 +1
    I am no longer interested working on this project. Seems to me besides two people nobody else step forward. I have specially missed one pin on Schematic design, after I ask you to double check my work…
  • alvideo
    alvideo over 4 years ago in reply to alvideo +1
    I redraw module inside wiring like original, exept i added for all IGBT gate resistors. In wiring connectors names are like in module picture (see below). ` Here some more wiring outside…
  • lanuser
    lanuser over 4 years ago in reply to mb443

    Images and Design has been moved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lanuser
    lanuser over 4 years ago in reply to mb443

    Also I have check numerus SEMIKRON SKIIP datasheets regarding Vge =15 V standard on all of them.

    I haven't not complete entire reverse PM to RC pinouts. however, as of right now looks like PM controls by ASSY NO. 207822 and not by Boost Board assy No: 200841

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mb443
    mb443 over 4 years ago in reply to lanuser

    Sure, it's good to know on Vge threshold, just one concern, normally they give a range like 4v - 8v.

    As of schematic it's a good start.

    And as of PFC part I'd worry about it last as unit can work if PFC is not even implemented or dead, like instead of 200A you may get 160-180A but it should work as PFC only recovers some lost energy due to inductive reactance small phase shift correction. 

    F.Y.I. below is fragment of the "Vge threshold" that we're looking for from the datasheet you posted above:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lanuser
    lanuser over 4 years ago in reply to mb443

    Let me look at the Semikron SKIIP datasheets.

    Here what I have found:

    NAC vs NAB:

    image

    Seems module has build in Chopper - IGBT ( this information has not been confirmed for PM SkiiP 33 )

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mb443
    mb443 over 4 years ago in reply to lanuser

    The first datasheet shows Vge (th) threshold in the range of 5 to 6.5v w/ average 5.8v and that measurement is done at 6ma in load, typical value of Ic is 250uA, not sure why german company decided to go w/ 6mA, probably it is their standard, but it's Ok.
    As of second datasheet above does not publish Vge threshold at all, so, you can only guess.

    Also, there are 4 generations of those SkiiP Power Modules and all are different as designed at different time,

    So, guessing may get us in trouble. Another parameter is Vce sat - also important as size of the radiator directly depends on the value of voltage  drop on collector-emitter at max load let say 50A will get us to let say Vce sat = 3v will be needed to dissipate 150W where 3v drop is a real number from datasheet above, and that is way over for DX200 radiator. So, less value is a preference, 

    As I've heard this 33NEC125T2 is heavily customized specifically for welders schematically w/ the best IGBTs used at that time, so I'd be careful, but sure you can experiment with what you have, you gotta start with something. Meantime, I'm thinking about the way to take measurement without destroying good power module which I can't afford, and we need to get a close match by most critical parameters and better match those IGBTs will help us to get a stable outcome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lanuser
    lanuser over 4 years ago in reply to mb443
    mb443 said:
    As I've heard this 33NEC125T2 is heavily customized for specifically for welders

    I am sure will find solution :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mb443
    mb443 over 4 years ago in reply to lanuser

    Seems like I wasn't able to take measurements due to my power module is not responding to anything due to possible damage from gates side while Collector-Emitter side doesn't have any visible burns and crystal looks ok.
    As requested I will add the schema I used to measure Vge threshold.

    image

    To measure voltage on the gate connect one multimeter set to DC voltage and begin raising it from 0v and up watch for current in Collector when it reaches 6mA and that would be a Vce threshold level. Then Vce saturated can be also measured with multimeter set on DC voltage connected to Collector-Emitter and watch when voltage stop dropping, so the lowest voltage would be your Vce saturated. 

    Warning! Since you will fully open IGBT, the maximum current will be going through transistor, so radiator is a MUST use as for example with 60v power supply and 20ohm load there will be 3A current going through IGBT and with roughly 3v saturation there will be 9Watt power dissipated as a heat. So to prevent IGBT from going into cardiac arrest, use radiator or make your measurements very quick. Radiator is also suggested if you interested in stable values of measurements. Or simply DO NOT measure Vce saturated, only Vge th is the most interested parameter anyway.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mb443
    mb443 over 4 years ago in reply to mb443

    in case anyone cares, the fragment on the bottom right is simply what is inside of any IGBT, as many think it's a new technology but in reality it's just a mosfet + bipolar transistor put together along with snabber diod into one case and call it IGBT, similar to darlington transistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lanuser
    lanuser over 4 years ago in reply to mb443

    Your test design is correct, however, instead of R* 5 ohm load replace with lightbulb.

    Also, if you are using  dual power supply make sure to combine GND.

    And yes while conducting test PM must have heat dissipation / radiator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mb443
    mb443 over 4 years ago in reply to lanuser

    Schema seems ok, as of PCB I can't really see the whole board as image is cut on a sides. And I'm pretty backed up with other things nowadays, so whenever i have time. Also, did you succeed measuring your PM? Wondering what is Vge threshold on those?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>