Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Driving e-Paper display with Adafruit Feather nRF52 Bluefruit LE, but not getting sharp Image
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 301 subscribers
  • Views 2729 views
  • Users 0 members are here
  • epaper
  • nrf52
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Driving e-Paper display with Adafruit Feather nRF52 Bluefruit LE, but not getting sharp Image

KKaushik
KKaushik over 3 years ago

I am driving e-Paper display with nRF52 Module named mentioned above, but not getting sharp image

#include <GxEPD.h>

#include <GxGDEH0213B73/GxGDEH0213B73.h> // 2.13" b/w newer panel

#include GxEPD_BitmapExamples

// FreeFonts from Adafruit_GFX
#include <Fonts/FreeMonoBold9pt7b.h>
#include <Fonts/FreeMonoBold12pt7b.h>
#include <Fonts/FreeMonoBold18pt7b.h>
#include <Fonts/FreeMonoBold24pt7b.h>


#include <GxIO/GxIO_SPI/GxIO_SPI.h>
#include <GxIO/GxIO.h>

#include "IMG_0001.h"

GxIO_Class io(SPI, /*CS=*/ 4, /*DC=*/ 3, /*RST=*/ 2); // arbitrary selection of 8, 9 selected for default of GxEPD_Class

GxEPD_Class display(io, /*RST=*/ 2, /*BUSY=*/ 5); // default selection of (9), 7

void setup()
{
Serial.begin(115200);
Serial.println();
Serial.println("setup");

display.init(115200); // enable diagnostic output on Serial

Serial.println("setup done");
//showpic();
}

void loop()
{
//showpic();
display.drawPaged(showFontCallback);
delay(5000);
}
void showFontCallback()
{
const char* name = "FreeMonoBold9pt7b";
const GFXfont* f = &FreeMonoBold9pt7b;
display.fillScreen(GxEPD_WHITE);
display.setTextColor(GxEPD_BLACK);
display.setFont(f);
display.setCursor(0, 0);
display.println();
display.println(name);
display.println(" !\"#$%&'()*+,-./");
display.println("0123456789:;<=>?");
display.println("@ABCDEFGHIJKLMNO");
display.println("PQRSTUVWXYZ[\\]^_");
#if defined(HAS_RED_COLOR)
display.setTextColor(GxEPD_RED);
#endif
display.println("`abcdefghijklmno");
display.println("pqrstuvwxyz{|}~ ");
}

void showpic()
{
//uint16_t x = (display.width() - 128) / 2;
uint16_t x = 0;
uint16_t y = 0;
display.fillScreen(GxEPD_BLACK);
display.drawExampleBitmap(gImage_IMG_0001, x, y, 128, 250, GxEPD_WHITE);
display.update();

}

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +3
    The black and white particles get separated based on voltage and duration of the applied signal. You can check the high voltage supply to ensure it is high enough (it could also need extra capacitance…
  • shabaz
    shabaz over 3 years ago in reply to KKaushik +2
    Where did you buy the display from? Did you buy it from the some source that the driver code came from, or not? You can see in the datasheet that you provided: The special parameters are not part…
  • feiticeir0
    feiticeir0 over 3 years ago in reply to KKaushik +1
    Hi ! I'm guessing, by the pictures, that's a display problem... Did it, in any time, give a sharper image ? Even the first time you thinker with it ?
Parents
  • shabaz
    0 shabaz over 3 years ago

    Where did you buy the e-paper display from?

    The code that drives them is fine-tuned to match production runs of e-paper displays, because the manufacturing process has variations from what I understand. The code usually has a load of configuration parameters. If you're using Adafruit code, then the configuration parameters will be best tuned for their displays.

    The display manufacturer is responsible for providing the set of values, it's not something you can derive yourself.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KKaushik
    0 KKaushik over 3 years ago in reply to shabaz

    https://drive.google.com/file/d/1ZL9M1V500O0vegqsBbeMTPr0Vli2cNjX/view?usp=sharing 
    Could you please which setting I need to look for to make changes in code as per datasheet provided by manufacturer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to KKaushik

    Where did you buy the display from? Did you buy it from the some source that the driver code came from, or not?

    You can see in the datasheet that you provided:

    image

    The special parameters are not part of the datasheet, since they can change after production runs. 

    The special parameters will most likely be within a header file in the code you're using.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KKaushik
    0 KKaushik over 3 years ago in reply to shabaz

    No, the display is from a direct manufacturer and not the ones in code which is from Adafruit libraries.

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to KKaushik

    I see, in that case, the manufacturer of the display needs to provide that data file, and you need to then modify the Adafruit code (header file most likely) to replace the config params with the ones that match your display. Otherwise, the result will never be perfect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago in reply to KKaushik

    I see, in that case, the manufacturer of the display needs to provide that data file, and you need to then modify the Adafruit code (header file most likely) to replace the config params with the ones that match your display. Otherwise, the result will never be perfect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • KKaushik
    0 KKaushik over 3 years ago in reply to shabaz

    Got it, I will contact the manufacturer about same. Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KKaushik
    0 KKaushik over 3 years ago in reply to shabaz

    Also, could you refer to what kind of waveform I'm supposed to look for with reference to the waveshare 2.13 EPD datasheet?

    https://www.waveshare.com/w/upload/d/d3/2.13inch-e-paper-b-Specification.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to KKaushik

    It's digitally described in the form of special config params, as mentioned. It's not in the datasheet, the manufacturer provides it in a file.