Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Stereo Phono Cartridge to both Stereo and Mono Amps
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 338 subscribers
  • Views 6673 views
  • Users 0 members are here
  • phono
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Stereo Phono Cartridge to both Stereo and Mono Amps

TC_Walker
TC_Walker over 3 years ago

Hello,

I am interested in a project to take a stereo signal from a record needle cartridge and split the signal into a stereo amp and also a mono amp to be used at the same time (and independently with some switching). I have tried a couple of simple methods that negatively effected the stereo signal. I am thinking op amps might be a way to do this but I am unable to design this. Regardless of what method is used sharing your knowledge would be so greatly appreciated.

- Tom

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +2
    Shabaz explains the principle in his message. (Although I think 1k resistors may be too low for some pre-amps) The problem is that a good mono mix is not made by adding the two channels of a stereo mix…
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett +2
    Hi Michael, I found a reference to ceramic pickups on http://www.douglas-self.com/ampins/library/ampartew.htm which directed to a Wireless World article. In the August 1971 PDF issue of Wireless World…
  • michaelkellett
    michaelkellett over 3 years ago in reply to TC_Walker +2
    It looks as if you are going to try building a pre-amp based on the WW design. Meanwhile I have a little charge amplifier from Jan Cumps to test. He designed the board based on some suggestions from…
  • shabaz
    0 shabaz over 3 years ago in reply to michaelkellett

    Hi Michael,

    I see what you mean. The charts below show the response measurement of the first stage (I can't simulate the entire circuit end-to-end due to a license limit).

    Due to the low input impedance they are setting the gain to more than 20 dB higher to compensate at the low end. With the 1nF model, the response then becomes levelled out with the input trimmer set to approx 40kohm. It doesn't seem an ideal way to interface to such a cartridge : ( I'll put this design on hold since it has these shortcomings, and it won't perform like a modern circuit. I guess magnetic cartridges superseded the ceramic ones and no-one improved these circuits much, since there doesn't seem to be many designs on the web.

    image

    Regarding Q6 and Q7, they were there to reduce load on the main stereo output, because the simulation showed a bit more distortion with a lower resistance for the load. I could increase the mixing resistances and replace with a single amplifier, but since it was just a single extra BJT I left it there since I'd already simulated with that topology. I didn't see much distortion for that section with the simulation, it was pretty negligible at that low output amplitude for the mono output, but perhaps I should have simulated with a higher input. I was just guessing what the cartridge level would be at that time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<