Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Latch ciruit Design Problem/Sugguestions
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 338 subscribers
  • Views 1283 views
  • Users 0 members are here
  • esp32
  • help
  • suggestion
  • circuit
  • Design
  • latch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Latch ciruit Design Problem/Sugguestions

Chuitoto
Chuitoto over 3 years ago

Hi! I'm working on a project which needs latch circuit in my design, which use for Power on/off by hardware and software...

VBAT is 12V. so I put it through a LDR to logic 3V3.

First I have a latch switch, when logic 3V3(pin2) connect to pin1. The top Pmons ON then power up the device.

When the  logic 3V3(pin2) connect to pin3, off_requ gose high(1) then go in some MCU input. The MCU will do some proccess., then set output off_pwr to hight (1) to disable the top Pmos. 

Will the below diagram works as I discribe above ? Feel free to give me some suggestion for improve design ! 

thank you so much if you do so! 

Latch circuit

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +1
    This should work fine. You can reduce the power in the on state by using N channel FETs instead of bipolar transistors. Something like BSS138. or 2N7000.
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    man, you like to spend money.  use this instead works great with AC no mus, no fuss. 

    Just make sure the relay contact can deal with the current, and lastly make sure the relay is rated for continuous operation. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 3 years ago

    man, you like to spend money.  use this instead works great with AC no mus, no fuss. 

    Just make sure the relay contact can deal with the current, and lastly make sure the relay is rated for continuous operation. image