Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Struggling to select the correct Analog Switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 337 subscribers
  • Views 2203 views
  • Users 0 members are here
  • pt100
  • analog switch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Struggling to select the correct Analog Switch

BigG
BigG over 3 years ago

I wish to create this circuit (not a fully complete design), where I am hijacking a Pt100 sensor for my own readings while still allowing an existing system to read the values correctly. I'm thinking that if I switch fast enough, with the help of smoothing capacitors, I could just about get away with it as there will be a fair bit of sampling and averaging to get a temperature value.

To do this, I decided to use an analog switch as these typically have low on resistance values. What I cannot figure out is whether I need a device like a Vishay DG419LEDY-T1-GE4 which has a signal range of -15V to 15V or I could use a SPDT analog switch with a lower voltage. I think I am correct in thinking that the max voltage of Vin is the max voltage allowed through the COM-NC pin etc.

I just wanted confirmation.

image

Of course, if there is an easier way to do this, I love to hear your views as I have a habit of over complication.

Thanks

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +3
    What is the existing system ? It may get very upset by the switching, or if are really lucky, you might not need switching at all. I have systems that measure using thermistors where one side if the…
  • BigG
    BigG over 3 years ago in reply to michaelkellett +1
    I was hoping not to switch but could not see how it would work without upsetting the system - I'm also working the principle that more resistance is better than lowering the overall resistance. With the…
  • scottiebabe
    scottiebabe over 3 years ago +1
    Step 1, solve the puzzle Step 2, win the prize Step 3, start probing around :)
Parents
  • shabaz
    0 shabaz over 3 years ago

    Hi Colin,

    If there was absolutely no other way (i.e. depends on your use-case/end requirement/connected equipment as Michael says), and you definitely had to read that same PT100, directly at the sensor, then if it were me, I'd probably experiment with a single SPDT reed relay (only needs one, if you've not got any common connections between your system and the existing system), but some systems might check for broken sensor connections, or have other issues with the connection being removed by your microcontroller periodically. Reed relay has current consumption, but still very low overall if (say) the temperature is only being measured (say) once a minute.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago

    Hi Colin,

    If there was absolutely no other way (i.e. depends on your use-case/end requirement/connected equipment as Michael says), and you definitely had to read that same PT100, directly at the sensor, then if it were me, I'd probably experiment with a single SPDT reed relay (only needs one, if you've not got any common connections between your system and the existing system), but some systems might check for broken sensor connections, or have other issues with the connection being removed by your microcontroller periodically. Reed relay has current consumption, but still very low overall if (say) the temperature is only being measured (say) once a minute.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • BigG
    0 BigG over 3 years ago in reply to shabaz

    Yes needs to be the same Pt100 as cannot insert another sensor in same location. Yes, you are right a single SPDT is probably all I need. Thanks Shabaz for the suggestion to use a reed relay. I will do some research.