Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Struggling to select the correct Analog Switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 337 subscribers
  • Views 2203 views
  • Users 0 members are here
  • pt100
  • analog switch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Struggling to select the correct Analog Switch

BigG
BigG over 3 years ago

I wish to create this circuit (not a fully complete design), where I am hijacking a Pt100 sensor for my own readings while still allowing an existing system to read the values correctly. I'm thinking that if I switch fast enough, with the help of smoothing capacitors, I could just about get away with it as there will be a fair bit of sampling and averaging to get a temperature value.

To do this, I decided to use an analog switch as these typically have low on resistance values. What I cannot figure out is whether I need a device like a Vishay DG419LEDY-T1-GE4 which has a signal range of -15V to 15V or I could use a SPDT analog switch with a lower voltage. I think I am correct in thinking that the max voltage of Vin is the max voltage allowed through the COM-NC pin etc.

I just wanted confirmation.

image

Of course, if there is an easier way to do this, I love to hear your views as I have a habit of over complication.

Thanks

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +3
    What is the existing system ? It may get very upset by the switching, or if are really lucky, you might not need switching at all. I have systems that measure using thermistors where one side if the…
  • BigG
    BigG over 3 years ago in reply to michaelkellett +1
    I was hoping not to switch but could not see how it would work without upsetting the system - I'm also working the principle that more resistance is better than lowering the overall resistance. With the…
  • scottiebabe
    scottiebabe over 3 years ago +1
    Step 1, solve the puzzle Step 2, win the prize Step 3, start probing around :)
Parents
  • Gough Lui
    0 Gough Lui over 3 years ago

    I wouldn't want to break any circuit the existing Pt100 is in, purely because its resistance is so low compared to the actual resistance that would be introduced by your switching elements. That would have a significant impact on the measured temperature by both systems. With a nominal resistance of 100-ohms at 25C, it really won't be happy if you added another 20-ohm (typ at 10mA) for that particular switch for example in the illustrated two-wire connection method.

    For slow-speed switching, perhaps you can get away with a nice gold-plated signal relay depending on the current. That would have much lower contact resistance and thus influence on temperature.

    I would still suggest reverse engineering the current circuit more. Many Pt100-based devices use three-wire or four-wire connections to negate lead resistance for higher accuracy. In the case of four-wire, you could conceivably use higher resistance switches as long as it's being compensated for by the four-wire connection (but watch the limits of compensation by the circuit). If it's three-wire, then likely it will be running a common ground side, so switching one-side and having compensation on that side is a possibility too.

    Instead, if you are able to reverse-engineer it further, then that would be even better. At a guess, most Pt100 RTDs are likely to be driven like a DMM would, with a constant current through its drive pair. A voltage is read back through a sense pair (depending on how it is configured, in two-wire, they are the same; in three-wire, they are separated on one side and commoned on the other; in four-wire, they are all independent). If you can know what this constant current is, then the Pt100 will have a voltage on its sense connections that will tell you the temperature - from there, I would probably choose a low input offset current op-amp and use it as a voltage buffer into your own system. That would present a very high impedance (thus affecting the current circuit very little) and avoid any loading effects. You will have to know what the measurement circuit's voltage is to avoid burning out an opamp, but it's likely to be small because they're not looking for a high current through the RTD, as its self heating would affect the result.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 3 years ago

    I wouldn't want to break any circuit the existing Pt100 is in, purely because its resistance is so low compared to the actual resistance that would be introduced by your switching elements. That would have a significant impact on the measured temperature by both systems. With a nominal resistance of 100-ohms at 25C, it really won't be happy if you added another 20-ohm (typ at 10mA) for that particular switch for example in the illustrated two-wire connection method.

    For slow-speed switching, perhaps you can get away with a nice gold-plated signal relay depending on the current. That would have much lower contact resistance and thus influence on temperature.

    I would still suggest reverse engineering the current circuit more. Many Pt100-based devices use three-wire or four-wire connections to negate lead resistance for higher accuracy. In the case of four-wire, you could conceivably use higher resistance switches as long as it's being compensated for by the four-wire connection (but watch the limits of compensation by the circuit). If it's three-wire, then likely it will be running a common ground side, so switching one-side and having compensation on that side is a possibility too.

    Instead, if you are able to reverse-engineer it further, then that would be even better. At a guess, most Pt100 RTDs are likely to be driven like a DMM would, with a constant current through its drive pair. A voltage is read back through a sense pair (depending on how it is configured, in two-wire, they are the same; in three-wire, they are separated on one side and commoned on the other; in four-wire, they are all independent). If you can know what this constant current is, then the Pt100 will have a voltage on its sense connections that will tell you the temperature - from there, I would probably choose a low input offset current op-amp and use it as a voltage buffer into your own system. That would present a very high impedance (thus affecting the current circuit very little) and avoid any loading effects. You will have to know what the measurement circuit's voltage is to avoid burning out an opamp, but it's likely to be small because they're not looking for a high current through the RTD, as its self heating would affect the result.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • BigG
    0 BigG over 3 years ago in reply to Gough Lui

    Yep, as I suspected this is a sneaky design challenge.

    Gough Lui said:
    I would still suggest reverse engineering the current circuit more. Many Pt100-based devices use three-wire or four-wire connections to negate lead resistance for higher accuracy. In the case of four-wire, you could conceivably use higher resistance switches as long as it's being compensated for by the four-wire connection (but watch the limits of compensation by the circuit). If it's three-wire, then likely it will be running a common ground side, so switching one-side and having compensation on that side is a possibility too.

    Yes it would be handy if they do that. I'm guessing that I will only find that out once I've messed with things / messed things up.

    The recommended constant current is 1mA so I'm assuming that's what they're using or it's very close to that value.

    I was thinking along similar lines regarding op amp, but as I do not know whether they are  working off a max of 24V or if it's 12V, or somewhere in between.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 3 years ago in reply to Gough Lui
    Gough Lui said:
    I would probably choose a low input offset current op-amp and use it as a voltage buffer into your own system. That would present a very high impedance (thus affecting the current circuit very little) and avoid any loading effects.

    I cannot quite see how this works. If possible, could you sketch it - I like pictures Grin