Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Struggling to select the correct Analog Switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 337 subscribers
  • Views 2202 views
  • Users 0 members are here
  • pt100
  • analog switch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Struggling to select the correct Analog Switch

BigG
BigG over 3 years ago

I wish to create this circuit (not a fully complete design), where I am hijacking a Pt100 sensor for my own readings while still allowing an existing system to read the values correctly. I'm thinking that if I switch fast enough, with the help of smoothing capacitors, I could just about get away with it as there will be a fair bit of sampling and averaging to get a temperature value.

To do this, I decided to use an analog switch as these typically have low on resistance values. What I cannot figure out is whether I need a device like a Vishay DG419LEDY-T1-GE4 which has a signal range of -15V to 15V or I could use a SPDT analog switch with a lower voltage. I think I am correct in thinking that the max voltage of Vin is the max voltage allowed through the COM-NC pin etc.

I just wanted confirmation.

image

Of course, if there is an easier way to do this, I love to hear your views as I have a habit of over complication.

Thanks

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +3
    What is the existing system ? It may get very upset by the switching, or if are really lucky, you might not need switching at all. I have systems that measure using thermistors where one side if the…
  • BigG
    BigG over 3 years ago in reply to michaelkellett +1
    I was hoping not to switch but could not see how it would work without upsetting the system - I'm also working the principle that more resistance is better than lowering the overall resistance. With the…
  • scottiebabe
    scottiebabe over 3 years ago +1
    Step 1, solve the puzzle Step 2, win the prize Step 3, start probing around :)
Parents
  • BigG
    0 BigG over 3 years ago

    I was reflecting on the comments made to my half-baked solution. Very enlightening and very helpful. Thanks.

    I do recall seeing a digital voltmeter solution using an Arduino and thought, why no incorporate that. So this is what I came up with (hopefully this a 3/4 baked solution). Haven't shown in diagram but assuming MCU GND can be attached to VSS (system ground) in Control Panel.

    Still not sure if it helps me determine the pt100 resistance value and thus the temperature and whether this new circuit will impact the control panels existing readings. Maybe I need different resistor values etc.

    I'm also assuming Analog Read probably needs opamp as per Gough Lui comment. Also assuming Analog switch can be swapped out for a different SPDT like a reed or solid state relay as on resistance is no longer a factor.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • BigG
    0 BigG over 3 years ago

    I was reflecting on the comments made to my half-baked solution. Very enlightening and very helpful. Thanks.

    I do recall seeing a digital voltmeter solution using an Arduino and thought, why no incorporate that. So this is what I came up with (hopefully this a 3/4 baked solution). Haven't shown in diagram but assuming MCU GND can be attached to VSS (system ground) in Control Panel.

    Still not sure if it helps me determine the pt100 resistance value and thus the temperature and whether this new circuit will impact the control panels existing readings. Maybe I need different resistor values etc.

    I'm also assuming Analog Read probably needs opamp as per Gough Lui comment. Also assuming Analog switch can be swapped out for a different SPDT like a reed or solid state relay as on resistance is no longer a factor.