Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using TVS Diode P6KE across relay coil but then also relay coil is getting damaged.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 340 subscribers
  • Views 4553 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using TVS Diode P6KE across relay coil but then also relay coil is getting damaged.

e14 Contributor
e14 Contributor over 10 years ago

We are using TVS diode across 24V DC-100AMPs relay for automotive application but my relay coil is getting damaged.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +1
    Unfortunately the schematic shows a relay and not what is connected on the load side, or how the 24v DC is sourced (ie switchmode supply, battery, etc). What is on the end of the 100A contacts.? ie a simple…
  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +1
    That image helps.... There is no heating apparent from the contact as it seems to be a nice copper colour. The coil wire appears to have fused. For any inductive circuit the In-rush/ON current is very…
  • mcb1
    mcb1 over 10 years ago in reply to e14 Contributor +1
    We are trying to help.... If you can't provide a circuit then I'm afraid my anwers are limited to guessing ... Mark
Parents
  • artful_bodger
    artful_bodger over 10 years ago

    I'm with lucie tozer.  I think you've got a heating problem caused by peaks in the alternator output.

    You say the relay operates 3 hours with no load, but was that on a lab supply, or on the alternator?

    Stick a scope on there and have a look at the coil volts.  I can't think of a way the load could directly damage the coil.

    Once you know what the waveform looks like, you can send it to the manufacturer for help.

    A charged battery will be around 28V (you have a battery in circuit?), or a bit more, so a 30V diode may be a bit tight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • artful_bodger
    artful_bodger over 10 years ago

    I'm with lucie tozer.  I think you've got a heating problem caused by peaks in the alternator output.

    You say the relay operates 3 hours with no load, but was that on a lab supply, or on the alternator?

    Stick a scope on there and have a look at the coil volts.  I can't think of a way the load could directly damage the coil.

    Once you know what the waveform looks like, you can send it to the manufacturer for help.

    A charged battery will be around 28V (you have a battery in circuit?), or a bit more, so a 30V diode may be a bit tight.