Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Rms converter to match HP3400A?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 72 replies
  • Subscribers 335 subscribers
  • Views 12284 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Rms converter to match HP3400A?

ggabe
ggabe over 3 years ago

What is your suggestion to match the specs of the HP3400A AC millivoltmeter’s rms converter with analog parts available today? I’m drawing a line to exclude AD conversion and digital rms calculation. So it stays analog.

Below is the spec sheet:

image

  • Sign in to reply
  • Cancel

Top Replies

  • ggabe
    ggabe over 3 years ago in reply to phoenixcomm +4
    My motivation is “restoration”. This is the only analog instrument I have. I like the retro vibe of the mirrored gauge. Three different rms converters in my parts box already, time to make them work all…
  • scottiebabe
    scottiebabe over 3 years ago in reply to scottiebabe +4
    .
  • scottiebabe
    scottiebabe over 3 years ago in reply to phoenixcomm +4
    .
Parents
  • Electrojim
    Electrojim over 3 years ago

    Not quite sure what you're asking here.  Is the 'converter' an add-on to the 3400A that you want to build from scratch and put into your meter?  Or do you just need an analog r.m.s. converter with those specs for something else? Or are you looking for a complete equivalent to the 3400A that does all measurements in the analog domain?  Old National Semiconductor app-note books had designs for r.m.s. measurement, although I'm not sure they went to 10MHz.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ggabe
    ggabe over 3 years ago in reply to Electrojim

    I have a 3400 with burned out thermocouple converter. I want to rebuild the guts between the input BNC and the analog meter. Building AC amplifiers with 10MHz <1% tolerance is a no issue. The rms converter with 5% error at 10MHz is. Also the crest factor. And again, the parts should be new, and not from an eBay thermal converter surplus.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Electrojim
    Electrojim over 3 years ago in reply to ggabe

    Right, I see your problem.  The meter having ranges in (I assume) 10dB steps probably means that the converter has to be really accurate over only a 20dB range or so, it's probably sitting somewhere in the meter circuitry where it's working on voltages in the tens to hundreds of millivolts or more. But you're right, the 10MHz requirement is a tough one.  Most of the r.m.s.-ing circuits I'm familiar with use the nonlinear characteristics of transistors in some feedback circuit, which if built with op-amps that can slew up a storm might be good to 10MHz.  Never built one though.  Best of luck!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Electrojim
    Electrojim over 3 years ago in reply to ggabe

    Right, I see your problem.  The meter having ranges in (I assume) 10dB steps probably means that the converter has to be really accurate over only a 20dB range or so, it's probably sitting somewhere in the meter circuitry where it's working on voltages in the tens to hundreds of millivolts or more. But you're right, the 10MHz requirement is a tough one.  Most of the r.m.s.-ing circuits I'm familiar with use the nonlinear characteristics of transistors in some feedback circuit, which if built with op-amps that can slew up a storm might be good to 10MHz.  Never built one though.  Best of luck!