Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Strobing Using RGB LEDs Instead Of Flash Tubes
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 335 subscribers
  • Views 3438 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Strobing Using RGB LEDs Instead Of Flash Tubes

publicimage
publicimage over 3 years ago

I would like to create a something like a strobe but with very bright RGB LEDs.

Can anyone suggest a product?

Can I use a MOSFET to power something like this? 

Which Arduino Would work best?

Please help!

--Vince

  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary over 3 years ago +1
    The Junk-Pile Strobe Tachometer.....and it really works! See the blog for some ideas. It's not so much the arduino, or the mosfet, but your LEDs are a critical component. A strobe has alot of power for…
  • robogary
    robogary over 3 years ago in reply to publicimage +1
    So more like flashing lights than a strobe...
  • ggabe
    ggabe over 3 years ago in reply to robogary +1
    Both Amazon and AliExpress has LED strobe party lights. Hard to beat Ali’s price, unless you already have the components on hand. You can always reverse engineer and replace the controller with an Arduino…
Parents
  • robogary
    robogary over 3 years ago

     The Junk-Pile Strobe Tachometer.....and it really works! 

    See the blog for some ideas. It's not so much the arduino, or the mosfet, but your LEDs are a critical component. A strobe has alot of power for a very short time, your led must be capable of handling the punch, and a power supply that can deliver it..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • publicimage
    publicimage over 3 years ago in reply to robogary

    Will I be able to use something like a capacitor? This is used in a xenon strobe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to publicimage

    The trigger concepts and circuits for an LED are much different than a xenon strobe bulb.

    For xenon tubes with distance between electrodes 13 to 32 mm and tubing inside diameter under 3 mm, use 350 to 550 volts for flash energy 5 to 12 millijoules per cubic millimeter. For lower flash energy, use slightly higher voltage. Ouch. 

    The LED will use a much lower forward voltage, often less than 20, but alot more amps to get a respectable flash. The flash on time can be hundredths of a second. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 3 years ago in reply to publicimage

    The trigger concepts and circuits for an LED are much different than a xenon strobe bulb.

    For xenon tubes with distance between electrodes 13 to 32 mm and tubing inside diameter under 3 mm, use 350 to 550 volts for flash energy 5 to 12 millijoules per cubic millimeter. For lower flash energy, use slightly higher voltage. Ouch. 

    The LED will use a much lower forward voltage, often less than 20, but alot more amps to get a respectable flash. The flash on time can be hundredths of a second.