Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need help to replace a resistor
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 334 subscribers
  • Views 9455 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need help to replace a resistor

ldarby
ldarby over 3 years ago

Hopefully this isn't a dumb question but this resistor is cracked and slightly burnt.  I measured it, it's open circuit.   It's from my bosch washing machine which is about 12 years old.  I think it's brown, black, silver, gold which is 0.1 Ohm (can't be grey, that's 1 giga ohm), but I've found several other photos showing this resistor on this pcb is brown black brown, 100 ohm, and people saying it's 100 ohm as well, and no one saying it's 0.1 ohm.  It's 'Ako 731799-06 BSH 9000449412'  if you would like search yourself.  Could it really be 100 ohm, and the burn slowly chared ring 3 to look grey/silver over time?  If it's supposed to be 100 ohm, and I replace it with 0.1, I'm sure it'll blow up...

Next question, since this failure seems to be very common, would it make sense to replace it with a higher power resistor e.g. 5W or 10W?

Thanks.


image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago in reply to ldarby +4
    Unfortunately not enough detail from the photos, the connection snakes off from the top side of the board, but I can't see where due to angle. Anyway, it's a resistor directly off the Live connection…
  • ldarby
    ldarby over 3 years ago in reply to anniel747 +2
    Yeah, oops, maybe was possible. There was a much larger crack (not shown in above photos), I tried opening up that crack but that made the whole shell pop off and took all the wire with it... lesson l…
  • ldarby
    ldarby over 3 years ago in reply to shabaz +2
    Thanks very much for that, the chip left of center is a full bridge rectifier, it connects to that, then the cap is 10uF, 400V, and that connects to the D (Drain) pin. I couldn't see any inductors though…
Parents
  • bobthemallett
    bobthemallett over 3 years ago

    Oh yeah, that's a 100R 5% (this type I doubt is available in 0R1), looks 3W or maybe 2W (smaller) (but check the size - dims are a VERY useful clue!). When a Power Resistor has smoked up it's often a FET gone closed circuit so check. If all going fine then should be a good enough rating but if you can find a 5W and get it to fit, can't hurt! Bob

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bobthemallett
    bobthemallett over 3 years ago

    Oh yeah, that's a 100R 5% (this type I doubt is available in 0R1), looks 3W or maybe 2W (smaller) (but check the size - dims are a VERY useful clue!). When a Power Resistor has smoked up it's often a FET gone closed circuit so check. If all going fine then should be a good enough rating but if you can find a 5W and get it to fit, can't hurt! Bob

    • Cancel
    • Vote Up -1 Vote Down