Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to control the HV converter with analog voltage signal?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 334 subscribers
  • Views 5288 views
  • Users 0 members are here
  • power_electronics
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to control the HV converter with analog voltage signal?

Dykan
Dykan over 3 years ago

The HV converter require 24V power supply and some analog voltage signals. I connect two 0~10V voltage signals to the pin of HV converter, 10HVA24-N1. However what I get from the output of HVA is 0V. Is there any thing wrong with my wiring?

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 3 years ago in reply to Dykan +3
    Pin 12 is the current monitor output. It will output a voltage that's proportional to the HV current being supplied by the module. Hopefully there's enough resistance in series with the output that you…
  • michaelkellett
    michaelkellett over 3 years ago in reply to Dykan +2
    So it looks as if your power supply thinks it is working. How is you divider working - (diagram) - its a strange co-incidence that 100uA into 0.63M would give excatly 63V. Your power supply max output…
  • dang74
    dang74 over 3 years ago +1
    Interesting device. Reading through the app note that is available on the manufacturer's website I noticed that pin 11 can be driven by TTL. The app note suggests that the level on pin 11 must be at least…
Parents
  • anniel747
    0 anniel747 over 3 years ago

    Pin 15?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anniel747
    0 anniel747 over 3 years ago

    Pin 15?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Dykan
    0 Dykan over 3 years ago in reply to anniel747

    Pin15 is the same as pin 6

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Dykan

    Probably time for photos of your setup, including the power supply, the connections to the device, and how you're testing. Are you using a proper connector for the output? We can't tell. Is your power supply capable of the current draw? Who knows.

    We don't know what we can't see, so please supply some detailed photos in case the issue can be identified, and also multimeter measurements of the supply and the current consumption when you enable it. Also, a photo of what're you've connected to the output.

    There are not many connections, not a lot to go wrong, so if you supply this detail it will probably help quickly resolve it.

    Please, no fuzzy photos, use a bright light if it helps to take the photos,  and no Dropbox etc.. you can add the photos inline in the discussion you created.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Dykan
    0 Dykan over 3 years ago in reply to shabaz

    The DB15 connector I used is connected to the input control terminal of the HVA, and the tested pins are corresponding and correct. My 24V power supply can supply up to 800W, which definitely meets the needs of HVA