Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What SoC should i use for this project?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 335 subscribers
  • Views 4436 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What SoC should i use for this project?

flows
flows over 2 years ago

Okay this is my first time using a forum to ask something so apologies for my english and questions asking.

Whats is my project: I want to make my own controller to control LED strips for ambient lights behinde my tv. The LED's sync to what’s happening on the screen.

My plan: I want to take a hdmi input from a source (like chrome cast or gaming console), process the image and then pas the hdmi input, out to the tv, via hdmi out. To split the hdmi input to the SoC and the tv, i will use a seperate hdmi splitter, if it takes to much bandwith or prossecing power to pass trough via the SoC.

What does the image prossecing look like?: I want to take a avarage of the colors of a area. This area will be allong the sides of the screen. I also added a really ruf sketch of what i mean by area. The number of areas depend on the number of LED's around the screen. I am not sure if this is the final way i am going to do this, but this gives you a idea of what i mean by image prossecing.

image

To cut on procesing cost/time i think i will maybe down scale the image it needs to proccess. For example when you have a 4k image input, it needs to collect a lot of pixel color values, and take a average of them. While we maybe dont need that much detail. I dont know how far i will down scale the image, but i will know this after testing.

The qeustion: So now you know my plan, my qeustion is: What SoC should i use for this project? The main reason i ask this qeustion is because i dont know how much computing power it wil take to prosses a image this way. I know i can probably use a raspberry pi, but i also dont want to use a overpowerd SoC for this project. Also because i maybe want to produce more of these i need to think about cost.

Requirments:

   - It needs to have I/O pins (ofcourse)
   - There needs to be a way that i can have hdmi in (in to the SoC ofc) (it doenst have to be include on the SoC)
   - It needs to output data to the LED strip with a rate that it looks smooth to what happens on the screen (i dont know how many FPS that is, i think around 15-30 FPS)
   - (This isn't a must but it would make the project more intresseting) There needs to be a way it can have wifi (preferably onboard wifi)

More info:

   - I will be writing a "library" my self to controll the LED strip
   - The program wil be written in C++
   - For the image prossecing i think i will use the openCV library
   - I will use the WS2812B LED's

If you have any qeustions ask me!

I haven't tryed any SoC yet, i do have the raspberry pi 4 B at home.

  • Sign in to reply
  • Cancel

Top Replies

  • saadtiwana_int
    saadtiwana_int over 2 years ago +6
    I have considerable experience with video processing up to around 1080p60 (not 4k). I can suggest you two ways to do this if 1080p60 is enough for you: 1. You can use a HDMI-to-USB3 frame grabber (~10…
  • saadtiwana_int
    saadtiwana_int over 2 years ago in reply to beacon_dave +3
    beacon_dave Regarding the EDID data in FPGA designs, I remember the Digilent IPs (free, open source) handle the EDID data for some of the popular formats,...you need to select the option when instantiating…
  • balajivan1995
    balajivan1995 over 2 years ago +2
    Seems like someone already did this with Raspberry PI and Neopixels. https://www.raspberrypi.com/tutorials/raspberry-pi-tv-ambient-lighting/
  • saadtiwana_int
    0 saadtiwana_int over 2 years ago in reply to beacon_dave

    beacon_dave Regarding the EDID data in FPGA designs, I remember the Digilent IPs (free, open source) handle the EDID data for some of the popular formats,...you need to select the option when instantiating the IP in vivado. But in line with what you have mentioned, those work when the FPGA is already powered on and configured. I haven't seen them adding a EEPROM alongside the FPGA for this purpose. But then again, these designs are not production-ready designs...they're more to get familiar with receiving HDMI (TMDS) data.

    For commercial designs, usually you will use a HDMI received IC before the FPGA (e.g, ADV7511 or LT8619C, or similar) but you run into licensing issues with HDMI. AMD (Xilinx) also has IPs for HDMI TX/RX for FPGAs with transceivers, but they are paid IPs and not cheap. 

    Anyway, thinking about it, I think it's getting complex with FPGAs...I think shabaz 's idea of using a RPi with a HDMI receiver sounds the most practical one, if the person doesn't want to buy a commercial system Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to dang74

    Didn't you get the memo about VGA being deprecated ? Slight smile

    The ADV7611 receiver IC looks like it could do a lot of the heavy lifting. 

    Low Power 165 MHz HDMI Receiver
    https://www.analog.com/media/en/technical-documentation/data-sheets/adv7611.pdf

    Their reference design is based on a HDMI to VGA convertor though. I guess they didn't get the memo either. Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<