Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Any interest in collaborating on a parasitic inductance power supply? It could be used to power small LV projects like IoT nodes and microcontrollers...
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 332 subscribers
  • Views 4975 views
  • Users 0 members are here
  • microcontrollers
  • power-supply
  • iot
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Any interest in collaborating on a parasitic inductance power supply? It could be used to power small LV projects like IoT nodes and microcontrollers...

PPE_COOP
PPE_COOP over 2 years ago

I have been thinking about a design for this for some time. Mostly to help with another project im working on but I thought other people may be interested in the possibilities also. I have already filed a provisional, please see below. Im possibly looking for help developing the idea into a full product/utility patent. I have one utility patent already and understand the process. The problem is that I am completely self taught and could really benefit from a development partner with better engineering skills than myself. I'm not sure if this is a place to ask for this type of help and I apologize if it's not. Please see the excerpt from the application below.

Parasitic inductance power supply


FIELD OF INVENTION
[0001] The present invention relates to a system and method for providing
low-voltage power to single or multiple devices using inductive coupling, which is
facilitated through the mains power feeders of other apparatuses or equipment.
BACKGROUND
[0002] There is a frequent requirement for extracting power from mains supply to
operate low-voltage devices, such as sensors or communication equipment, which
may be independent or integrated with the mains-powered equipment. The
conventional approach involves direct connections to mains power, necessitating the
use of mains-rated power supplies, fuses and complex power electronics. This
method is often excessive for devices needing only milliampere-level current at very
low voltage. An alternative, more efficient solution is the use of parasitic inductive
coupling, which allows for the extraction of power without physically connecting to
the mains conductors. This method can efficiently power various devices, including
battery chargers, ensuring continuous power supply to low-power equipment, even
when the mains power is switched off.


SUMMARY
[0003] This invention involves a method where a coil of wire is wrapped around an
AC mains power conductor connected to power utilization or generation equipment.
Functioning similarly to a current transformer, the fluctuating magnetic flux from
the mains conductor induces an electrical potential in the coil. This induced voltage
is then modified and regulated through electronic circuitry, enabling it to power
small, low-voltage loads. This method effectively eliminates the need for direct
electrical connections to the mains conductors, offering a simpler and less intrusive
power supply solution for low-power devices.

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 2 years ago in reply to PPE_COOP +3
    Perhaps you need to read what I wrote again because you missed the most critical part. Fundamentally, wrapping a coil around an AC mains cable is pointless unless you separate the conductors. Which…
  • anniel747
    anniel747 over 2 years ago +2
    Deleted
  • beacon_dave
    beacon_dave over 2 years ago in reply to javagoza +2
    Just add electronics... TI Designs: TIDA-01385 Energy Harvesting From Current Transformer With Supercapacitor for Fault Indicator Reference Design https://www.ti.com/lit/ug/tidud59/tidud59.pdf
Parents
  • baldengineer
    baldengineer over 2 years ago
    PPE_COOP said:
    This invention involves a method where a coil of wire is wrapped around an
    AC mains power conductor connected to power utilization or generation equipment.

    And that's where I lose interest. 

    For anything like this to be effective, you need the AC mains conductors separated. Otherwise, any coil wrapped around both conductors won't have much of a magnetic field. So, now you need a special installation that doesn't use traditional wiring products, a special coil wrapped around a single conductor, and a special device-side coil to couple the device-to-be-powered.

    That's a lot of special stuff, which is not usually associated with the phrase "cost-effective."

    So, let's say you create a magic inductor that works while wrapped around both conductors. Okay. You still have to deploy the coil anywhere you want a device. It seems pretty likely that you'll want as little material between the two (e.g. drywall). At that point, why wouldn't you just have a normal outlet installed?

    Sorry, it sounds like an interesting idea on paper. But I can't see any practical implementation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 2 years ago
    PPE_COOP said:
    This invention involves a method where a coil of wire is wrapped around an
    AC mains power conductor connected to power utilization or generation equipment.

    And that's where I lose interest. 

    For anything like this to be effective, you need the AC mains conductors separated. Otherwise, any coil wrapped around both conductors won't have much of a magnetic field. So, now you need a special installation that doesn't use traditional wiring products, a special coil wrapped around a single conductor, and a special device-side coil to couple the device-to-be-powered.

    That's a lot of special stuff, which is not usually associated with the phrase "cost-effective."

    So, let's say you create a magic inductor that works while wrapped around both conductors. Okay. You still have to deploy the coil anywhere you want a device. It seems pretty likely that you'll want as little material between the two (e.g. drywall). At that point, why wouldn't you just have a normal outlet installed?

    Sorry, it sounds like an interesting idea on paper. But I can't see any practical implementation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • PPE_COOP
    PPE_COOP over 2 years ago in reply to baldengineer

    I think you should read it again because what you said reveals an inaccurate understanding of the basic principal. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to PPE_COOP

    Perhaps you need to read what I wrote again because you missed the most critical part. 

    Fundamentally, wrapping a coil around an AC mains cable is pointless unless you separate the conductors.

    Which significantly limits the practical usability of such a solution.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to PPE_COOP

    PPE_COOP Words of friendly advice:  Way too aggresive of a response for the culture here - especially if you're looking for someone to work with you.  There are a lot of very smart and helpful people on the forum and they value the civility of the community. Thumbsup

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • PPE_COOP
    PPE_COOP over 2 years ago in reply to kmikemoo

    Did you read his response to me? See below

    This invention involves a method where a coil of wire is wrapped around an
    AC mains power conductor connected to power utilization or generation equipment.
    And that's where I lose interest.

    For anything like this to be effective, you need the AC mains conductors separated. Otherwise, any coil wrapped around both conductors won't have much of a magnetic field. So, now you need a special installation that doesn't use traditional wiring products, a special coil wrapped around a single conductor, and a special device-side coil to couple the device-to-be-powered.

    That's a lot of special stuff, which is not usually associated with the phrase "cost-effective."

    So, let's say you create a magic inductor that works while wrapped around both conductors. Okay. You still have to deploy the coil anywhere you want a device. It seems pretty likely that you'll want as little material between the two (e.g. drywall). At that point, why wouldn't you just have a normal outlet installed?

    Sorry, it sounds like an interesting idea on paper. But I can't see any practical implementation.