Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Any interest in collaborating on a parasitic inductance power supply? It could be used to power small LV projects like IoT nodes and microcontrollers...
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 332 subscribers
  • Views 4982 views
  • Users 0 members are here
  • microcontrollers
  • power-supply
  • iot
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Any interest in collaborating on a parasitic inductance power supply? It could be used to power small LV projects like IoT nodes and microcontrollers...

PPE_COOP
PPE_COOP over 2 years ago

I have been thinking about a design for this for some time. Mostly to help with another project im working on but I thought other people may be interested in the possibilities also. I have already filed a provisional, please see below. Im possibly looking for help developing the idea into a full product/utility patent. I have one utility patent already and understand the process. The problem is that I am completely self taught and could really benefit from a development partner with better engineering skills than myself. I'm not sure if this is a place to ask for this type of help and I apologize if it's not. Please see the excerpt from the application below.

Parasitic inductance power supply


FIELD OF INVENTION
[0001] The present invention relates to a system and method for providing
low-voltage power to single or multiple devices using inductive coupling, which is
facilitated through the mains power feeders of other apparatuses or equipment.
BACKGROUND
[0002] There is a frequent requirement for extracting power from mains supply to
operate low-voltage devices, such as sensors or communication equipment, which
may be independent or integrated with the mains-powered equipment. The
conventional approach involves direct connections to mains power, necessitating the
use of mains-rated power supplies, fuses and complex power electronics. This
method is often excessive for devices needing only milliampere-level current at very
low voltage. An alternative, more efficient solution is the use of parasitic inductive
coupling, which allows for the extraction of power without physically connecting to
the mains conductors. This method can efficiently power various devices, including
battery chargers, ensuring continuous power supply to low-power equipment, even
when the mains power is switched off.


SUMMARY
[0003] This invention involves a method where a coil of wire is wrapped around an
AC mains power conductor connected to power utilization or generation equipment.
Functioning similarly to a current transformer, the fluctuating magnetic flux from
the mains conductor induces an electrical potential in the coil. This induced voltage
is then modified and regulated through electronic circuitry, enabling it to power
small, low-voltage loads. This method effectively eliminates the need for direct
electrical connections to the mains conductors, offering a simpler and less intrusive
power supply solution for low-power devices.

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 2 years ago in reply to PPE_COOP +3
    Perhaps you need to read what I wrote again because you missed the most critical part. Fundamentally, wrapping a coil around an AC mains cable is pointless unless you separate the conductors. Which…
  • anniel747
    anniel747 over 2 years ago +2
    Deleted
  • beacon_dave
    beacon_dave over 2 years ago in reply to javagoza +2
    Just add electronics... TI Designs: TIDA-01385 Energy Harvesting From Current Transformer With Supercapacitor for Fault Indicator Reference Design https://www.ti.com/lit/ug/tidud59/tidud59.pdf
Parents
  • ciorga
    ciorga over 2 years ago

    For the technical part of your application, it looks to me that you may be looking for someone with strong skills in fundamental Physics and strong skills in electrical/electronic engineering.  Can you define the scope of the collaboration?  What is your goal of the collaboration activity?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • PPE_COOP
    PPE_COOP over 2 years ago in reply to ciorga

    Thanks for your response, unfortunately it looks like someone beat me to the gate  https://www.ti.com/lit/ug/tidud59/tidud59.pdf 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to PPE_COOP

    And that's a tenuous at best solution too (suggested by TI to sell their chips : )
    There are far simpler ways to implement a backup supply for signalling power issues wirelessly, which are already deployed in products.

    For a more _general_ solution (e.g. various typically seen IoT nodes), an inductive method has many issues (many already mentioned by people).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago in reply to PPE_COOP

    And that's a tenuous at best solution too (suggested by TI to sell their chips : )
    There are far simpler ways to implement a backup supply for signalling power issues wirelessly, which are already deployed in products.

    For a more _general_ solution (e.g. various typically seen IoT nodes), an inductive method has many issues (many already mentioned by people).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • PPE_COOP
    PPE_COOP over 2 years ago in reply to shabaz

    True, but you can't beat it for simplicity if the only power source available is 480V AC 60A feeder. I'm in the US. We can't tap into any power from a piece of UL listed equipment without voiding the listing and or warranty. The other solution would be to use a very low power device with a battery and change it once a year. This is going to be the route I go. It just complicates the programming and limits the amount of data that can be shared.

    Could tap the 480 AC in the equipment disconnect but that would require 600V fuses and at least 2 different steps to get down to 3.3 volt range, at least with the power supplies that are UL listed and regularly available to me.

    Thanks for your reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to PPE_COOP

    Battery-powered has significant advantages too, that may make it cheaper and simpler overall. It's one of the most popular methods currently, so it's definitely worth considering for your application if possible.

    Separating conductors for inductive transfer will need electrically qualified personnel to install, which costs a lot more. Also battery-powered devices can be fitted at the optimal location for the sensor (which might not be close to wires) or for best wireless coverage.

    Lots of battery-powered wireless sensors advertise 10-year battery life nowadays, and can be replaced at a frequency that isn't too different from replacement or repair/maintenance of other sorts of equipment.

    Granted there may be specialist circumstances where sensors are being deployed in extremely inaccessible locations, for which perhaps that TI solution could be suitable. Transmitting a lot of data in the type of environment you mention may also need a wired or inductive solution, e.g. continuous logging perhaps.