Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum POWER FOR SOLENOID VALVE
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 35 replies
  • Subscribers 331 subscribers
  • Views 6528 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

POWER FOR SOLENOID VALVE

Afiq
Afiq over 2 years ago

When 36W supply to specification 16W solenoid valve normally open, is there is effect to the solenoid valve?

  • Sign in to reply
  • Cancel

Top Replies

  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Afiq +5
    your valve works with 230V AC, it will not work (to specification, if at all) with a 24V power supply
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Andrew J +4
    Maybe ordered the wrong one? There is a 24 V version:
  • michaelkellett
    michaelkellett over 2 years ago in reply to shabaz +3
    The article is a bit misleading since it refers to inrush current when it means current when the solenoid armature is extended out of the coil. It may common to describe it this way but it's not that helpful…
Parents
  • robogary
    0 robogary over 2 years ago

    Solenoids are inductors. There is a holding current (power) and inrush current.

    The power supply needs to match the required voltage of the solenoid, provide the holding current, and also stay reasonably stiff to maintain voltage during short inrush current.

    It depends on the solenoid inrush current whether the 36w power source has enough power to survive turning on. A capacitor across the power supply can help provide extra energy during the inrush when the solenoid is turned on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to robogary

    Holding current is actually higher than initial current for a solenoid, since the solenoid appears like an inductor. It's not the same as (say) a DC motor, which will have a higher initial (inrush) current (unless it's stalled).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 2 years ago in reply to kmikemoo

    They do create counter EMF each time they move.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Afiq
    0 Afiq over 2 years ago in reply to anniel747

    image    This is my solenoid valve voltage rating

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anthocyanina
    0 Anthocyanina over 2 years ago in reply to Afiq

    your valve works with 230V AC, it will not work (to specification, if at all) with a 24V power supply

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Afiq

    And you could make yourself a science experiment to see why this is the case. Get an electromagnet (any electromagnet, could be a relay coil, or a spool of wire) and by applying different voltages, try to approximately see what difference in force you're seeing. Try half the voltage, then a quarter of the voltage, and then a tenth of the voltage. What you'll  observe will make it very clear.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Afiq
    0 Afiq over 2 years ago in reply to shabaz

    shabaz to be clear can you emphasize me the causes of solenoid valve not function when testing? Can you advise me the solution to these problems/causes?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Afiq

    The electronic portion (assuming it is a solenoid version and not a motor) is just a coil of wire, so ordinarily that could outlast a lifetime, although the winding can get damaged. You can do a very basic, very partial test by checking with a multimeter to see if it has gone open circuit. Other than that, the item is mechanical, so there can be plenty of mechanical problems (accidentally knocked plunger, stuck plunger due to dirt, etc. 

    Since it is a gas safety valve, it's best to replace it with a new modern one. Otherwise, if it ever fails and there is damage or someone is injured, the person that repaired and re-installed it will be the one that will be imprisoned.

    Obviously that's an expensive part, but if you're just looking to experiment with a solenoid valve (and don't intend to install it in it's normally intended application) you can get plenty of small low-voltage (e.g. 24V) devices for very little cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Afiq
    0 Afiq over 2 years ago in reply to shabaz

    Is it possible to fix and repair the plunger that being dirty or rusting? Because when there have gone open circuit, the voltage and Amp is enough, and have supplied but the solenoid valve cant trigger to close valve. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Afiq

    Personally I think no, it should be thrown away in a condition that no-one repairs it. I know there's a strong desire to repair and re-use, but in a critical application the $100 is not worth the risk to lives (and there would be a high risk). Everyone knows of gas explosion stories in their own towns or neighbourhoods, so it's not rare for things to go badly wrong. This would increase the risk a lot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Afiq
    0 Afiq over 2 years ago in reply to shabaz

    Our solenoid valve rating voltage and power is specification 24VDC and 18W. The solenoid valve(normally open) we tested was supply with 24VDC, after connect with the coil, the voltage was drop to 7VDC. Why this happen and what is advise to these problem? Is this power source need to continuously supply 24VDC into the solenoid valve?

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to Afiq

    Afiq You have overloaded your 24V power source.  The solenoid that you have provided a picture of, as Anthocyanina stated, is made to be powered with 230V AC.  Using a lower voltage source will not provide sufficient power to create the magnetism required to move the plunger.  Also, if the coil is made for AC and not DC, putting DC into it will also not provide sufficient power to create the magnetism required to move the plunger.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to Afiq

    Afiq You have overloaded your 24V power source.  The solenoid that you have provided a picture of, as Anthocyanina stated, is made to be powered with 230V AC.  Using a lower voltage source will not provide sufficient power to create the magnetism required to move the plunger.  Also, if the coil is made for AC and not DC, putting DC into it will also not provide sufficient power to create the magnetism required to move the plunger.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Afiq
    0 Afiq over 2 years ago in reply to kmikemoo

    Alright. Well note kmikemoo . I get your point.