Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Timeout Error when Reading Measurements from Impedance Analyzer Solartron 1260 via NI MAX using IEEE 488/GPIB
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 333 subscribers
  • Views 5427 views
  • Users 0 members are here
  • PCIB
  • NIMax
  • impedance analyzer
  • read error
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Timeout Error when Reading Measurements from Impedance Analyzer Solartron 1260 via NI MAX using IEEE 488/GPIB

Abdul
Abdul over 2 years ago

Hi, 

 I'm working with a Solartron A1260 Impedance/Gain-Phase Analyzer and attempting to read measurements on the NI MAX interface connected through a PCI bus. The analyzer itself is functioning correctly and can receive "Write" commands, as you can see the measurements on blue screen, but when I try to "Read" these measurements using NI MAX, I encounter a timeout error, as illustrated in the attached screenshot.The only command I can read is `*IDN? `. but my goal is to "Read" that simple measurement data of impedance analyzer on NI MAX interface.

I have tried adjusting the timeout/Bytes settings and reviewing the connection, but the issue persists. It seems like the main challenge is that I'm not sure about the correct commands to read the measurement data. Here are the details of my setup:


- Device Model: Solartron 1260 Impedance/Gain-Phase Analyzer
- Connection: Interface through PCIB
- Software: NI MAX
- Issue: Timeout error EABO during GPIB read operation

- Troubleshooting Steps: Adjusted timeout settings, adjusted bytes, changed addresses, checked GPIB command syntax, changed GPIB

 I would greatly appreciate any advice on the proper GPIB commands for reading measurements from a Solartron 1260 or any troubleshooting steps that might resolve this timeout error.

Thank you in advance for your help!

image

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • Abdul
    Abdul over 2 years ago +4
    Subject: Successful Update: Command Reading on NI MAX Interface Achieved! Dear Element14 Community, I have successfully configured the NI MAX interface to read commands from the impedance analyzer…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz +3
    I read the paper. Very useful to learn / understand a working conversation for this brand. Warning to Abdul , at the end of the paper, the writer explains how one of his scripts damaged the instrument…
  • shabaz
    shabaz over 2 years ago +2
    You could also check for code for other Solartron products of that era, in case you can spot any difference. For instance, a student used a 1260A here: https://www.slideshare.net/JosephHaystead/enel301…
Parents
  • shabaz
    0 shabaz over 2 years ago

    You could also check for code for other Solartron products of that era, in case you can spot any difference.

    For instance, a student used a 1260A here: https://www.slideshare.net/JosephHaystead/enel301-report-joseph-haystead1132999

    The Python code is in his report:

    image

    His code uses this terminator (but looks like there may be DIP switches etc on the instrument to set it?):

    image

    And this timeout:

    image

    Then he wrote a load of commands to set up the instrument, before doing the sweep:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to shabaz

    I read the paper. Very useful to learn / understand a working conversation for this brand.

    Warning to   Abdul , at the end of the paper, the writer explains how one of his scripts damaged the instrument permanently. He indicates what part may have caused this. Read it well before taking over the sources.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Jan Cumps

    Wow. That would be awful if that happened. It looks like a really nice instrument.

    I have a very old Keithley multimeter that I hardly power up, because although it works great so far, I'm worried that it has those RIFA capacitors inside, and possibly other dried out capacitors too. Need to spend time pulling it apart, but it's been at the back of the list for a good couple of years. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Abdul
    0 Abdul over 2 years ago in reply to Jan Cumps

    Dear Jan, could you please share the link of paper or any reference? Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Abdul

    Jan's referring to that uni paper slideshare.net link, where you can scroll down to read each page, but not downloadable without a lot of effort and possibly a subscription.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Abdul
    0 Abdul over 2 years ago in reply to shabaz

    aa OK..Thank you 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Abdul
    0 Abdul over 2 years ago in reply to shabaz

    aa OK..Thank you