Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum i want to build a circuit that expands dc range
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 335 subscribers
  • Views 1665 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

i want to build a circuit that expands dc range

acdc90
acdc90 over 2 years ago

Hello

most of the time i repair stuff. so not used to designing 

the input to this circuit min=0.48v max=2.5v

i want to expand the output to min=0 max =2.5v

this is for a anilog input and power supply of 5v

if i needed to generate a negative rail i could just use dc-dc module 

as it would only be a 1 off i would just use vero board and DIL ic  

    thank for looking  

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to acdc90 +3
    Unfortunately, this still needs a lot more information. Unless you're fully open about the actual use-case, and provide as much detail as possible about what this is for, it's near-impossible to help.…
  • michaelkellett
    michaelkellett over 2 years ago +1
    There are lots of ways this could be done but none are perfect. You need to tell us what the source of the signal is and where its going. The more you explain the context the better the answer you will…
Parents
  • dang74
    0 dang74 over 2 years ago

    The way I interpret your setup is as follows:

    You are using a circuit to calibrate a DAQ instrument.

    Ideally you would like this 'stimulus circuit' to operate from 0V to 2.5V.

    Unfortunately instead of 0V, the stimulus circuit only goes down to 0.48V.

    My comments:

    If your stimulus circuit has an op-amp  ensure that it is a rail to rail type, or look to using a negative rail as you suggest in your later post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dang74
    0 dang74 over 2 years ago

    The way I interpret your setup is as follows:

    You are using a circuit to calibrate a DAQ instrument.

    Ideally you would like this 'stimulus circuit' to operate from 0V to 2.5V.

    Unfortunately instead of 0V, the stimulus circuit only goes down to 0.48V.

    My comments:

    If your stimulus circuit has an op-amp  ensure that it is a rail to rail type, or look to using a negative rail as you suggest in your later post.