Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum UKCA (or CE) marking required for LED ceiling lamps?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 34 replies
  • Subscribers 333 subscribers
  • Views 8014 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

UKCA (or CE) marking required for LED ceiling lamps?

Andrew J
Andrew J over 2 years ago

One for the sparkys here in the UK: does an LED ceiling lamp sold in the UK market require a UKCA (or CE) marking?  Any other marking to show regulatory compliance, if necessary?

I ask, because I have received a LED ceiling lamp that has 7 arms with LEDs in a round metal holder at the ends.  It is intended for direct connection to the 240V lighting circuit with the full voltage going to each metal holder at the end of the arms (no earthing point in those metal holders.)

The ceiling rose is also metal, has no earthing point, has 30AWG (or close) out to the LED holders intended to be connected to supplied (but not fitted) slightly thicker wires which then need to be connected to the lighting circuit.  Frankly, it looks dangerous to me and I'm not installing it; really I ought to have known better but there you go, impulse purchase.

I'm going to push for money back and wanted to know if a lack of regulatory marking was something I could add to the evidence.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Andrew J +4
    Offer it to the altar of the god of unsafe UK appliances: https://www.bigclive.com/
  • Jan Cumps
    Jan Cumps over 2 years ago +2
    Not going to comment on UK standards, but on the safety and grounding expectations: Does it have this symbol for double isolation on it? That would define that it's supposed to be wired without ground…
  • Andrew J
    Andrew J over 2 years ago in reply to Jan Cumps +2
    If they don't send me a return label perhaps I will
Parents
  • shabaz
    0 shabaz over 2 years ago

    I've not been following the latest, but I think UKCA might be (or becoming) unessential now, provided the CE mark is there. All a mess. But for sure there should be either CE or UKCA on it, if not both. But I don't have a reference you could point them to : (

    We use 5-arm ceiling fixtures, but went with retro-fit, i.e. each stem has an Edison E14 socket on the fixture.

    Now big problem with that, is that the LED bulbs with E14, are not as good as LED bulbs with E27. Simply because there's more space for electronics+cooling with E27.

    But the traditional multi-arm fixtures are more commonly E14. The solution there was to insert in E27-to-E14 adapters. They don't look too bad, although obviously the bulb will protrude from the fixture slightly.

    The adapters that we used came from cp-lighting.co.uk (they seem reasonable, nothing spectacular).

    image

    EDIT: Hm, those adapters are out of stock. But I'm sure there must be other manufacturers of those. 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to shabaz

    They’ve used SMD LEDs.  By popular demand, here’s a couple of photos.  I would have to find a safe way to connect those tiny wires to mains circuit wires - there’s a small number of those dunce cap type connectors included and presumably I’m supposed to connect 7 pairs of these to mains wiring in one cap.  The chips are unmarked and there are no parts on the back of that card.  I don’t trust any of this to stick it on a downstairs ceiling underneath our bedroom.  To be fair, I wouldn’t put it up anywhere.

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to beacon_dave

    Great discussion for a Friday. Relaxed

     beacon_dave Every light fixture that I can remember installing has much smaller wires than the circuit that it gets connected to.  With as small as that wire is, it would probably act as its own fusible link.  If we really think about it, everything we plug into a wall outlet suffers the same risk.  Most power cords are 18AWG or 16AWG.  Even my (now defunct) dehumidifier only had a 14AWG cord.

     Jan Cumps It is the same in the US.  Even the high voltage lighting (277v or 480v) never contains an internal fuse.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to kmikemoo
    kmikemoo said:
    With as small as that wire is, it would probably act as its own fusible link.

    It likely depends on the nature of the fault. If it's dead short then most likely. But what if the fault draws a current that isn't enough to trip the fuse/breaker at the consumer unit but still enough to cause the smaller conductors to go red hot and start melting their way through the insulation. If that isn't contained, e.g. flex across carpet, wood floor, soft goods etc. then you end up with a fire starter situation.    

    kmikemoo said:
    If we really think about it, everything we plug into a wall outlet suffers the same risk.

    Here in the UK the plug that is inserted into the wall outlet has its own fuse which usually is rated a such that it protects the flex to the appliance it is supplying.

    I think Big Clive did some flex fire starter cable scenarios on his YouTube channel. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to kmikemoo

    I don't ever recall installing a mains-supplied device that had wire that thin though.  Yes, perhaps 18AWG, maybe even 22AWG.  But the gauges you mention can all carry a good amount of current.  I'd made an assumption that the 12W in the letter codes printed on the PCB actually referred to 12 watts, and thus a current consumption of around 50mA but I don't care, the wires shouldn't be that thin for a mains connection.  I don't know if there's likely to be an issue with inrush current or not.  

    In this case, nothing is connected up at all, so the purchaser/installer would need to go to town with ferrules and connector blocks and earthing.  It's not right, and I bet the regs have something to say about that for a domestic appliance/fitting. the fact that there's been no attempt at regulatory conformance makes me concerned enough not to use this thing.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to kmikemoo
    kmikemoo said:
    Great discussion for a Friday.

    This is not the video I was thinking of but seeing as it is Friday and well, it's Big Clive...

    Cable test ends in flames: 
    https://www.youtube.com/watch?v=gwwiCftM4Qg

    All the usual questions included...

    "is it going to burst into flames ?"

    "Should I have a fire extinguisher handy for this ?"

    "I'm regretting doing this on the bench..."

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Andrew J

    As an experiment, It's worth cutting some recent IEC power cables.

    When I get a device that comes with a set of IEC cables for several regions, I usually cut one of those that's not for my area. There is regularly not a lot of wire in there. And the wire isn't always copper or copperish anymore.
    But they look and feel thick and strong from the outside.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to Jan Cumps

    If you get a UK 13A plug from a 'questionable source', then its always worth cracking open the supplied ceramic fuse as loads are counterfeit. Amongst other things, there should be quartz sand inside them, which the counterfeits usually don't bother with.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 2 years ago in reply to Jan Cumps

    Lots of plastic and some CCA wire is the norm nowadays.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to Jan Cumps

    Yes I know.  I once purchased a 24V power brick from Amazon and the output wires were not much better than those above and it was rated at 3A!!  Recently wired up an IEC cable to use at the museum and its wires were fine for the 10A it is rated for.  I guess really it doesn't matter if others do it and get away with it, nobody should be doing it! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to Jan Cumps

    John Ward's YouTube channel has interesting experiments with suspect power cables:

    C5 Power Lead Destroyed
    https://www.youtube.com/watch?v=rfU5lzXAHAQ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to beacon_dave

     beacon_dave That is FANTASTIC!!! LaughingJoy  I love Big Clive.  Thank you for sharing that.  I may have to watch that video clip a few more times over the weekend.

    In the US, our plugs have no overcurrent protection built in - except for some of the Christmas (fairy) lights.  Now I'm wishing that I hadn't thrown out the UK plugs that I got with a few pieces of test equipment.

    I've cut apart a bunch of IEC cables as the jackets don't always stay in the molded plugs.  I agree that there is not a lot of conductor in there.  If it's the female end that fails and there's at least 1.5mm² conductor, it might get used for a power pigtail.  Any smaller and it gets cut again and recycled.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to beacon_dave

     beacon_dave That is FANTASTIC!!! LaughingJoy  I love Big Clive.  Thank you for sharing that.  I may have to watch that video clip a few more times over the weekend.

    In the US, our plugs have no overcurrent protection built in - except for some of the Christmas (fairy) lights.  Now I'm wishing that I hadn't thrown out the UK plugs that I got with a few pieces of test equipment.

    I've cut apart a bunch of IEC cables as the jackets don't always stay in the molded plugs.  I agree that there is not a lot of conductor in there.  If it's the female end that fails and there's at least 1.5mm² conductor, it might get used for a power pigtail.  Any smaller and it gets cut again and recycled.