Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum TENMA 72-13360 , dynamic mode
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 334 subscribers
  • Views 1526 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

TENMA 72-13360 , dynamic mode

azad_123
azad_123 over 1 year ago

I  purchased TENMA 72-13360 programmable Dc source, actually my requirement is to change Dc voltage from one level to different level. i am trying it in dynamic mode that is available in the option, but i couldn't achieve it, instead of step change in Dc supply i'm getting ramp change, i am unable to give dynamic number and dynamic step to achieve sudden change in the voltage level. how to set slope to get step change, can any one please help me , it is very urgent for my research work 

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 1 year ago +2 verified
    What edge time do you need for your tests? Power supplies are typically specialised in keeping steady power. Their output capacity makes that they aren't fast voltage jumpers. You may have to use a…
  • michaelkellett
    michaelkellett over 1 year ago in reply to azad_123 +2
    You can control this power supply via PC serial port or network connection. You can use any programming language you like but unless you have deep pockets you will need to write your own software. …
  • michaelkellett
    michaelkellett over 1 year ago +1
    You may have made a mistake in choosing this power supply. It's cheap but very loosely specified. They give no data on rise and fall time for a change in demand. Could you explain what waveforms you…
Parents
  • michaelkellett
    0 michaelkellett over 1 year ago

    You may have made a mistake in choosing this power supply. It's cheap but very loosely specified. They give no data on rise and fall time for a change in demand.

    Could you explain what waveforms you are trying to achieve and the purpose of them and maybe some kind of work around will be possible. Remember that the supply is a singe quadrant type (can only source current and not sink it) so the fall times with light loads will be poor.

    Are you using remote control and the VSTEP command ?

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • azad_123
    0 azad_123 over 1 year ago in reply to michaelkellett

    I didn’t use remote control. What software is required for that ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • azad_123
    0 azad_123 over 1 year ago in reply to michaelkellett

    I didn’t use remote control. What software is required for that ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 1 year ago in reply to azad_123

    You can control this power supply via PC serial port or network connection.

    You can use any programming language you like but unless you have deep pockets you will need to write your own software.

    There are code examples on the web using Python.

    I don't have one of these power supplies so I can't experiment but I think you should be able to enter more steps.

    The instructions in the user manual are very unclear - how do you set the time between steps ?

    For a pulse such as you want I would expect more steps,

    t0, 15V

    t1, 15V  (t1 - 10) about 1 second

    t2, 18V (t2 - t1) as short a time as possible.

    t3, 18V(t3 - t2) about 1 second

    t4, 15V (t4 - t3) as short a time as possible)

    and so on

    But typically power supplies like this will not be fast enough to test your booster properly.

    You can learn a great deal about your booster supply by applying fast load steps which are much easier to manage.

    The other key tool is simulation - if you simulate the booster and compare the simulated load response with reality and get a good match, then you can be fairly confident that the simulation will also be good for an input step.

    I have never tested a booster for fast input steps - difficult conditions (like engine cranking across a car 12V supply) have big voltage swings but low rates of change. If you have a decent sized input capacitor (not always possible) then fast step changes on the input don't happen. Special testers are available to apply fast input pulses and transients but it is usual to hire them rather than buy if you have a tight budget.

    Good luck.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • azad_123
    0 azad_123 over 1 year ago in reply to michaelkellett

    By using manual 

    Iam first setting M1=20V

    the. Pressing knob giving slope value =20

    time 3seconds

    and closing M1

    and now Turning on M2 

    giving M2 =30V 

    pressing knob giving slope value =20

    time 3 seconds 

    Then dynamic number =5

    step number =2 

    this is how Iam giving 


    my doubt is what should be the slope value and time value to be given .

    To get step change 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 1 year ago in reply to azad_123

    What happens if you set the slope value to 0 or 1 ?

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer