Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Cheap Alternatives to Flex Sensors for Gesture Glove Project
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 336 subscribers
  • Views 1224 views
  • Users 0 members are here
  • needed
  • Reply
  • Plzzz
  • fast
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Cheap Alternatives to Flex Sensors for Gesture Glove Project

Aniket_kumar_raj
Aniket_kumar_raj 6 months ago

Remember when I asked about a material for a glove that can detect finger movement? The best answer I got was magnet-type stuff, but that’s actually not cheap. I tried going for flex sensors, but getting 5 flex sensors is out of budget for my school science exhibition team. I decided to try Velostat, but I’m not sure if it will work.

What do you guys recommend? Also, what can I add to make this a killer, jaw-dropping project? This is my last school project where I can really flex my tech skills (or maybe our team’s tech skills Smile).

The exhibition is on the 28th, but my team is kind of lazy, and shipping takes too long for these things. It’s for National Science Day, so I really want this to be amazing. Please help me make this project next-level!

Also, if you have any other cool ideas (even unrelated ones), feel free to suggest them. The idea hasn’t been finalised yet.

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton 6 months ago +3
    Hey Aniket_kumar_raj , I've done a little edit to your message that might get a bit more input for you, and moved it to a forum more suited for your question - hopefully you'll receive some suggestions…
  • shabaz
    shabaz 6 months ago in reply to Aniket_kumar_raj +3
    You need a project plan, and at some stage you need to have completed some research, then come up with a potential design that won't stretch your entire plan beyond its end date (i.e. keep perspective…
  • cstanton
    cstanton 6 months ago in reply to shabaz +2
    shabaz said: I'd move the goal and detect different objects rather than grips, or detect grips by picking up different objects. For instance, conductors on the forefinger and thumb, each connected to one…
Parents
  • shabaz
    0 shabaz 6 months ago

    I can't see how you can realistically do anything if the budget is so tight, and you've got 19 days to order, prototype, and prepare a demo. This is called leaving it too late (you and your team have only yourselves to blame; don't think you should entirely blame the team, since you're involved too).

    Instead of five sensors, you could reduce effort and cost by fivefold by converting the project to a gesture mitt that senses only one movement.

    You didn't state the aim, but if it were me on such a timeframe, I'd move the goal and detect different objects rather than grips, or detect grips by picking up different objects. For instance, conductors on the forefinger and thumb, each connected to one end of an ohmmeter, or to a microcontroller ADC. Then, have cubes with two conductive surfaces on opposite sides, wired internally with a known-value resistor. When you pick up an object, the circuit completes, and the ohmmeter will register a measurement. Cubes with different resistors will all be distinguishable from one another.

    You could also experiment with trying to make cubes that vary resistance the harder they are pressed, but that could be a phase two.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton 6 months ago in reply to shabaz
    shabaz said:
    I'd move the goal and detect different objects rather than grips, or detect grips by picking up different objects. For instance, conductors on the forefinger and thumb, each connected to one end of an ohmmeter, or to a microcontroller ADC. Then, have cubes with two conductive surfaces on opposite sides,

    I'm thinking "what would be the utmost minimal viable product?" in a project like this, and to me that would be "switches stuck to a glove with wires" and then identifying which switches they are, then you change to it being 'gesture' based at the touch points (index finger to thumb, for example, or little finger to thumb) and if two switches are pressed together at the same time, you have a proof of concept that requires very little to work, maybe some wires and a light bulb to say "this represents a circuit, with budget this could give a signal" and then you're talking about what you could do.

    Difficult to determine without knowing what parts are available for sure.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cstanton
    0 cstanton 6 months ago in reply to shabaz
    shabaz said:
    I'd move the goal and detect different objects rather than grips, or detect grips by picking up different objects. For instance, conductors on the forefinger and thumb, each connected to one end of an ohmmeter, or to a microcontroller ADC. Then, have cubes with two conductive surfaces on opposite sides,

    I'm thinking "what would be the utmost minimal viable product?" in a project like this, and to me that would be "switches stuck to a glove with wires" and then identifying which switches they are, then you change to it being 'gesture' based at the touch points (index finger to thumb, for example, or little finger to thumb) and if two switches are pressed together at the same time, you have a proof of concept that requires very little to work, maybe some wires and a light bulb to say "this represents a circuit, with budget this could give a signal" and then you're talking about what you could do.

    Difficult to determine without knowing what parts are available for sure.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz 6 months ago in reply to cstanton

    That's a good idea; simpler and provides something easy to demo, and unlikely to go wrong on the day.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave 6 months ago in reply to cstanton

    If using Velostat, them perhaps switch from gloves to socks.

    Aim for sensor pad areas below the heel, the ball, and the toe where you typically have control of pressure over. Typically there will be two feet, so six analogue sensor inputs.

    Then come up with multiple interesting use cases for a foot-based controller. 

    Add sound and light to attract attention to your project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Aniket_kumar_raj
    0 Aniket_kumar_raj 6 months ago in reply to beacon_dave

    Bro u got the winning point I was trying to say, add something to make it attract attention. Love the idea , but adding it under foot could be paining,I mean I can't move my foot too much up and down continuously, Any Ideas that you have that's very unrelated but attracts attention

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave 6 months ago in reply to Aniket_kumar_raj

    Perhaps try standing - easier to change pressure under different parts of your foot when standing. 

    Connect it to lengths of pixel LEDs and/or a synth as a wearable and start walking/dancing.

    Perhaps think 'Big' with pressure pads and visual and audible feedback.

    https://www.youtube.com/watch?v=CF7-rz9nIn4

    Could create a two-player game paddle controller and connect to RetroPie. People like interacting with stuff.

    Turn it into a Wii Fit type balance board controller and use the XY data to create generative art.

    Recreate a science type experiment showing how the properties of Velostat could be used in STEM subjects.