Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum ERSA soldering iron tip suddenly un-tinnable
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 336 subscribers
  • Views 882 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

ERSA soldering iron tip suddenly un-tinnable

davebullockmbe
davebullockmbe 4 months ago

Hi I have an ERSA I-CON PICO solder station that has served me really well for several years when suddenly the 'pencil' tip has become un-tinnable.
It is the :-

://uk.farnell.com/ersa/0102pdlf04-sb/tip-soldering-iron-pencil-0-4mm/dp/1203967

A 0.4mm pencil tip which is great for getting into solder the tiny legs of SMD IC's.
I had used ERSA Digital 2000A's for years and years and then bought two of the I-Con Pico's (one for me and one for my son) a few years ago as we are both into SMD development and assembly.
I have never had a problem with the tip of the iron until recently when I just couldn't get the very tip of the bit to accept solder.
The solder station is not used on a daily basis (hobby use only) and is only switched on when required, I always use the supplied brass (Brillo pad) tip cleaner and this has kept the tip clean and operational until now.
Inspecting the tip I can see that it is still sharp with no visible pitting or corrosion, however it has a grey appearance instead of a 'silver' tinned area right at the tip.
I imagine that these tips have a special coating and shouldn't have anything abrasive applied (sandpaper/file etc) so I am wondering if the tip can be easily restored, or has it reached the end of it's life??
Any suggestions would be gratefully received, as both solder stations are suffering the same problem.

Thanks ...Daveimage

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 4 months ago +3
    I think that you have to treat the tip as having reached the end of its life. I have used tip cleaner (sort of waxy stuff in a little pot) but the effect doesn't last long). MK
  • Jan Cumps
    Jan Cumps 4 months ago in reply to phoenixcomm +2
    phoenixcomm said: did you read the NASA spec. only sponges For earth-bound projects, there's the IPC standard. " IPC advises in the IPC-7711/7721 that especially in lead-free soldering it is better…
  • Jan Cumps
    Jan Cumps 4 months ago +2
    I have used these products to revive tip wetting issues: They aren't general maintenance solutions. Intended to recover what otherwise would be a throwaway.
Parents
  • shabaz
    0 shabaz 4 months ago

    In my subjective opinion 0.4 mm pointy tips are easy to irreversibly destroy when they are hot and the point is tapped against a hard surface.

    I use a non-pointy, 1 mm bevel (i.e. sloped) tip for SMD down to 0.65 mm pitch parts such as TSSOP.

    Sometimes it helps to use an even bigger tip (e.g. spoon), and also relying on flux to make the solder easily float around and cling to metal without bridges across pins being formed.

    At 0.4 mm pitch parts (like QFN) I often switch to reflow tools (in my case, preheater+hot air) but still feasible with a soldering iron and even with large tips and flux. A very fine pointy tip could be used there, but personally I wouldn't keep it regularly attached to my soldering iron; the very fine pointy tips still have their uses, but more niche purposes I feel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz 4 months ago

    In my subjective opinion 0.4 mm pointy tips are easy to irreversibly destroy when they are hot and the point is tapped against a hard surface.

    I use a non-pointy, 1 mm bevel (i.e. sloped) tip for SMD down to 0.65 mm pitch parts such as TSSOP.

    Sometimes it helps to use an even bigger tip (e.g. spoon), and also relying on flux to make the solder easily float around and cling to metal without bridges across pins being formed.

    At 0.4 mm pitch parts (like QFN) I often switch to reflow tools (in my case, preheater+hot air) but still feasible with a soldering iron and even with large tips and flux. A very fine pointy tip could be used there, but personally I wouldn't keep it regularly attached to my soldering iron; the very fine pointy tips still have their uses, but more niche purposes I feel.