Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum CAN BUS to RS232/SPI converter
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 320 subscribers
  • Views 2902 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

CAN BUS to RS232/SPI converter

Former Member
Former Member over 9 years ago

Hello,

I am looking for low-cost CAN bus to RS232 or SPI converter. Do you have any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +1
    An MCP2515 from Microchip might do what you want. MCP2515T-I/ST MICROCHIP, CAN Bus, Controller, SPI, 3, 2, 2.7 V, 5.5 V, TSSOP, Newark element14 Canada MCP2515-I/P MICROCHIP, CAN Bus, Controller, SPI,…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    Try one of these

     

     

    CAN Interface IC | Products | Interface | TI.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Robert Peter Oakes

    These seem to be tranceivers. Is there one amongst them that offers conversion to RS232 or SPI?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to Jan Cumps

    Seeed and Sparkfun do CAN-BUS shields which would allow you to go from SPI to  RS-232RS-232 using an Arduino etc

     

    "The MCP2515 is a second generation stand-alone CAN controller. It is pin and function compatible with the MCP2510 and also includes upgraded features like faster throughput, databyte filtering, and support for time-triggered protocols."

    MCP2515 - Interface- Controller Area Network (CAN)

     

    • 18-pin package
    • Simple SPI interface to any MCU
    • One-shot mode ensures message transmission is attempted only once
    • Databyte filtering
    • Start-of-Frame (SOF) output
    • Low-power CMOS Technology
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 9 years ago in reply to Jan Cumps

    Seeed and Sparkfun do CAN-BUS shields which would allow you to go from SPI to  RS-232RS-232 using an Arduino etc

     

    "The MCP2515 is a second generation stand-alone CAN controller. It is pin and function compatible with the MCP2510 and also includes upgraded features like faster throughput, databyte filtering, and support for time-triggered protocols."

    MCP2515 - Interface- Controller Area Network (CAN)

     

    • 18-pin package
    • Simple SPI interface to any MCU
    • One-shot mode ensures message transmission is attempted only once
    • Databyte filtering
    • Start-of-Frame (SOF) output
    • Low-power CMOS Technology