Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for an oscilloscope / logic analyser, maybe usb?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 6 answers
  • Subscribers 336 subscribers
  • Views 726 views
  • Users 0 members are here
  • oscilloscope
  • logic analyser
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for an oscilloscope / logic analyser, maybe usb?

stanto
stanto 4 months ago

Anyone using a portable/handheld oscilloscope/logic analyzer?

Im looking for recommendations of something to pick up.

Ideally with capabilities to hook into python or coding libraries over USB too.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 4 months ago +9 suggested
    I quite like the Pico scopes. Sparked off by another thread I've just been comparing my 6242e (which I got from E14 in a RoadTest) and a 5444B which I bought myself (it's now superseded by the 5444d…
  • BigG
    BigG 4 months ago +5 suggested
    If you want a device that can hook into Python, I would suggest looking at the Analog Devices ADALM2000 device. https://developer.analog.com/docs/system-level/software/libm2k/index.html https://analogdevicesinc…
  • shabaz
    shabaz 4 months ago +4 suggested
    Hi! Portability is underrated; it allows one to capture signals more frequently, saving loads of time. I've noticed jancumps uses a handheld device, and it very successfully helps out for all sorts of…
Parents
  • kk99
    0 kk99 4 months ago

    I think it is worth taking a look at something from Digilent. I personally use AD3 for basic things. WaveForms is really great software that has ready-to-use components, e.g., Waveform Generator, Impedance Analyzer, Spectrum, or Supplies that could be modulated by the generator to simulate noise. There is also support for SDK. Here is an example of using the SDK to integrate the usage of some devices with ngscopeclient. Of course, the hardware is a bit limited if you're looking for something with a low-noise front end, but the series ADP3X50 or new ADP2440/2450 could be quite good. In that area I think that PicoScope gives more flexibility and better parameters. You can find hardware that has a fast sampling rate with large memory, like the Series 3000e or the latest 5000e series, where you can get a hybrid solution, native 16-bit, plus the same features from the 3000e.

    Here is similar as Michael measurement (1kHz sine 1V amplitude from AD3 generator) done with AD3:

    image
    image
    image
    And as a curiosity, output from Siglent SDS824X HD:
    image

    image

    image

    image

    I saw there is something like Saleae Logic MSO, their logic analyzers and software are really good, but the oscilloscope part, I suppose, is still in development and not mature as other solutions.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kk99
    0 kk99 4 months ago

    I think it is worth taking a look at something from Digilent. I personally use AD3 for basic things. WaveForms is really great software that has ready-to-use components, e.g., Waveform Generator, Impedance Analyzer, Spectrum, or Supplies that could be modulated by the generator to simulate noise. There is also support for SDK. Here is an example of using the SDK to integrate the usage of some devices with ngscopeclient. Of course, the hardware is a bit limited if you're looking for something with a low-noise front end, but the series ADP3X50 or new ADP2440/2450 could be quite good. In that area I think that PicoScope gives more flexibility and better parameters. You can find hardware that has a fast sampling rate with large memory, like the Series 3000e or the latest 5000e series, where you can get a hybrid solution, native 16-bit, plus the same features from the 3000e.

    Here is similar as Michael measurement (1kHz sine 1V amplitude from AD3 generator) done with AD3:

    image
    image
    image
    And as a curiosity, output from Siglent SDS824X HD:
    image

    image

    image

    image

    I saw there is something like Saleae Logic MSO, their logic analyzers and software are really good, but the oscilloscope part, I suppose, is still in development and not mature as other solutions.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer