Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the best way to drive a relay?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 339 subscribers
  • Views 8221 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the best way to drive a relay?

swankybarbecue4
swankybarbecue4 over 8 years ago

I want to use raspberry pi GPIO pins to control a few relays. I was planning to use a 3904 NPN transistor with a 330 ohm resistor on the base of the 3904 and a fly back diode across the coil of the relay (just as shown in the attached image). My questions are: would it be more efficient power consumption wise to drive the relay with an MOSFET or power resister? And will I destroy an NPN 3904 transistor over time if I use it in the circuit shown below? I see people using BC transistors (like a BC 141) instead of an NPN transistor like I described. image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +3
    Your circuit should work fine depending on the coil impedance. I prefer a MOSFET because they are more efficient - no wasted base current, less load on the digital output, and more voltage across the relay…
  • geralds
    geralds over 8 years ago +3
    Hi, This is often an important question, but not often really correctly answered. First you have see your application, e.g. which component you will drive. A relay normally is current driven by the given…
  • luislabmo
    luislabmo over 8 years ago +3
    I think before considering a final solution, you need to ask yourself what are exactly your needs, that way you can define what will work best for your specific scenario so, here my two cents: I agree…
Parents
  • dougw
    dougw over 8 years ago

    Your circuit should work fine depending on the coil impedance.

    I prefer a MOSFET because they are more efficient - no wasted base current, less load on the digital output, and more voltage across the relay.

    You just need to pick one with enough current capacity and a low enough turn on voltage.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 8 years ago

    Your circuit should work fine depending on the coil impedance.

    I prefer a MOSFET because they are more efficient - no wasted base current, less load on the digital output, and more voltage across the relay.

    You just need to pick one with enough current capacity and a low enough turn on voltage.

    • Cancel
    • Vote Up +3 Vote Down