Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the best way to drive a relay?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 339 subscribers
  • Views 8214 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the best way to drive a relay?

swankybarbecue4
swankybarbecue4 over 8 years ago

I want to use raspberry pi GPIO pins to control a few relays. I was planning to use a 3904 NPN transistor with a 330 ohm resistor on the base of the 3904 and a fly back diode across the coil of the relay (just as shown in the attached image). My questions are: would it be more efficient power consumption wise to drive the relay with an MOSFET or power resister? And will I destroy an NPN 3904 transistor over time if I use it in the circuit shown below? I see people using BC transistors (like a BC 141) instead of an NPN transistor like I described. image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +3
    Your circuit should work fine depending on the coil impedance. I prefer a MOSFET because they are more efficient - no wasted base current, less load on the digital output, and more voltage across the relay…
  • geralds
    geralds over 8 years ago +3
    Hi, This is often an important question, but not often really correctly answered. First you have see your application, e.g. which component you will drive. A relay normally is current driven by the given…
  • luislabmo
    luislabmo over 8 years ago +3
    I think before considering a final solution, you need to ask yourself what are exactly your needs, that way you can define what will work best for your specific scenario so, here my two cents: I agree…
  • shabaz
    shabaz over 8 years ago

    Hi Merrick,

     

    I see you've copied a diagram from some website, but if that website didn't help explain or provide you with some confidence that the circuit was a suitable way of doing things, then it isn't a very good website to use for learning. You're better off grabbing a couple of beginner books, because they will cover this. Please see the information (in the body of the post, and in the comments section) here: I Want to Do Electronics!  Where do I start?

     

    It will be far quicker than trying to explain the behaviour of a NPN transistor, or a MOSFET, or a power resistor. Also, you should just try it (with low voltage) to experiment with it. If you want to see example circuits connected to GPIO, check out this link, it has a relay circuit too, and you'll see it is similar to what you've shown in the diagram.

    Raspberry Pi GPIO Explained

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago

    Merrick,

     

    When it comes to switching a load (i.e. LED, relay, etc.) my go to part is a MOSFET.  For a long time I was afraid of the issues of static damage and I steered away for FETs in general for switches/drivers.  That being said, modern MOSFET are very reliable and in many way a far superior choice for driving loads.  With MOSFETs it is very possible to obtain parts with very little Source to Drain impedances (<10mOhms). With any amount of current flowing, impedance is your enemy.  Power dissipation in the MOSFET is determined by the voltage drop across the Source to Drain times the current flow.  Assuming that the load current is 500mA, a MOSFET with a Rds = 0.01 ohms would only generate a voltage drop of 5mV, or a power dissipation 2.5mW.  That is cool (i.e not hot).

     

    Although not a relay, here is a schematic snippet of a MOSFET being used as an LED driver:

    image

    Applying a positive signal (3.3V to 5.V) at R3 turns the MOSFET on,  with a low level signal (<1V) the MOSFET is off.

     

    High quality MOSFETs are fairly cheap and very reliable.

     

    Good Luck!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago

    Your circuit should work fine depending on the coil impedance.

    I prefer a MOSFET because they are more efficient - no wasted base current, less load on the digital output, and more voltage across the relay.

    You just need to pick one with enough current capacity and a low enough turn on voltage.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 8 years ago

    If replacing the transistor with a MOSFET don't forget to still include the flyback diode across the relay's coil (the MOSFET won't last long otherwise).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 8 years ago

    Hi,

     

    This is often an important question, but not often really correctly answered.

     

    First you have see your application, e.g. which component you will drive.
    A relay normally is current driven by the given voltage.
    A LED is current driven, have also a threshold voltage - the diode forward voltage.

    On the drivers sides - the NPN, or PNP (Si) have 0,7V threshold, they are current driven devices.
    A MOSFET normally is voltage driven, but have much more a gate - voltage threshold, nom. so about 2 ...4V with that the D-S channel goes open.
    But "newly" we also have a "logical-gate MOSFET". image

    With that devices you can come directly from an µC port.

    They can have a threshold about 0,7 .. to 1,5V G-S, then the D-S channel will open complete.

     

    Driving from logical ports, you have your given driving voltage also the current limit, the driver cannot more drive that he can. (SOAR !!!!! )

    So there are many driver schematics.

     

    For me i use often simple drivers.

    An NPN or PNP (is for logical inverters) with a few parts, done.
    Or an logical-gate MOSFET if i have to drive many current with an Controller port.
    Because a NPN, PNP (or similar, inverted) combination needs more devices as you can have space on your PCB for example.

     

    - So, a relay with the freewheeling diode, they both are married for ever, don't forget it !!!!


    Then you can select current driver, or voltage driver. Your application tells it for your needing.
    A high current, high voltage relay needs a power transistor to driving it.
    With bipolare transistors you must perhaps use darlington transistors as well.

     

    For a small relay also some LED indicators I'll suggest you use a simple driver with an NPN (there are many high current driver with very low C-E_on voltage).

    e.g. Zetex (Diode) are very high C-E voltage resistant.

    They have also logical-MOSFETs (mostly N-channel devices, because they are mostly used in logical circuits) with very low G-S threshold.

    e.g. ZVN4424A - DIODES INC. - MOSFET-Transistor, n-Kanal, 260 mA, 240 V, 6 ohm, 10 V, 1.3 V | Farnell AT

    A n-channel MOSFET with so 1,3V threshold G-S,  fine what you can use with your Raspberry.

     

    Or as SMD mounted device, this device is better for switching circuits, e.g. as  motor / relay driver, or in DC-DC converters.

    http://www.farnell.com/datasheets/2097784.pdf?_ga=2.109346752.437430279.1512899497-63280803.1512144825

     

    Some transistors.....MOSFETs.

    n-Kanal DIODES INC. MOSFET-Transistoren | Farnell AT

     

     

    Best Regards
    Gerald

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 8 years ago

    I think before considering a final solution, you need to ask yourself what are exactly your needs, that way you can define what will work best for your specific scenario so, here my two cents:

     

    • I agree with genebren and dougw, to drive an inductive load generally a Mosfet is better than a transistor. Here is a good guide on Relay switch circuits.
    • Is the relay going to remain ON for long periods? Then consider using a latching Relay and explore using a P-Channel or an N-Channel Mosfet.
    • You can keep improving your circuit, like adding an opto-coupler, and play with the circuit to turn-On/Off the relay using a high or low digital signal from your RPi.

     

    Other considerations:

    • Do you need the relay to turn on/off as fast as possible? then you will need to add few more components.
    • And yes, don't forget the flyback diode or you may fry your RPi.

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down