Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the best way to drive a relay?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 339 subscribers
  • Views 8221 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the best way to drive a relay?

swankybarbecue4
swankybarbecue4 over 8 years ago

I want to use raspberry pi GPIO pins to control a few relays. I was planning to use a 3904 NPN transistor with a 330 ohm resistor on the base of the 3904 and a fly back diode across the coil of the relay (just as shown in the attached image). My questions are: would it be more efficient power consumption wise to drive the relay with an MOSFET or power resister? And will I destroy an NPN 3904 transistor over time if I use it in the circuit shown below? I see people using BC transistors (like a BC 141) instead of an NPN transistor like I described. image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +3
    Your circuit should work fine depending on the coil impedance. I prefer a MOSFET because they are more efficient - no wasted base current, less load on the digital output, and more voltage across the relay…
  • geralds
    geralds over 8 years ago +3
    Hi, This is often an important question, but not often really correctly answered. First you have see your application, e.g. which component you will drive. A relay normally is current driven by the given…
  • luislabmo
    luislabmo over 8 years ago +3
    I think before considering a final solution, you need to ask yourself what are exactly your needs, that way you can define what will work best for your specific scenario so, here my two cents: I agree…
Parents
  • geralds
    geralds over 8 years ago

    Hi,

     

    This is often an important question, but not often really correctly answered.

     

    First you have see your application, e.g. which component you will drive.
    A relay normally is current driven by the given voltage.
    A LED is current driven, have also a threshold voltage - the diode forward voltage.

    On the drivers sides - the NPN, or PNP (Si) have 0,7V threshold, they are current driven devices.
    A MOSFET normally is voltage driven, but have much more a gate - voltage threshold, nom. so about 2 ...4V with that the D-S channel goes open.
    But "newly" we also have a "logical-gate MOSFET". image

    With that devices you can come directly from an µC port.

    They can have a threshold about 0,7 .. to 1,5V G-S, then the D-S channel will open complete.

     

    Driving from logical ports, you have your given driving voltage also the current limit, the driver cannot more drive that he can. (SOAR !!!!! )

    So there are many driver schematics.

     

    For me i use often simple drivers.

    An NPN or PNP (is for logical inverters) with a few parts, done.
    Or an logical-gate MOSFET if i have to drive many current with an Controller port.
    Because a NPN, PNP (or similar, inverted) combination needs more devices as you can have space on your PCB for example.

     

    - So, a relay with the freewheeling diode, they both are married for ever, don't forget it !!!!


    Then you can select current driver, or voltage driver. Your application tells it for your needing.
    A high current, high voltage relay needs a power transistor to driving it.
    With bipolare transistors you must perhaps use darlington transistors as well.

     

    For a small relay also some LED indicators I'll suggest you use a simple driver with an NPN (there are many high current driver with very low C-E_on voltage).

    e.g. Zetex (Diode) are very high C-E voltage resistant.

    They have also logical-MOSFETs (mostly N-channel devices, because they are mostly used in logical circuits) with very low G-S threshold.

    e.g. ZVN4424A - DIODES INC. - MOSFET-Transistor, n-Kanal, 260 mA, 240 V, 6 ohm, 10 V, 1.3 V | Farnell AT

    A n-channel MOSFET with so 1,3V threshold G-S,  fine what you can use with your Raspberry.

     

    Or as SMD mounted device, this device is better for switching circuits, e.g. as  motor / relay driver, or in DC-DC converters.

    http://www.farnell.com/datasheets/2097784.pdf?_ga=2.109346752.437430279.1512899497-63280803.1512144825

     

    Some transistors.....MOSFETs.

    n-Kanal DIODES INC. MOSFET-Transistoren | Farnell AT

     

     

    Best Regards
    Gerald

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 8 years ago

    Hi,

     

    This is often an important question, but not often really correctly answered.

     

    First you have see your application, e.g. which component you will drive.
    A relay normally is current driven by the given voltage.
    A LED is current driven, have also a threshold voltage - the diode forward voltage.

    On the drivers sides - the NPN, or PNP (Si) have 0,7V threshold, they are current driven devices.
    A MOSFET normally is voltage driven, but have much more a gate - voltage threshold, nom. so about 2 ...4V with that the D-S channel goes open.
    But "newly" we also have a "logical-gate MOSFET". image

    With that devices you can come directly from an µC port.

    They can have a threshold about 0,7 .. to 1,5V G-S, then the D-S channel will open complete.

     

    Driving from logical ports, you have your given driving voltage also the current limit, the driver cannot more drive that he can. (SOAR !!!!! )

    So there are many driver schematics.

     

    For me i use often simple drivers.

    An NPN or PNP (is for logical inverters) with a few parts, done.
    Or an logical-gate MOSFET if i have to drive many current with an Controller port.
    Because a NPN, PNP (or similar, inverted) combination needs more devices as you can have space on your PCB for example.

     

    - So, a relay with the freewheeling diode, they both are married for ever, don't forget it !!!!


    Then you can select current driver, or voltage driver. Your application tells it for your needing.
    A high current, high voltage relay needs a power transistor to driving it.
    With bipolare transistors you must perhaps use darlington transistors as well.

     

    For a small relay also some LED indicators I'll suggest you use a simple driver with an NPN (there are many high current driver with very low C-E_on voltage).

    e.g. Zetex (Diode) are very high C-E voltage resistant.

    They have also logical-MOSFETs (mostly N-channel devices, because they are mostly used in logical circuits) with very low G-S threshold.

    e.g. ZVN4424A - DIODES INC. - MOSFET-Transistor, n-Kanal, 260 mA, 240 V, 6 ohm, 10 V, 1.3 V | Farnell AT

    A n-channel MOSFET with so 1,3V threshold G-S,  fine what you can use with your Raspberry.

     

    Or as SMD mounted device, this device is better for switching circuits, e.g. as  motor / relay driver, or in DC-DC converters.

    http://www.farnell.com/datasheets/2097784.pdf?_ga=2.109346752.437430279.1512899497-63280803.1512144825

     

    Some transistors.....MOSFETs.

    n-Kanal DIODES INC. MOSFET-Transistoren | Farnell AT

     

     

    Best Regards
    Gerald

    • Cancel
    • Vote Up +3 Vote Down