FPGA
  • Technologies
  • More
FPGA
Forum USB keyboard decoder
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 4 answers
  • Subscribers 583 subscribers
  • Views 4371 views
  • Users 0 members are here
  • fpga
Related

USB keyboard decoder

ahmedmohamed85
ahmedmohamed85 over 6 years ago

Hi,

i have a project where i need to interface Artix7 FPGA, with usb keyboard, what is the best module or component to do this?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago in reply to ahmedmohamed85 +3 suggested
    I think the best quick and dirty way to do it is with something like this: https://www.hobbytronics.co.uk/usb-host-keyboard There are several such devices around, best look somewhere local to you, or maybe…
  • michaelkellett
    michaelkellett over 6 years ago in reply to ahmedmohamed85 +3 verified
    I don't see why not, PS/2 interface uses open collector drivers with the pull ups normally to 5V. If there are no pull ups in the keyboard and you don't want to talk back to the keyboard, you might be…
  • michaelkellett
    michaelkellett over 6 years ago +2 suggested
    You need to tell us a lot more about the project. Do you want to do this once, or for production. Do you care about cost. Is you FPGA on a board or will you be designing a board. Is this a task you have…
  • johnbeetem
    0 johnbeetem over 6 years ago

    This may be too late to be useful, but here's what I'd look into.

     

    Basically, you need to be a USB host to talk to a USB device like a keyboard.  USB hosts are pretty complex, which is why some people have suggested running Linux.  Personally, I think that's overkill.

     

    I would recommend checking into the Maxim MAX3421E "USB Peripheral/Host Controller with SPI Interface".  According to the description, this IC can be used as a USB peripheral or USB host, and should be a whole lot less work than implementing a USB host controller in an FPGA.

     

    Another possibility is a Microchip SAM D21, which is a small 32-bit microcontroller with a USB host/device interface.  This would require a lot of software, but that may already be available.

     

    You should be able to find a breakout/development board for either of those chips.

     

    I have not used either of those products myself.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<