Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed Hardware Design Zynq Z7020 on picozed fried during SW download
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 1839 views
  • Users 0 members are here
  • dead chip
  • soc
  • zynq 7000
  • avnet
  • xilinx
  • picozed
Related

Zynq Z7020 on picozed fried during SW download

mashedcorn
mashedcorn over 3 years ago
I purchased a picozed 7Z20 and made a custom carrier board for it.  I was able to power it on and get the FPGA DONE LED to light up, I was able to program the Zynq chip PL through VIVADO, and I was able to begin programming the PS through vitis.  towards the end of downloading my SW to the board I lost JTAG connection and I am afraid my Z720 chip is now dead, it gets instantly hot when powered on and draws around 3x the current it did when I first booted it up. 
 
the board had been on for a fair amount of time, 10 minutes of power cycling it while trying to get it set up on a test bench, probably 5 minutes of me setting up and downloading the PL firmware a couple of times, 20 minutes between then and trying the SW download.
 
I'm wondering if anyone might have any insight into what went wrong here, Is it possible for the chip to overheat and kill itself?, I don't have any heatsink or fan on the chip but I figured there was some built in thermal protection but maybe I'm wrong.  Otherwise, I'm not sure what might have happened if it was working fine. I doubt JTAG programming could fry the chip
  • Sign in to reply
  • Cancel
  • dang74
    0 dang74 over 3 years ago

    I hope your chip is still fine.  I don't have a lot of background on your specific problem.  However a couple of years ago I read through the the guide lines for designing a carrier board for the PicoZed.  I seem to remember that there was a very specific sequence for applying all the different power rails to the PicoZed.  Did you ensure that your carrier board respects the power sequencing requirements?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mashedcorn
    0 mashedcorn over 3 years ago in reply to dang74

    Yes I have a regulator for the VCCIO that only gets enabled once the power good signal comes from the module so power up should be respected, the rest of the boot up sequence is handled by the SOM. As I stated I was able to power up, it was detected, and I programed the board, the FPGA DONE light would light up correctly once booted. It is definitely dead as it gets too hot to touch very quickly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • saadtiwana_int
    0 saadtiwana_int over 3 years ago

    "Is it possible for the chip to overheat and kill itself?, I don't have any heatsink or fan on the chip.."

    I have used 7z020 in several designs, some rather large ones, without a heatsink and never had any issues so far. In vivado you can see the power report to get an estimate on your design's power consumption. My designs have had up to 2W of estimated power consumption as per the power report, and while the chip got hot it didn't get damaged. If your design is small and yet the actual power consumption is very high, then perhaps something else went wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 over 3 years ago in reply to mashedcorn

    I was trying to stay hopeful but you might be correct in assuming that the device was damaged.  So strange that things seemed to go south during the software load.  I am not really an AMD/Xilinx guy so I can't really pin point what could have gone wrong here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mashedcorn
    0 mashedcorn over 3 years ago in reply to saadtiwana_int

    Thanks for the info, I didn't know about this in Vivado, It says 1.8W for my design, When I first plugged in the board I was drawing around 600 mA at 5V so about 3W.

    After burning out the chip its drawing around 1.5A (although that might be the limit of the power supply).  I will have to check the power draw of the other peripherals on the 5V rail to see if 3W is suspicious. 

    I do have one of my connectors to the board bodged on so I will double check the traces I have cut and rerouted to make sure I didn't miss anything, the only thing that could be an issue are the VCCO and 5V rail connections as everything else is generic gpio for the PL or the programming lines and I know those work for sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • flyingbean
    0 flyingbean over 3 years ago

    Here is a quick answer for Zynq FPGA power rails. The power rail table was from TI design for Zyqn 7015(tidua66.pdf):

    image

    Zynq 7015 is similar to 7020 except the high speed bus at PS side.

    One tip to check whether the FPGA is dead or not if you cannot use JTAG: check FPGA temperature after powering it on. If FPGA temperature is blow 40~50C after power on and the PS does have proper clock input/power rails are fine, FPGA most likely is dead.