FPGA
  • Technologies
  • More
FPGA
Forum Xilinx Spartan-7 FPGA Maker Board by Digilent giveaway
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 586 subscribers
  • Views 4535 views
  • Users 0 members are here
  • arty s7
  • xilinx;
Related

Xilinx Spartan-7 FPGA Maker Board by Digilent giveaway

kk99
kk99 over 7 years ago

Hi,
I am after a review of Xilinx Spartan-7 FPGA board and now I am participating a the Path to Programmable training project. I would like to a give a Xilinx Arty S7 board from roadtest review for a person whose is interested to make a roadtest, project or would like to learn FPGA based this board. Please let me know in comments if you are interested.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to Fred27 +5
    I've spent some time this morning looking at the PSOC programmable logic in the light of several comments in E14 suggesting it as a low cost route into learning about FPGA. My conclusion is that it is…
  • johnbeetem
    johnbeetem over 7 years ago in reply to michaelkellett +4
    I did a lot of research into the PSoC 5 when it first came out. I was excited to see that almost all of configuration registers were documented, so that it would be possible to write my own design tools…
  • Fred27
    Fred27 over 7 years ago in reply to neuromodulator +3
    The CY8CKIT-049-42XX CY8CKIT-049-42XX is even cheaper although the ARM core is programmed via bootloader rather than a JTAG debugger I was planning to combine the CY8CKIT-049-42XX CY8CKIT-049-42XX andCY8CKIT…
  • johnbeetem
    johnbeetem over 7 years ago in reply to michaelkellett

    I did a lot of research into the PSoC 5 when it first came out.  I was excited to see that almost all of configuration registers were documented, so that it would be possible to write my own design tools.  I was then disappointed to find out that the routing registers were not documented, so you're pretty much limited to using PSoC Creator which requires using a Windows machine.  Ah well.

     

    I did see that PSoC 5 (and 4) are really quite marvellous chips, but I agree with Michael that they're really not FPGAs.  A PSoC 5 is like having a big breadboard with a bunch of PLAs, a bunch of bit-slice ALUs (actually byte-slice), analog components, and a reasonably powerful CPU well-integrated with the other devices, all smashed into a tiny chip.  It's a nifty device for playing with lots of different technologies provided that you're willing to tolerate Windows.

     

    The PLAs are reasonably powerful, but 48 PLAs is not the same as a proper FPGA with thousands of logic elements.  PLAs make dandy "glue logic", but you'll soon run out if doing a serious logic function.

     

    I still recommend iCE40 as a great starting FPGA and also as a solution when you need a relatively small FPGA.  You can get 1K gate parts in QFN, VQFP and TQFP packages.

     

    To David Murphy: I suggest downloading both the iCE40 data sheet and the PSoC 5LP architectural reference manual.  Read each one for one hour and see how far you get image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • anuag_ashim
    anuag_ashim over 7 years ago in reply to Fred27

    Sweet deal. I am also interested to learn about this kit

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gsgill112
    gsgill112 over 7 years ago

    Thats very generous of you kk99 .

     

    I have been since long trying to get my hands on an FPGA based board to learn FPGA programming. This looks like a very good opportunity.

     

    If you are still interested in giveaway I would be very interested to learn  image.

     

    Thanks again.

     

    Regards,

    GS Gill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kk99
    kk99 over 7 years ago

    Hi all,
    I will send the Xilinx Spartan-7 board to Fred27. We had talk via PM and he is still interested to try this cool board.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 7 years ago

    Thanks kk99 . I've also got some STM32 boards gathering dust. You've inspired me to find a useful home for them.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<