Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Researchers Develop Robotic Swarm That Acts Like a Smart Material

    Catwell
    Catwell
    These tiny disk-shaped robots work together to lift and manipulate objects or support weight. (Image Credit: Brian Long/UCSB) UC researchers sought inspiration from embryonic tissues to develop a swarm of robots that act like smart material. The dis...
    • 5 Mar 2025
  • This Device Could Put Out Fires Using Nothing But Low-Frequency Sound Waves

    Catwell
    Catwell
    Operating at 30-60 hertz, the sound extinguisher douses flames in just seconds. (Image Credit: George Mason University/YouTube) Back in 2015, two engineering students at George Mason University developed a fire extinguisher that puts out fires usin...
    • 26 Feb 2025
  • Researchers Turn to Nature to Develop Robotic Butterfly

    Catwell
    Catwell
    The robotic butterfly wings are actuated via magnetic fields and can perform precision movements without electronics or batteries. (Image credit: University of Darmstadt) German researchers from the Technical University of Darmstadt and the Helmholt...
    • 14 Feb 2025
  • Researchers Develop Drone with Bird-Like Legs

    Catwell
    Catwell
    The RAVEN drone features bird-inspired legs to help improve walking, jumping, take-off, and landing capabilities. (Image Credit: Alain Herzog) École Polytechnique Fédérale de Lausanne (EPFL) and UC Irvine researchers built RAVEN...
    • 18 Dec 2024
  • Ikea Kallax Insert with Door as DIN rail housing

    Jan Cumps
    Jan Cumps
    Ikea Kallax is a modular storage range. Used in houses and offices. I'm going to turn their "Insert With Door" into an industrial DIN plug-in. It will be able to hold automation and compute devices in an office-like environment. An i...
    • 23 Nov 2024
  • Robotic Arms Play The Cello For The First Time As Part of a Symphony Orchestra

    Catwell
    Catwell
    The cello-playing robot performed a piece composed by Jacob Muhlrad at the Malmö Live Concert Hall in Sweden (Image Credit: malmosymfoniorkester/Instagram) In a world-first, two industrial robotic arms played the cello with a symphony orchestr...
    • 22 Nov 2024
  • TEPCO Collected Melted Fuel Sample from the Fukushima Daiichi Nuclear Power Plant

    Catwell
    Catwell
    Penetration from the robotic telescope. (Image Credit: TEPCO) Telesco, a remote-controlled extendable robot, recently retrieved a small amount of melted fuel from a reactor at the Fukushima Daiichi nuclear power plant. According to the Tokyo Electri...
    • 8 Nov 2024
  • Robots Race in Micromouse Maze Competition

    Catwell
    Catwell
    The HAL900 micromouse robot participated in the APEC 2024 micromouse competition. (Image Credit: Micromouse/Youtube) Anyone else feel the need to compete in this? For years, competitors have participated in Micromouse events to build a small, autono...
    • 5 Nov 2024
  • Meet These Three Interesting Robots – a Conductor, Doctor and a Shark

    Catwell
    Catwell
    The MAiRA Pro S robot is an ensemble of three arms that conduct music. (Image Credit: David.Suenderhauf/Hellerau hall) Dresden, Germany, deployed MAiRA Pro S, a three-arm music conducting robot that acts like a human orchestra conductor. Recently, i...
    • 23 Oct 2024
  • Mushrooms on the Move: Mushroom Given Robot Body and Learns to Crawl

    Catwell
    Catwell
    The biohybrid robot uses the mushroom’s rhythmic voltage spikes to control its locomotion. (Image credit: Cornell University) It’s almost unbelievable. Researchers from Cornell University have placed a mushroom behind the controls of a r...
    • 10 Sep 2024
  • California Startup Comes Up with a New Way to Generate Power with Sunlight at Night

    Catwell
    Catwell
    Reflect Orbital tested its concept by fitting mylar mirrors on a hot air balloon that reflected sunlight on a moving truck. (Image Credit: Reflect Orbital) Fly by night, conceptual, viral, whatever the case may be, this idea is inspiring. It's ...
    • 3 Sep 2024
  • Silicone Raspberries Used to Train Robot Harvesters

    Catwell
    Catwell
    EPFL has developed a robotic arm capable of identifying ripe fruit and can harvest them without damage. (Image credit: EPFL) Engineers from EPFL's CREATE Lab have developed and tested a robotic arm capable of harvesting raspberries without dama...
    • 22 Aug 2024
  • Tons of E-Waste Could be Prevented with New Recyclable Circuit Boards

    Catwell
    Catwell
    The new material has nearly the same performance as traditional PCB material but can be completely recycled. Researchers from the University of Washington have developed a new formulation for circuit boards that offers performance on par with tradi...
    • 19 Aug 2024
  • How The Las Vegas "Sphere" Works

    Catwell
    Catwell
    The Las Vegas Sphere is a technological feat, boasting the world's largest interior and exterior screens. (Photo by Y2kcrazyjoker4 is licensed under CC BY 4.0) With a $2.3 billion construction cost, the Las Vegas Sphere is home to the world'...
    • 16 Aug 2024
  • Japanese Government Retires the Floppy Disk

    Catwell
    Catwell
    Last month, the Japanese Digital Agency scrapped all 1,034 regulations governing floppy disk use, except for one that applies to vehicle recycling. (Image credit: Wikipedia) It's almost the end of floppy disk use in the industrial world. The Jap...
    • 6 Aug 2024
  • Rockwell’s ArmorKinetix Distributed Servo Drives Facilitate Smaller Machine Designs

    Catwell
    Catwell
    The ArmorKinetix Servo Drives can also lower system costs and increase productivity and uptime. (Image via Rockwell) Rockwell Automation touts its new ArmorKinetix Distributed Servo Drives as the technology behind faster deployments and more capable...
    • 1 Aug 2024
  • Why Southwest Airlines Remained Unaffected by The Worldwide IT Outage

    Catwell
    Catwell
    (Image Credit: april_kim/Pixabay) “Don’t fix what isn’t broken” is a big motto in the design world. I always love stories of old technology still doing its job, and well. This is one of those cases. Last week, the world exper...
    • 23 Jul 2024
  • Bota Systems PixONE Torque Sensor Features Hollow Shaft Design for Robotics Applications

    Catwell
    Catwell
    The PixONE platform packs a 6-axis IMU, gyroscope, temperature sensor and can handle payloads up to 250 kg. (All images via Bota Systems) Bota Systems, a Zurick-based developer and manufacturer of multi-axis force-torque sensors, recently unveiled i...
    • 18 Jul 2024
  • Japan Proposes an Underground Transportation System to Deliver Cargo

    Catwell
    Catwell
    (Image Credit: Tama66/pixabay) The Japanese Transport and Tourism Ministry is planning to develop a huge 310-mile automated underground conveyor belt, called the Autoflow-Road, transporting packages from Tokyo to Osaka. Japan hopes this will address...
    • 12 Jul 2024
  • Meet The Mini Replica of TARS Showcased at Open Sauce 2024

    Catwell
    Catwell
    The mini TARS replica robot was built by Charlie Diaz. (Image Credit: Charlie Diaz/hackster.io) Charlie Diaz is no stranger when it comes to Interstellar. The film features TARS, a two-legged robot, and he felt inspired enough to build a mini versio...
    • 10 Jul 2024
  • Maple Seed-Inspired Robot Uses Light to Control Its Glide Path

    Catwell
    Catwell
    Image showing a natural maple samara (left) and artificial seed (right) while descending. (Image Credit: Jianfeng Yang / Tampere University) Researchers at Tampere University, Finland, and the University of Pittsburgh collaborated to develop a robot...
    • 3 Jul 2024
  • Robots Look More Lifelike With This Lab-Grown Human Skin Tissue

    Catwell
    Catwell
    The left image shows a 3D mold covered with living skin. The right image shows a 2D facial robot covered with living skin. ©2024 Takeuchi et al. CC-BY-ND Lifelike robots are starting to take shape and become a reality. Researchers at the Univer...
    • 28 Jun 2024
  • Robotic Snail Swarm Work Together to Move Across Challenging Terrain

    Catwell
    Catwell
    As shown in the image, the snail robots can work together or individually to move across terrain, climb, or overcome obstacles. (Image Credit: Zhao et al., Nature Communications, 2024) Researchers at the Chinese University of Hong Kong developed a r...
    • 14 Jun 2024
  • Climeworks' Massive Direct Air Capture Tech Begins Removing Carbon from The Air

    Catwell
    Catwell
    The Mammoth carbon capture plant began operations and aims to capture 36,000 tons of carbon per year. (Image Credit: Climeworks) Mammoth, a carbon capture plant built by Climeworks, recently started removing CO2 from the earth's atmosphere. Base...
    • 22 May 2024
  • NASA Seeks New Plans for The Mars Sample Return Mission

    Catwell
    Catwell
    An illustration of the Mars Sample Return mission. (Image Credit: NASA/ESA/JPL-Caltech) According to NASA, the existing Mars Sample Return (MSR) mission plans to return the Mars rock samples before 2040 need to be reconsidered. The space agency says...
    • 16 May 2024
<>