Internet of Things
  • Technologies
  • More
Internet of Things
Blog Building a Reflow Oven: Part 1 – Getting Started
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 27 Jul 2014 3:59 PM Date Created
  • Views 7401 views
  • Likes 2 likes
  • Comments 29 comments
  • reflow
  • ioe
  • internet_of_everything
  • smd
  • internet_of_things
  • surface-mount
  • labs
  • iot
  • soldering
  • tools
Related
Recommended

Building a Reflow Oven: Part 1 – Getting Started

shabaz
shabaz
27 Jul 2014

Contents

Part 1 (You're here) Introduction and Test bed setup

Part 2: Experimentation with a heating element and some basic measurements

 

Introduction

Some people (not me) can successfully solder incredibly tiny Quad Flad No-lead (QFN) parts such as the one in the photo below by hand using a soldering iron or a hot air gun (the photo below is from a commercial board, not hand soldered). For wireless devices and modern sensors, surface mount device (SMD) packages as small as QFN have become the normal, default package.

image

 

Solder paste allows other methods to be used. A hot plate is one option. Another popular method is to use an oven.

image

 

At work, we may purchase a small reflow oven or hot plate at some date. However, for now, I decided to attempt to create a simple oven for home use.

 

There are lots of reflow oven projects on the Internet based on modified toaster ovens, but it is difficult to replicate them because manufacturers keep bringing out new toaster ovens and the older ones become unavailable.

 

The aim was to try to create an oven from scratch, using off-the-shelf readily available heating elements. This would allow others to be able to repeat the exercise, which in theory has two huge benefits. Firstly it allows people to replicate with confidence that the same consistent results should be achievable. Secondly it allows people to share their findings and help improve everyone’s ovens!

 

Setting Expectations

Commercial reflow ovens use many clever techniques and may need a gas supply too. It will be impossible to achieve high quality results in the simple reflow oven that will be constructed. Here is an example production quality oven:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

At best, the reflow oven that will be created might be just-about usable for prototypes. I’m not knowledgeable in thermodynamics so it is quite an experimental oven. If people have suggestions they will be gratefully received.

 

Finally this project uses mains line power which can easily kill. This project also gets hot which may cause burns, toxic smoke or a fire. Please check with a qualified expert before building this project.

 

Trying out some Heating Elements

To speed up development, the strategy was to start constructing a potential enclosure while narrowing down heating element possibilities at the same time. A couple of heating elements will be tested. If they are unsuitable, then more will be tried. The controller for the reflow oven will be based on an off-the-shelf microcontroller development board. For the initial experiments, no electronic oven control capability will be used; the heating element will be switched on/off using a mains switch. The initial tests will be in free air. The test results won’t be usable since the elements are not in an enclosure, but the aim here is to just get some experience with the heating elements and begin to see their characteristics.

image

 

The photo above shows the setup so far. The heating element is suspended 100mm above a scrap circuit board. For now, the element is connected to the mains through an IEC connector with built-in fuse and switch, as shown in the photo below. It may need to be replaced with a hot IEC socket for the actual build.

image

 

Here is an annotated photo of the setup:

image

 

Another view without all the cables:

image

 

Next Steps

The heating elements will be experimented with; some additional information on this tomorrow!

  • Sign in to reply

Top Comments

  • fvan
    fvan over 12 years ago +2
    Sounds like the outcome of this project could be very interesting for a lot of hobbyists, I like it Frederick
  • shabaz
    shabaz over 12 years ago in reply to fvan +2
    Hi Frederick, Exactly, this is really a community project that hopefully interests others, I'm not the expert here, I think other hobbyists may be, especially physics/mechanics experts! so I'll happily…
  • jw0752
    jw0752 over 12 years ago +1
    Thanks for sharing your experiment with us. John
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    image

    I bought a gunge dispenser direct from China via Aliexpress for about £75 - very crude (one switch doesn't work properly, footswitch connector broken, leaks air) and you don't get much in the way of needles etc. I then spent as much again on syringe barrels, 2 sensible sized air to syringe thingies that actually clip on and off properly and three different sizes of needle (in packs of 25).

    With hindsight the dispenser itself is a waste of time, all you need is a solenoid valve, a timer settable between 10 and 500m s and a pressure regulator.

    You can buy a regulator and solenoid valve of decent quality for about £75 (or less if you look hard) and build the timer form almost any micro development board you might have kicking about. The dispensers all talk about having suck back but you only need that for runny stuff - not needed for solder paste.

    When this dispenser fails (I don't think I'll need to wait long) I'll make the next one (I even have suitable air parts from an old test rig.).

     

    You can buy a much more reasonable looking dispenser from a UK source for £225. Analog timed glue dispenser adhesive dispensing - this is where I got my barrels and nozzles from.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to michaelkellett

    O yes what did you use as a compressor as well ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to Problemchild

    I have an ultra quiet compressor very like this one:

     

    Bambi BB24V Compressor - Air Compressors - Air Compressors - Workshop Equipment | Axminster Tools & Machinery

     

    I also have a very noisy big one but I wouldn't want to work near it !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 12 years ago in reply to Problemchild

    I have an ultra quiet compressor very like this one:

     

    Bambi BB24V Compressor - Air Compressors - Air Compressors - Workshop Equipment | Axminster Tools & Machinery

     

    I also have a very noisy big one but I wouldn't want to work near it !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett

    You guys might like this then.

    I've had a report from someone who brought one via another source, and apart from too much (his fault) he said it worked well.

     

    http://digistump.com/products/107

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to mcb1

    Hi Mark,

     

    Thanks for finding this! I notice there is a video of it here: https://www.tindie.com/products/Pieco/paste-press/

    It certainly looks useful.

    It looks like the microdot releases one dot per press, while the Pieco one needs a different button pressed to stop. So this might be a bit tricky, but at a far lower price may well be worth trying out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to michaelkellett

    Looks like a nice compressor, if a bit pricey how have you found it ?