Internet of Things
  • Technologies
  • More
Internet of Things
Blog Digital Logic µFR NFC Card Reader - part 4: first meaningful ISO14443 / APDU conversation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 16 Dec 2020 9:48 PM Date Created
  • Views 2853 views
  • Likes 2 likes
  • Comments 1 comment
  • security2go
  • apdu
  • smartcard
  • iso14443
  • nfc
Related
Recommended

Digital Logic µFR NFC Card Reader - part 4: first meaningful ISO14443 / APDU conversation

Jan Cumps
Jan Cumps
16 Dec 2020

In this article I make a c++ application for the D-Logic card reader and a set of smart cards.

This time I focus on the ISO14443_4 / APDU protocol. Getting results instead of focusing on Object Oriented Design.

image

 

In contrast to previous posts, I'm going for some real results here.

The goal is to use the smart card session I created in the previous posts, to have a discussion with the application running on the card:

  1. Open a session with the smart card,
  2. retrieve ID and card version.

 

A summary of terms used:

  • APDU: it's a protocol to interact with the software that's running on some smart cards.
  • ISO14443_4: a protocol for smart cards that can represent their internal functionality as APDU interactions

 

The Infineon card that's on the reader in this post is specialised to provide key / encryption related functionality.

The card holds a number of keys (going fast here, there's a lot more to it) that can be used in secure transactions.

A few of the APDU functions are:

  • store and communicate public keys
  • generate keys
  • hash data based on its private key

 

I'm not using any of these here. I'm going to show public key exchange in a next blog.

In this post, I open an APDU application session, and return the card's APDU ID.

An APDU session is really like running an application on a server. The card has to be on the reader, to keep a session alive, and to keep giving energy to the card.

Once you remove the card, the session is broken and void.

 

APDU Command Code

All the values from line 2 to line 7 are exactly the same APDU command bytes as in Infineon's application developer instructions.

I've pasted the relevant part in the table below the code.

 

void CardISO14443::selectApp() {
  uint8_t cls = 0x00;
  uint8_t ins = 0xA4;
  uint8_t p0 = 0x04;
  uint8_t p1 = 0x00;
  uint8_t data_out[13] = {0xD2, 0x76, 0x00, 0x00, 0x04, 0x15, 0x02, 0x00, 0x01, 0x00, 0x00, 0x00, 0x01};
  uint8_t data_out_len = 0x0D;
  uint8_t data_in[20];
  uint32_t max_data_in_len = 20;;
  uint32_t response_len;
  uint8_t send_le = 1;
  uint8_t apdu_status[2];


  UfrFactory::Status status = UfrFactory::retvalConvert(uFR_APDU_Transceive(
      cls, ins, p0, p1,
      data_out, data_out_len,
      data_in, max_data_in_len, &response_len, send_le,
      apdu_status)
  );
  if (status != UfrFactory::UFR_OK) {
    throw CardException(status);
  }
}

 

There's only one line of code that calls the APDU app on the card: line 15.

Line 2 to 12 is declaring variables and preparing the message to the card.

Line 21-23 is exception handling.

 

Here's than analysis of line 6, the APDU command.

Because I'm running the first, mandatory command to start the app session, I can just reuse my analysis of the Android example app for the card:

 

Command analysis from my first post:

Send the SELECT APP command

 

This is the first command you have to send to the card before it can be used in a scenario.

The APDU command: 00A404000DD276000004150200010000000100.

 

image

image source: User Manual Blockchain Security 2Go Starter Kit

 

APDU Send / Receive Communication Script

image

 

  • 00 this is the instruction's class
  • A4 this is instruction A4: SELECT APP (open application session)
  • 0400 parameters 1 and 2 (both a byte). 04 indicates that the app is determined by the DF name. Second parameter is not used in this function.
  • 0D the AID data field hereafter has a length of 13, (0x0D)
  • D2760000041502000100000001 the AID of the Infineon cards.
  • 00 length of the reply. The value Infineon's guide suggests here surprises me...

 

 

APDU Answer from the Card:

 

After sending the above APDU command the card, here's the reply received in the buffer data_in.

image

 

And my analysis of the Android phone app response is again valid, because I tapped the same smart card:

 

Response analysis from my first post:

Analyse the Reply

 

This is what what the card sends back: 0002090C2900020040001576312E309000.

  • 00 the pin isn't set for this card
  • 02 09 0C 29 00 02 00 40 00 15  the ID of this particular card
  • 76 31 2E 30 the ascii version string.  v1.0.
  • 90 00 the return code. Success

 

Full scenario in the c++ main code (the Eclipse project with current version of the source is attached:

 

      isocrd->setISO14443_4();
      isocrd->selectApp();
      isocrd->unsetISO14443_4();

 

I added the unsetISO14443_4() call while testing. During my tests, the second time I ran the program, with the card still on the reader, would fail.

I read in my reader's manual that it's mandatory to close the data stream to the app after the last APDU call.

image

That turns operation back to normal RF card mode, and fixes my test failure.

 

Related Blog
Blockchain - Talk Directly to the Infineon 2Go Smart Cards API
NFC Card Reader Protocol of Digital Logic µFR - part 0: intent
µFR NFC Card Reader - part 1: first C program for Linux (RPi, BB, ...)
µFR NFC Card Reader - part 2: first C++ program
µFR NFC Card Reader - part 3: C++ Class to handle ISO14443 / APDU cards
µFR NFC Card Reader - part 4: first meaningful ISO14443 / APDU conversation
µFR NFC Card Reader - part 5: refactor, look back at initial design
Attachments:
digitallogic_rfc_cpp_20201216_2.zip
  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 5 years ago

    I've refactored a bit.

     

    In my design, the reader checks the card type, and returns an object of that type.

    The type of card returned isn't depending on the reader though.

    The reader may have capabilities to talk or not talk to certain cards, but it isn't the one that needs to know.

    Else, I'd have to create a reader for many card types, while the reader capabilities don't change.

    I'm going to restrict the reader knowledge to "ability to serve according to smartcard standards"

     

    So I moved it out to the factory.

    The standard factory knows how to create common known  cards. And how to use a reader.

     

    For specialised cards, I'll provide a specialised factory. It can use the existing reader class, but knows how to create specialised cards.

    For the Infineon Security2Go cards, I'll create a S2GoFactory and a CardS2Go class.

    The factory will use reader API to check if the card is of the S2Go type, and if yes, create a CardS2Go object.

    Else it will fail.

     

    The CardS2Go will be a child of the CardISO14443 class. Because it uses that class' functions. But additionally runs a S2Go specific application API.