Internet of Things
  • Technologies
  • More
Internet of Things
Blog DIY fun: Building a Mains Power Line Sniffer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Aug 2014 4:35 PM Date Created
  • Views 8082 views
  • Likes 8 likes
  • Comments 23 comments
  • mains
  • texas_instruments
  • sensor
  • ti
Related
Recommended

DIY fun: Building a Mains Power Line Sniffer

shabaz
shabaz
11 Aug 2014

Introduction

Attempting to put up a shelf over the weekend to create my own lab, I couldn’t find my mains power tracer. These things are used to detect buried mains cables in walls; the detectors are low cost, and available at DIY stores. The more wiring that is stuck into homes the more important such a tool becomes.

 

With the local stores being shut on a Sunday, I figured it was time to either borrow one or build one.

 

This post documents an AC mains power tracer that can be built in a couple of hours. It has benefits over some store-bought models; it is ultra-sensitive, and requires no adjustment/calibration.

image

 

As usual, be careful with mains voltages. The circuit described here is not intended to be exposed close to uninsulated wires or open enclosures. It is an aid to locate live wiring behind walls.

 

Design Detail

Typical mains power line detectors are often integrated with metal detection capability too. The design I implemented only detects AC mains power.

 

Anyone who has experimented with field effect transistors will not have failed to notice that the extremely high input impedance allows you to have lots of fun with electrostatics. Charging up a comb or balloon and then bringing it close to the gate provides sufficient charge to control the FET. There are lots of classic circuits that can be googled based around the popular 2N3819 or MPF102 junction FET (JFET) devices to construct electronic equivalents of the old ‘gold-leaf electroscopes’, usually using not much more than a JFET, an LED and a battery.

 

It was time to try different things! There are some nice op amps available, so it was decided to construct an op amp based circuit and see how well it works.

If this was to be a low-cost design for DIY store, then a JFET or low-cost op amp circuit would be designed, perhaps with some nulling capability at switch-on, and an LED indicator.

 

For this design, some nicer parts are used. An analog meter is used to display the measured field. This is far better than an LED for this use-case in my opinion. As you drag the device across a wall, you can easily watch for the peak on an analog meter. I used a random meter from a junk box, but there are lots of options such as an edge mount panel meteredge mount panel meter or my favorite - a round meterround meter - both would work fine.

image

 

Furthermore, an interesting op amp from Texas Instruments was used for converting the tiny current from the electric field into a measurable quantity. The selected device, LMP7721LMP7721, is ideal for building a transimpedance amplifier to perform the current to voltage conversion.

The circuit diagram is shown below.

image

 

The photo here shows how it was constructed. The orange blob on top of the op amp is an axial 100nF capacitor100nF capacitor C1. The resistor you can see to the left of it is R1.

image

 

The op amp is available in an SO8 package, so a small SMD adapter board from TISMD adapter board from TI was used - the adapter board is great value, it comes with the terminal strips too, all ready to solder.

There is a 100 Mohm resistor100 Mohm resistor in the op amp feedback, and it was soldered in the air – the inverting input of the op amp was not soldered to the adapter board, but was carefully bent so that all soldering was in the air. Also, finger contact with the resistor and C2 and C3 was avoided to prevent grease (use tweezers).

 

Resistor R3 is a small, non-critical value (I used a trimmer resistor but it is not needed). I used a 200uA meter. R3 just provides some protection for the op amp and the meter. In a similar vein, R2 and C2 are an attempt to provide some protection from spikes. I’m not sure how effective it is, these values were not calculated nor tested.

 

The entire circuit is driven from a non-critical supply voltage of around 3V (I tested with a 3.3V supply). The non-inverting input is at the same voltage as the most negative supply. This is not usually good for an AC input, however it means that no rectifier is needed at the output. It was found the circuit as-is performs well. It is extremely sensitive, from the needle deflection you can sense mains power lines from a foot away (30cm).

 

The oscilloscope trace below shows the output when the circuit is held close to the mains supply cable to my desk lamp. It is quite a large output (20msec spaced peaks corresponding to 50Hz mains supply).

image

Summary

The circuit worked very well although I still have not fitted the shelf : ) As a reminder, don’t rely on the circuit – it is just an aid. I can’t guarantee its reliability or safety. It is an experimental circuit, not for DIY enthusiasts.

 

To make the circuit more usable/practical, I drilled out a hole for it in a Hammond enclosure Hammond enclosure (not got round to finishing that either!). I may power it from two N-sized batteries if they fit. A larger case and AAA batteries would be better.

image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 12 years ago in reply to shabaz +2
    Hi Shabaz - I have just completed making my interpretation of the Shabaz AC Line Sniffer. This was my first attempt to make a usable device using surface mount chips. I had a cheap SOIC-20 adapter board…
  • jw0752
    jw0752 over 12 years ago +1
    Hi Shabaz, Thanks for sharing this cool project with us. I have always enjoyed making my own test instruments. It helps not to have a critical application. I can't wait to give this one a try. John
  • mcb1
    mcb1 over 12 years ago +1
    Nice work. You can also some of those voltage sticks. There are a number around that are very sensitive, and therefore useless inside a switchboard for detecting which wire is live. This would be an ideal…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    Oh, so only good for none North America then huh. I guess I will have to completely re-design for North American 60Htz image sensing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to Robert Peter Oakes

    Hi Peter,

    Good name for it, spider nest is appropriate!

    I didn't do any filtering for 50Hz, so it should work as-is for 60Hz/North America. Things like a tone output or a battery-check would also be quite good, I didn't get as long as I wanted on this project, the shelves still have to go up!!

    Also another idea was to connect the output to an interrupt pin on a microcontroller (or to any ADC built-in to the microcontroller), and see the exact frequency over time, maybe plot it on a graph, to see what time the load for the region is highest : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    The "ACspider" it is then.

     

    You should encourage Douglas to incorporate it into his mailbox which seems to full of it's cousins versions.   image

     

    Any real hacker wouldn't worry about the mains and if you stick a cable then use it to make the shelf glow.

    This safety thing seems to be for someone else ...  image

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    The "ACspider" it is then.

     

    You should encourage Douglas to incorporate it into his mailbox which seems to full of it's cousins versions.   image

     

    Any real hacker wouldn't worry about the mains and if you stick a cable then use it to make the shelf glow.

    This safety thing seems to be for someone else ...  image

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 12 years ago in reply to mcb1

    Hehe yes it improves the lighting for the shelf area.

    it's not so necessary in your own home if you know where the wiring is, i.e. vertically off switches/sockets. I do remember seeing someone else's wall where they had a cable running at 45 degrees from the light switch which was interesting image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    Never rely on the electrician running cables vertically back up the wall.

    I did at my place except where there was a window, and that one went horizontal from just beside it.

     

    mark