Internet of Things
  • Technologies
  • More
Internet of Things
Blog Fail of the week with ESP8266 Cheap Wifi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: camuyano
  • Date Created: 17 Oct 2014 11:24 PM Date Created
  • Views 4171 views
  • Likes 4 likes
  • Comments 24 comments
  • uart_to_wifi_convert_module
  • hobbyist
  • esp8266
Related
Recommended

Fail of the week with ESP8266 Cheap Wifi

camuyano
camuyano
17 Oct 2014

A little more than a month ago a friend told me about a cheap wifi module. So I searched for this piece of wifi magic and founded the ESP8266 Wifi module. And it is really cheap. Depending on where you get it and the version we can say is between $5 and $8 for one module. Told myself I can spare $8 for this Wifi promise land so I ordered two for a little more than $8.

Yesterday I got them, right away I got very exited!! On yes, new toy!

First I realized that I ordered the ESP8266 ESP-03 model. Seems to be one of the favorites (from the forums) because it has several exposed digital IOs. But .... (there is always a but) it has no pin headers, so I said, no problem I solder a few and get done with it. Pin space separation is not the same as my pin headers. I then move to plan B (or C, hard to keep track when you are exited to get this working). Anyhow, the idea was to place it on a perf board and solder small wires to the position of some pin headers so I can wire this up.

I did manage to hook up some wires then the moment came. I got the usb to serial, connected to the device, opened the terminal window and.... and..... nothing! Nothing at all.

As of now I do not know if I damaged the device or the soldering is not good enough or even if I am totally wiring it incorrectly. For that I air my frustration here while I manage to get a lease from sleeping time to continue working on this.

It may be nothing, but this board has the antenna upside down. Comparing it to the other, and to others in the web. It might be nothing.

image

What is my future plan:

I got two of this, in the new un-touched one I will be more carefull.

1. Only wire the needed pins to avoid overheating the thing.

2. Hook everything through a level shifter to make sure I am on the safe side of the 3.3V

3. Pray

4. See what happens

 

Also there is one of the other versions in the way so I will try with other versions. I am sure this will be sorted out, and I will be able to use this for the Christmas decorations. But if someone is using one of these modules, or just have any comment, please do.

I will update with progress about this for others to benefit, there are not that many youtube videos about this device. However it seems to be working for a lot of folks.

 

I don't easily give up. Hope tonight I have the time to make this work.

  • Sign in to reply

Top Comments

  • hansaya
    hansaya over 11 years ago +2
    YAY!, got it working after countless hours of playing with this. Connect these lines CONNECT GPIO15 TO GROUND CONNECT CH_PD TO HIGH test this with serial terminal with 9600bud This should get the device…
  • jw0752
    jw0752 over 11 years ago +1
    Hi Javier, This type of problem happens to me frequently. The good part is that I usually end up learning more from my experience than I would have if the thing worked right the first time. I look forward…
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Hi Guys I'm very confused about this ESP03 chip. After watching countless hours of videos and reading, what do i actually have to connect to get this to work? I understand that I can only use 3.3volts…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi Guys I'm very confused about this ESP03 chip. After watching countless hours of videos and reading, what do i actually have to connect to get this to work? I understand that I can only use 3.3volts. I cannot find a valid print to use to possibly get this to work. Do I only have to connect those wires as mentioned above

    "Connect these lines

    CONNECT GPIO15 TO GROUND

    CONNECT CH_PD TO HIGH"

    to be able to talk to this or do I have to connect VCC , GND, UTXD and URXD also? Also I believe that the Arduino RX and TX is 5 volts as well, so I guess I would have to use a voltage divider with those as well. Am I on the right track?

     

    I burned up one chip soldering it together. Then I think I might have blown another one connecting the TX and RX to the arduino. Got two left so Help would be appreciated.

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi Guys I'm very confused about this ESP03 chip. After watching countless hours of videos and reading, what do i actually have to connect to get this to work? I understand that I can only use 3.3volts. I cannot find a valid print to use to possibly get this to work. Do I only have to connect those wires as mentioned above

    "Connect these lines

    CONNECT GPIO15 TO GROUND

    CONNECT CH_PD TO HIGH"

    to be able to talk to this or do I have to connect VCC , GND, UTXD and URXD also? Also I believe that the Arduino RX and TX is 5 volts as well, so I guess I would have to use a voltage divider with those as well. Am I on the right track?

     

    I burned up one chip soldering it together. Then I think I might have blown another one connecting the TX and RX to the arduino. Got two left so Help would be appreciated.

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • camuyano
    camuyano over 11 years ago in reply to e14 Contributor

    I have not connected the ESP -03 but on the esp 02 or 01. You must connect CH_PD to 3.3, I connect the RST to 3.3 as well. On that other model the GPIO0 is grounded for firmware update. And when doing so it must be grounded on power up of the device, and the device will go into "firmware update" mode. The 03 version described here I tried but since I was not able to make it work I continue working on the esp01 or 02 (I keep messing the versions).

    You must definitely some sort of voltage divider for the TX and RX. I have used several level shifter methods working (again with the other version).

    Here is how I connected the one I am working with http://www.element14.com/community/groups/internet-of-things/blog/2014/11/04/esp8266-developing-using-an-arduino

    I am on the way of building a new board for the surface mount esp model but I have not tested (http://www.element14.com/community/blogs/nerdito/2014/12/13/other-board-for-the-esp8266).

     

    A voltage divider can be two resistor or just get a level shifter from ebay or sparkfun. I used a bidirectional level shifter to avoid my "skils" to burn the chip.

    People that has commented here have used successfully the model so they might help you more.

    When connected correctly please post back, I know I will (but I might as well burned mine).

    Try to connect it as best as you can and do firmware update then continue from there. Default firmware may be very buggy and produce weird results.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to camuyano

    For what it is worth, one of the guys in our club has put together this.

    It might help, but not having brought one I'm not sure. (I might need to buy some just to see what they are like)

    Notes: ESP8266 by follower - labradoc.com

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to mcb1

    Javier

    Okay I'm blaming you now for me purchasing 5 of them. image

    I decided to get two different models, for ease of mounting.

    http://www.ebay.com/itm/like/201206173209

    http://www.ebay.com/itm/like/201205524305

     

    Mark