Internet of Things
  • Technologies
  • More
Internet of Things
Blog How to setup a home automation server with EnOcean Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: malakai
  • Date Created: 2 Jun 2014 6:31 AM Date Created
  • Views 3092 views
  • Likes 1 like
  • Comments 4 comments
  • home-energy_control
  • raspberry-pi
  • enocean_pi
Related
Recommended

How to setup a home automation server with EnOcean Pi

malakai
malakai
2 Jun 2014

A complete walk through can be found in my Road Test Review on setting up the EnOcean Pi and Sensors:

 

http://www.element14.com/community/roadTestReviews/1795

 

With my recent arrival of the EnOcean Pi Road Test Kit I thought a tutorial on setting up the Gateway would be a great article to start with. The Sensor Kit is on backorder so I will fill my time working with just the EnOcean Pi Gateway for now.

 

This entire process is outlined within the White Paper :

 

Raspberry Pi talks EnOcean - How to setup a home automation server with EnOcean Pi or USB 300

 

Source: http://www.enocean.com/fileadmin/redaktion/pdf/white_paper/wp_Raspberry_talks_EnOcean.pdf

 

 

Steps to setup the EnOcean Pi

 

1. Connect the EnOcean Pi board to the Raspberry Pi

 

image

 

Disable Serial Console

sudo nano /boot/cmdline.txt

 

The file should look like this:

 

dwc_otg.lpm_enable=0 console=ttyAMA0,115200 kgdboc=ttyAMA0,115200 console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 elevator=deadline rootwait

 

Remove all references to ttyAMA0 so the contents are:

 

dwc_otg.lpm_enable=0 console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 elevator=deadline rootwait

 

Exit and Save the File. CTRL+X

 

Update Raspbian

 

sudo apt-get update && sudo apt-get upgrade

 

Install the required Perl packages:

 

sudo apt-get install perl libdevice-serialport-perl libio-socket-ssl-perl libwww-perl

 

Install FHEM (Check to make sure you are getting the latest FHEM Version Home of FHEM.)

 

wget http://fhem.de/fhem-5.5.deb

sudo dpkg –i fhem-5.5.deb

 

2. Display FHEM Web Interface

 

Start your browser and type following to the link field:

 

http://<Raspberry_Pi_IP>:8083/fhem

 

 

You will get the following user interface on the screen:

 

imageimage

 

FHEM recognizes and configures the EnOcean PI. It receives radio telegrams from all EnOcean devices within the neighborhood (10-30m within buildings). Device entities will be created automatically for each new received EnOcean device (every EnOcean radio module or device has a unique manufacturer ID). Switches are by recognized by their specific RPS telegram, sensor types are recognized via learn button with 1BS or 4BS telegram. By default devices with EnOcean radio protocol will be to room EnOcean.

 

3. FHEM auto configurations

 

FHEM server is configured via the configuration file fhem.cfg.

Start the configuration file editor via the FHEM menu item “Edit files”.

 

image

 

Gateway:

 

If USB 300 is plugged and configured to the Rapsberry Pi correctly following code will be generated automatically by the FHEM autocreate function:

 

image

 

define TCM310_0 TCM 310 /dev/ttyUSB0@57600

 

If EnOcean Pi is plugged and configured to the Rapsberry Pi correctly following code will be generat-ed automatically by the FHEM autocreate function:

 

image

 

define TCM310_0 TCM 310 /dev/ttyAMA0@57600

 

 

At this point in the log file it returned the following:

 

2013.02.01 07:43:29 3: Can't open /dev/ttyAMA0: Permission denied

To remedy this add the users pi and fhem into the tty groups:

 

sudo usermod -a -G tty pi

sudo usermod -a -G tty fhem

Switch:

 

imageimage

 

After you press the rocker the first time a new device entry is generated:

 

define EnO_switch_FEFFFEFB EnOcean FEFFFEFB

attr EnO_switch_FEFFFEFB room EnOcean

attr EnO_switch_FEFFFEFB subType switch

define FileLog_EnO_switch_FEFFFEFB FileLog .../log/EnO_switch_FEFFFEFB-%Y.log EnO_switch_FEFFFEFB

attr FileLog_EnO_switch_FEFFFEFB logtype text

attr FileLog_EnO_switch_FEFFFEFB room EnOcean

 

Manufacturer ID is 0xFEFFFEFB, telegram data will be logged automatically.

 

 

Sensor:

 

imageimageimage

 

This is an example of an temperature (room controller) sensor. After you press the learn button the time a new device entry is generated:

 

define EnO_sensor_0088F03E EnOcean 0088F03E attr EnO_sensor_0088F03E manufID 00B

attr EnO_sensor_0088F03E room EnOcean

attr EnO_sensor_0088F03E subType roomSensorControl.01

define FileLog_EnO_sensor_0088F03E FileLog ./log/EnO_sensor_0088F03E-%Y.log EnO_sensor_0088F03E

attr FileLog_EnO_sensor_0088F03E logtype text

attr FileLog_EnO_sensor_0088F03E room EnOcean

 

Manufacturer ID is 0x0088F03E, telegram data will be logged automatically and can be displayed within a diagram.

 

 

Interface:

 

With the user interface you can visualize and configure graphical user elements to visualize events and send control telegrams to actuators.

 

A reference of FHEM commands for EnOcean can be found at:

 

http://fhem.de/commandref.html#EnOcean

 

A small guide “how to” can be found at: http://fhem.de/HOWTO.html

 

For German users there is an additional forum available: http://forum.fhem.de/

 

 

Example of visualization:

 

Following visualization example has been generated by STM 330 (temperature sensor) with HSM 100 (humidity sensor plugged):

 

#ID:0088F03E STM_330 temperatur & humidty sensor

define Sensor_0088F03E EnOcean 0088F03E

attr Sensor_0088F03E manufID 00B

attr Sensor_0088F03E room EnOcean

attr Sensor_0088F03E subType roomSensorControl.01

define FileLog_EnO_sensor_0088F03E FileLog ./log/EnO_sensor_0088F03E-%Y.log Sensor_0088F03E

attr FileLog_Sensor_0088F03E logtype text

attr FileLog_Sensor_0088F03E room EnOcean

 

image

 

More Resources:

 

EnOcean Link Trial Software is also available follow this article

element14: How to use EnOcean Pi with Raspberry Pi

 

For an overview see the article

EnOcean Pi: Transforms Raspberry Pi into a Wireless Gateway

 

Also See:

Greg Fenton's Article EnOcean Sensor Kit (ongoing) with 3D Printed housing for the Temperature Module.

 

 

For more details on setting up the EnOcean Pi and Sensors see my review

 

http://www.element14.com/community/roadTestReviews/1795

.

Attachments:
imagewp_Raspberry_talks_EnOcean.pdf
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Hi Todd, Good overview here. I wanted to point out that the unique 32 it EnOcean IDs are known as chip IDs and are similar to MAC addresses in functionality. The manufacturer ID is something a little bit…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi,

    I have the EnOcean sensorkit and a raspberry pi 2 B, I followed each point of this tutorial and tried many other (one of them was the "Raspberry talks enocean" for example). But in each case I always have the same problem : the "EnOcean" button doesn't appear on the side in fhem and I can't continue the configuration.

     

    Does anyone had this problem ? Any help would be welcome image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi,

    I have the EnOcean sensorkit and a raspberry pi 2 B, I followed each point of this tutorial and tried many other (one of them was the "Raspberry talks enocean" for example). But in each case I always have the same problem : the "EnOcean" button doesn't appear on the side in fhem and I can't continue the configuration.

     

    Does anyone had this problem ? Any help would be welcome image