Internet of Things
  • Technologies
  • More
Internet of Things
Blog LPC551x/S1x: Cortex-M33 based MCU with New Levels of Cost and Performance Efficiency
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: leo_
  • Date Created: 28 Apr 2020 4:51 AM Date Created
  • Views 2357 views
  • Likes 4 likes
  • Comments 8 comments
  • arm cortex m33
  • nxp webinar
  • industrial
  • arm cortex
  • hs usb
  • consumer electronics
  • 32-bit mcu
  • low power
  • can fd
  • 32-bit
  • mcu
  • iot
  • cortex-m33
  • nxp
  • lpc
Related
Recommended

LPC551x/S1x: Cortex-M33 based MCU with New Levels of Cost and Performance Efficiency

leo_
leo_
28 Apr 2020

Semiconductor industry is always evolving at an unprecedented speed. You may feel this trend when changing your smart phone from an older generation to the latest offering from Apple or Samsung, and found that the screen and performance of the device is better than you ever could imagine, just like the time when you change your personla computer several years ago.

 

However, not only the power of a high-end processor is enhancing continuously, the benefit of technology upgrade also lies in MCUs. Intruduced in 2019, NXP's LPC5500 general purpose microcontroller series has brought more computing power into our daily life while maintain low power comsumption. Now, within a year's time, the third family in LPC5500 series——the LPC551x/S1x microcontroller family is in mass production.

 

LPC5500

You may already heard of the LPC5500 MCU series from NXP. Leveraging the ArmRegistered CortexRegistered-M33 technology, LPC5500 combines significant product architecture enhancements and greater integration over previous generationsof NXP's microcontrollers, offering dramatic power consumption improvements and enhanced security features including SRAM PUF based root of trust and provisioning, real-time execution from encrypted images , and asset protection with Arm TrustZoneRegistered-M Technology.

 

LPC551x/S1x

The LPC551x/S1x MCU family expands LPC5500 into a new price point, offering significant advantages for developers, including pin-, software- and peripheral-compatibility for ease of use and to help accelerate time to market, while still leveraging the cost-effective 40-nm NVM process technology.

The LPC551x/S1x is the entry-level family within the LPC5500 MCU series, providing new levels of cost and performance efficiency in addition to security and system integration for industrial, IoT and general embedded applications.

imageimage

 

Key Strength and differenciators

  • Ultra-efficient 40-nm flash technology
    • Over 600 CoreMarks and as low as 32uA/MHz
  • System Integration for Industrial and IoT Markets
    • High-Precision ADCs
    • CAN-FD for industrial control
    • HS USB with On-Chip PH
  • Enhanced safety and security with Arm TrustZone-M technology
  • Comprehensive enablement with MCUXpresso Ecosystem

 

Applications

LPC551x/S1x is suitable for a wide range of applications such as industrial and building automation, consumer products and smart home applications.

Leveraging the integration of a high-speed/high resolution ADC module, the CAN-FD interface, the LPC551x/S1x is suitable for remote IO, sensor nodes, elevator control panel, smart lighting and other industrial and building automation applications.

Due to its rich interface offering such as CAN-FD, HS USB, up to 8 FlexComm interfaces along with its great power efficiency and low-price, this microcontroller is ideal to be deployed in consumer products such as gaming peripherals, tracking systems and power tools.

Its advanced security features make the LPC551x/S1x MCU family the right fit in security systems and in smart home related applications

 

Enablement

Like other NXP MCUs, LPC551x/S1x is fully supported by NXP's MCUXpresso ecosystem, which includes a free downloadable IDE, dedicated SDK package where you could find lots of example codes, and pin configuration tool.

NXP also designed LPCXpresso55S16 development board as the ideal platform for evaluation and development. The board features an on-board LPC-Link2 debug probe based on the LPC4322 MCU for a performance debug experience over high speed USB, with easy firmware update options to support CMSIS-DSP or a special version of J-link LITE from SEGGER.

image

 

Global Launch Webinar

NXP has fulling launched the LPC551x/S1x to the broad market with availability of both sample silicon and the board. Register Now for this Webinar here. In the mean time, if you want to know more about this exciting new product, please visit nxp.com/LPC551x .

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 6 years ago +1
    I have one of these on the way, but I'm mainly interested in investigating a feature you haven't mentioned - the Programmable Logic Unit (PLU). It's a small bit of programmable logic attached to the main…
  • leo_
    leo_ over 6 years ago in reply to Fred27 +1
    Strange...but thank you very much for the notice!
  • leo_
    leo_ over 6 years ago in reply to Fred27

    Strange...but thank you very much for the notice!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago in reply to leo_

    leo_  I can see the webinar is now available, but your links have a missing colon and the https// (no colon) trips thing up.

     

    Corrected links:

    Making Security and Performance Efficiencies Attainable For Your Cost-Conscious Industrial or IoT Application

    which should lead to

    https://register.gotowebinar.com/register/7706444420176748811

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 6 years ago

    I've now got an LPC55S16-EVK board to play with so I shall be delving into the PLU when I have time. I've also got an LPC8N04 but it seems that as NFC was added to the LPC804 the PLU was taken away.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 6 years ago in reply to Fred27

    That is right.

    But  PLU starts from ARM-M0+ LPC804.

    LPC55S69 is top niche balancing price and performance. Features like powerquant, security are unique.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • leo_
    leo_ over 6 years ago in reply to Fred27

    Sorry I was not clear enough here.... the invitation and registration link of the mid May launch webinar will be posted here on the community.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>