Internet of Things
  • Technologies
  • More
Internet of Things
Blog Quadcopter Charge Notifier using Particle Photon
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 2 Jan 2016 10:44 PM Date Created
  • Views 2775 views
  • Likes 8 likes
  • Comments 20 comments
  • particle
  • particle_boards
  • photon
  • iot
  • notification
  • quadcopter
Related
Recommended

Quadcopter Charge Notifier using Particle Photon

fvan
fvan
2 Jan 2016

I received my first quadcopter for Christmas, a XS Nano Quad from Revell. It’s a tiny quadcopter, which I find extremely fun to play with. Unfortunately, the battery lasts only about 5 minutes (3.7V 100mAh) and the charge time is between 30 and 40 minutes.
Because I regularly forget I put it to charge, I decided to make a simple device which can notify me as soon as the battery is fully charged, allowing me to maximise play time!

 

Using a Particle Photon and a photoresistor, changes in light intensity from the charge indicator LED can be measured and used to trigger a notification via the IFTTT service.

imageimage

As usual, all details including code are available on my blog: Quadcopter Charge Notifier using Particle Photon – Frederick Vandenbosch

 

Let me know what you think! What would you use such a notification system for?

  • Sign in to reply

Top Comments

  • gadget.iom
    gadget.iom over 10 years ago +2
    Nice little hack! :)
  • mcb1
    mcb1 over 10 years ago +2
    That's a great non invasive method of checking and notifying. I'm sure it has many other applications, especially for small toys. Mark
  • crjeder
    crjeder over 10 years ago in reply to DAB +2
    That's the same with all rotary wings. The just need a lot of energy to stay in the air. For an example to the more extreme end see this: www.youtube.com/watch You need more batteries to have more fun
Parents
  • mcb1
    mcb1 over 10 years ago

    That's a great non invasive method of checking and notifying.

     

    I'm sure it has many other applications, especially for small toys.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 10 years ago

    That's a great non invasive method of checking and notifying.

     

    I'm sure it has many other applications, especially for small toys.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fvan
    fvan over 10 years ago in reply to mcb1

    This approach could be used with anything having an indicator LED for status. It may not be the best solution, but the goal was, as you said, to be non-invasive.