Internet of Things
  • Technologies
  • More
Internet of Things
Blog Vehicle Simulator Project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 18 Jun 2014 2:57 AM Date Created
  • Views 1751 views
  • Likes 3 likes
  • Comments 3 comments
  • android
  • trip
  • bluetooth
  • obdii
  • cape
  • virtual
  • Black
  • simulation
  • obd2
  • recorder
  • real
  • rtr
  • vtr
  • runner
  • BeagleBone
  • vehicle
  • gps
  • simulator
Related
Recommended

Vehicle Simulator Project

dougw
dougw
18 Jun 2014

blog entry #2

see also Blog #1 Vehicle Simulator - VTR / RTR    and blog #3 Vehicle Simulator Project - update

 

This is an update to the initial blog on a vehicle simulator here:

http://www.element14.com/community/groups/internet-of-things/blog/2014/05/02/vehicle-simulator--vtr-rtr

 

This simulator looks like an operating vehicle to any instrumentation or application that can interface to a normal vehicle via its OBDII connector. The data supplied by the simulator is real trip data collected by the Trip Recorder function of the system. There is additional sensor data available that is collected directly from the Car Cape sensor suite during the same reference trips, such as GPS position, compass heading, accelerations, angular rates, barometric pressure, temperature and ambient light.

The system is built around a Beaglebone Black with a "Car Cape" mounted on it to provide an OBDII interface, a sensor suite, a user interface and a wireless communications interface. The system may be used as either a simulator or as a stand-alone trip recorder.

 

Since the introductory blog, we have been busy designing hardware, ordering parts and building hardware. We have also been setting up a Beaglebone Black development environment and configuring an operating system build and experimenting with CAN bus communications.

 

Status

We have built 3 capes with CAN bus capability and a suite of functionality appropriate for our vehicle applications. The various features are outlined in bullets around the Car Cape image below.

The software and hardware are currently functional enough for 2 Beaglebone Blacks, with installed capes, to communicate over the CAN bus.

Not shown are a separate keypad card and a separate OBDII connector card which also has a DC-DC converter to supply 5 volts the BBBs. These cards are built, but not fully tested yet.

image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 12 years ago +1
    Hi Doug, This has an incredible amount of sensors, GPS, and so on. Probably, people could use it for many purposes even beyond vehicle apps, just use the bits of functionality they need :-) You may have…
Parents
  • mitko369
    mitko369 over 12 years ago

    Agree with Shabaz - so many additional use cases!!!

    Perfect development environment for getting ready for connected cars. People can start using it for experimenting to develop new apps for the upcoming mass market. Early adopters always have higher chance for success image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mitko369
    mitko369 over 12 years ago

    Agree with Shabaz - so many additional use cases!!!

    Perfect development environment for getting ready for connected cars. People can start using it for experimenting to develop new apps for the upcoming mass market. Early adopters always have higher chance for success image