Internet of Things
  • Technologies
  • More
Internet of Things
Blog WeatherBrella - Experiencing Brellazilla
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: zengirl2
  • Date Created: 12 May 2014 12:49 AM Date Created
  • Views 2913 views
  • Likes 1 like
  • Comments 24 comments
  • internet_of_things
  • weather
  • umbrella
  • sparkcore
  • iot
Related
Recommended

WeatherBrella - Experiencing Brellazilla

zengirl2
zengirl2
12 May 2014

image

You may recall that in my last post I described the umbrella business as being rather nasty -- I now have additional support for that theory. The umbrella on the right is the one I received from a company geared to weddings. Their site said returns were impossible and they even declared that they take photos of everything that leaves their warehouse. Well, I guess this little Brellazilla slipped through the cracks. As you can see, the handle is stained, and be glad this is not smellavision. It reeks of cigarette smoke and I can already picture the rainy wedding where this umbrella sat sadly in someone's ashtray. Luckily, once confronted with my photograph, the company immediately decided to take the umbrella back. However, I wasn't willing to risk another purchase with them. I went straight to a company that specializes in umbrellas, and luckily, they carried the same exact brand. I can't tell you how beautiful white looks when it is actually clean and smells fresh (yeah, we all know it is really called off-gassing). Anyway, I'm really excited, not so much by the clean umbrella, but by the screw in its handle.

 

I wanted a screw in the handle so that it would be removable, making it easier to create a new 3D printed version. Well, the screw on this handle turned out to be misleading. Once I removed it, the handle would not budge. "Oh, it's probably just an awesome pressure fit", I thought to myself. Well, it was a little more than that. Apparently, something was blocking one of the side walls. I tried jabbing with various jeweler's tools inside the bottom of the handle, and it was evident that there was some movement, but not enough to release it. I started thinking of how plastics work, and my first thought was that freezing it might help. So, with my husband's help, we put some canned air inside. It did indeed fog up the metal shaft, but still the piece wouldn't budge. Finally, I thought of how I loosen all syrup jar lids -- a hot faucet. In about two minutes, my husband had a tug of war with the handle, and believe me, he is a stocky 6'3", and the umbrella was no match. Finally, an umbrella without a handle! It turns out, when the screw had passed through, it had caused the metal shaft to dimple, and it was just enough to keep it stuck. I'm just glad it worked, because I wasn't sure if I was just going to have to melt it off.

image

So, now I can start to imagine how a circuit might work in this small space. I know the SparkCore will be tiny, but I'm still not sure I can fit a battery with it. If I do get the parts to fit inside, I will have to do a screw cap, much like I did with my previous umbrella project, to allow for access to the battery. It may also make the LED situation tricky. I was hoping to use one NeoPixel to conserve energy. However, for a nice glow it would have to be situated at the top of the handle, probably in the way of the screw cap. A better choice would be to use a small NeoPixel strip in a length of 5 or 6 and wrap it around the inside. Not only would it have a nice glow, but it would also be out of the way of the moving parts. There is one last challenge, and that is the button. If I enlarge the diameter of the handle, I will also have to increase the thickness of the button in order for the umbrella to open. So many tricky details to worry about it, but I still believe something interesting is possible. For now, I'm eagerly awaiting the SparkCore so I can get started on the challenge of coding.

 

 

image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Hi Leslie, You are so good at explaining the "unforeseen" elements of making. Take the handle off an umbrella, how hard could it be! Luckily you have the right level of persistence to go beyond initial…
  • shabaz
    shabaz over 12 years ago in reply to zengirl2 +1
    Hi Leslie, Thanks! : ) The diagram below shows how the Olimex module can be used: I did a similar circuit topology, to make myself a portable 5V/3.3V power supply (basically just replaced the "Sparkcore…
  • shabaz
    shabaz over 12 years ago in reply to zengirl2 +1
    Hi Leslie, I cut out an opening, this is what is looked like end-on: This was the completed thing, I had 0V/5V/3.3V wires, that I could plug into any circuit. With the switch turned on, Ithe power would…
  • zengirl2
    zengirl2 over 12 years ago in reply to shabaz

    That definitely looks like a good choice for your project, and now you have cleared up the mystery about going straight in with wires.  Now I think I need to find out what the boost converter is doing on the battery shield of the SparkCore. I was looking at a similar charging device at SparkFun a month ago that has a boost built in, just in case this was an option. I just don't understand why one would boost the power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to zengirl2

    Hi Leslie,

     

    I cut out an opening, this is what is looked like end-on:

    image

     

    This was the completed thing, I had 0V/5V/3.3V wires, that I could plug into any circuit. With the switch turned on, Ithe power would be turned on to the circuit. With the switch turned off, I could charge the unit (actually I could charge the unit with the switch turned on, but I don't think that is a good idea, it may confuse the charging IC).

    image

    If you have room for the Olimex board, I think it could be a convenient way to save having to make the LiPo removable.

     

    (The olimex board output is just the battery output, i.e. about 3.7V, so if the sparkCore needs 3.3V, then a regulator is needed, the olimex board doesn't contain that).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zengirl2
    zengirl2 over 12 years ago in reply to shabaz

    I was hoping that was the case. So, it looks like you just hard wire the SparkCore and then just plug into USB for recharge. Did you leave an opening in your housing for the USB, or do you just pull your unit out of there for charging?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to zengirl2

    Hi Leslie,

     

    Thanks! : )

    The diagram below shows how the Olimex module can be used:

    image

    I did a similar circuit topology, to make myself a portable 5V/3.3V power supply (basically just replaced the "Sparkcore" in the diagram above with a DC-DC converter to get 5V and 3.3V outputs.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zengirl2
    zengirl2 over 12 years ago in reply to shabaz

    Shabaz,

     

    I like your new monster pic image As for the part, I'm just not picturing how it would work. I get the battery plugged in at the jST, but I don't know how this connects to the SparkCore.  You can tell I've been on the "remove LiPo" bandwagon for too long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>