Internet of Things
  • Technologies
  • More
Internet of Things
Blog WeatherBrella - Experiencing Brellazilla
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: zengirl2
  • Date Created: 12 May 2014 12:49 AM Date Created
  • Views 2920 views
  • Likes 1 like
  • Comments 24 comments
  • internet_of_things
  • weather
  • umbrella
  • sparkcore
  • iot
Related
Recommended

WeatherBrella - Experiencing Brellazilla

zengirl2
zengirl2
12 May 2014

image

You may recall that in my last post I described the umbrella business as being rather nasty -- I now have additional support for that theory. The umbrella on the right is the one I received from a company geared to weddings. Their site said returns were impossible and they even declared that they take photos of everything that leaves their warehouse. Well, I guess this little Brellazilla slipped through the cracks. As you can see, the handle is stained, and be glad this is not smellavision. It reeks of cigarette smoke and I can already picture the rainy wedding where this umbrella sat sadly in someone's ashtray. Luckily, once confronted with my photograph, the company immediately decided to take the umbrella back. However, I wasn't willing to risk another purchase with them. I went straight to a company that specializes in umbrellas, and luckily, they carried the same exact brand. I can't tell you how beautiful white looks when it is actually clean and smells fresh (yeah, we all know it is really called off-gassing). Anyway, I'm really excited, not so much by the clean umbrella, but by the screw in its handle.

 

I wanted a screw in the handle so that it would be removable, making it easier to create a new 3D printed version. Well, the screw on this handle turned out to be misleading. Once I removed it, the handle would not budge. "Oh, it's probably just an awesome pressure fit", I thought to myself. Well, it was a little more than that. Apparently, something was blocking one of the side walls. I tried jabbing with various jeweler's tools inside the bottom of the handle, and it was evident that there was some movement, but not enough to release it. I started thinking of how plastics work, and my first thought was that freezing it might help. So, with my husband's help, we put some canned air inside. It did indeed fog up the metal shaft, but still the piece wouldn't budge. Finally, I thought of how I loosen all syrup jar lids -- a hot faucet. In about two minutes, my husband had a tug of war with the handle, and believe me, he is a stocky 6'3", and the umbrella was no match. Finally, an umbrella without a handle! It turns out, when the screw had passed through, it had caused the metal shaft to dimple, and it was just enough to keep it stuck. I'm just glad it worked, because I wasn't sure if I was just going to have to melt it off.

image

So, now I can start to imagine how a circuit might work in this small space. I know the SparkCore will be tiny, but I'm still not sure I can fit a battery with it. If I do get the parts to fit inside, I will have to do a screw cap, much like I did with my previous umbrella project, to allow for access to the battery. It may also make the LED situation tricky. I was hoping to use one NeoPixel to conserve energy. However, for a nice glow it would have to be situated at the top of the handle, probably in the way of the screw cap. A better choice would be to use a small NeoPixel strip in a length of 5 or 6 and wrap it around the inside. Not only would it have a nice glow, but it would also be out of the way of the moving parts. There is one last challenge, and that is the button. If I enlarge the diameter of the handle, I will also have to increase the thickness of the button in order for the umbrella to open. So many tricky details to worry about it, but I still believe something interesting is possible. For now, I'm eagerly awaiting the SparkCore so I can get started on the challenge of coding.

 

 

image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Hi Leslie, You are so good at explaining the "unforeseen" elements of making. Take the handle off an umbrella, how hard could it be! Luckily you have the right level of persistence to go beyond initial…
  • shabaz
    shabaz over 12 years ago in reply to zengirl2 +1
    Hi Leslie, Thanks! : ) The diagram below shows how the Olimex module can be used: I did a similar circuit topology, to make myself a portable 5V/3.3V power supply (basically just replaced the "Sparkcore…
  • shabaz
    shabaz over 12 years ago in reply to zengirl2 +1
    Hi Leslie, I cut out an opening, this is what is looked like end-on: This was the completed thing, I had 0V/5V/3.3V wires, that I could plug into any circuit. With the switch turned on, Ithe power would…
  • shabaz
    shabaz over 12 years ago in reply to zengirl2

    Hi Leslie,

     

    In this size-optimised design, you may most likely need the external charger as Andy says. If you can find space though, it may be possible to permanently leave the charger in the handle, because this means you don't need to find another JST connector (and they can be stiff usually too, and difficult to plug/unplug frequently).

    I've had good experience with this Olimex charger, it is 30x13mm, maybe it might fit?

    image

    The unpopulated pads that you can see in the photo can be used for the output from the battery, to your circuit. I placed a small switch in series at that point, so that the load could be switched off during charge.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zengirl2
    zengirl2 over 12 years ago in reply to Workshopshed

    Andy,

     

    I've heard that I can help cut down on power usage by playing with the time period of queries to the net. As for batteries, I was hoping to use a LiPo and remove it for recharging.  That's good to know that the SparkCore has a regulator;  I think the only problem is that there won't be a JST connector on the unit. So, I'm definitely going to have to cobble something together. I will take a look at RC stuff to see if they have a good battery fix -- good idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zengirl2
    zengirl2 over 12 years ago in reply to mcb1

    That sounds cool. Sounds like a good use of light effects, as the umbrellas would give the flakes the appearance of gently spinning. Recently the Brooklyn Ballet did some fun costumes with NYC Resistor -- tutus that had snowflakes thanks to Arduino. I've already added dance project to my bucket list.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 12 years ago in reply to zengirl2

    I don't claim to be a wearables expert, but have built quite a few battery driven things over the years. The 3.3v requirement for the SparkCore should be helpful as it should mean more options for batteries. At 100 - 300mA the current draw is quite a lot for batteries so you might want to have some kind of auto switch off or look into if the SparkCore has any low power options to shut bits down and then start them back up as needed.

    If you have a look on radio controlled vehicals or UAV website you might get tips for small light batteries. A Lithium Ion Polymer Battery (LiPO) battery could work which is what the SparkCore site seems to recommend.

    VyOuaYNOTBCkSZ2Ns3TG

    However, you might want to go down the approach of having removable batteries or an external charging circuit and connector to save space. You can connect a battery directly to your SparkCore, it has an onboard regulator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to zengirl2

    Leslie

    I thought of your umbrella last night at a High School Stage challenge.

    They had several umbrellas with white leds attached on the 'wet' side in the shape of a snowflake.

    These were VERY effective and a really cool stage effect.

     

    Sorry no pictures.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>