Internet of Things
  • Technologies
  • More
Internet of Things
Blog World's First General Purpose Cortex-M33 MCU Series Got UPGRADE and EXPANDED
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: leo_
  • Date Created: 13 Nov 2019 4:22 AM Date Created
  • Views 1654 views
  • Likes 4 likes
  • Comments 6 comments
  • Cortex-M
  • nxp microcontrollers
  • nxp semiconductors
  • iot
  • nxp
  • arm
  • lpc
Related
Recommended

World's First General Purpose Cortex-M33 MCU Series Got UPGRADE and EXPANDED

leo_
leo_
13 Nov 2019

As world's first general purpose Arm Cortex-M33 based microcontroller series, NXP's LPC5500 has drawn a lot of audience since initial announcement 1 year ago.

 

LPC55S6x was launchec in Q1 2019 as the first product family in this series. Due to the advanced Cortex-M33 architecture, the first-time introduction of TrustZone into microcontrollers and NXP's advanced security design and PowerQuad core to accelerate calculation, this product has attracted market interest to a large extent.

 

NXP didn't stop developing further based on the initial launch, in fact, it is surprised to see that the LPC55S6x has got an upgrade after only half a year time. Originally the microcontroller runs at 100MHz event though it is already dual qual design, CoreMark has reached 750+. But now NXP offers LPC55S6x full family at 150MHz core frequency, for both the main core and the second core, which makes this product more powerful for various kind of IoT applications.

 

Not only we see the upgrade of the ice breaker, NXP also launches its second family in LPC5500——The LPC552x/S2x family. This product is defined as mainstream Cortex-M33 MCU with the same 40nm NVM process technology as LPC55S6x does. The LPC552x/S2x runs at 150MHz single core and offers high performance efficiency as well. This time you can also choose to have or not have all the security features to maximize the cost efficiency to the largest extent. With the same level of advance design and more streamlined feature set, LPC552x/S2x provides a more cost effective way to develop IoT applications and offers more choices.

 

image

 

Main feature of LPC552x/S2x:

  • Cortex-M33 up to 150 MHz, FPU and MPU
  • Up to 512 KB on-chip flash, 256 KB total
  • Advanced Security: PRINCE module for real-time encryption, CASPER for hardware acceleration, AES-256, SHA2 module, SRAM PUF (LPC55S2x only)
  • FlexComm, USB HS, USB FS
  • 16-bit ADC, ACMP, Temp Sensor
  • 5 x 32b Timers, SCTimer/PWM, RTC, MRT, WWDT
  • Programmable Logic Unit
  • Power-saving modes
  • 1.8V to 3.6V
  • Operating temperature range -40 °C to +105 °C
  • Available in HLQFP100, VFBGA98 and HTQFP64 (Nov 2019) packages

 

 

Check out nxp.com/lpc552x for more information.

  • Sign in to reply

Top Comments

  • phoenixcomm
    phoenixcomm over 6 years ago in reply to clem57 +1
    clem57 Dito, It looks as it will work well with Smarthab
  • clem57
    clem57 over 6 years ago in reply to phoenixcomm +1
    The Eagle has landed
  • noorpuri
    noorpuri over 6 years ago +1
    The unique feature of LPC55S6x is Math accelerator sub system. That make it a competitor to STM32H7.
  • noorpuri
    noorpuri over 6 years ago

    The unique feature of  LPC55S6x is Math accelerator sub system. That make it a competitor to STM32H7.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to phoenixcomm

    The Eagle has landed

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to clem57

    clem57 Good Luck Clem!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago in reply to phoenixcomm

    Well to day is D-Day for the return home...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to clem57

    clem57

    Dito, It looks as it will work well with Smarthab

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>