Internet of Things
  • Technologies
  • More
Internet of Things
Forum udev rules error on BBB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 523 subscribers
  • Views 2505 views
  • Users 0 members are here
Related

udev rules error on BBB

ramanc51
ramanc51 over 10 years ago

Hi all

             In my BBB i written udev rule 99-usb-serial.rules at /etc/udev/rules.d to fix my usb-serial converter ttyUSB0 name as static(e.g printer), but this rules not create symlink as i given below, alos i saw error that unable to open '/sys/udev/ttyUSB0', is there glue to resolve this error?

 

my 99-usb-serial.rules

 

SUBSYSTEMS=="usb-serial", MODE="0666", ATTR{idVendor}=="0403", ATTR{idProduct}=="6001", SYMLINK+="printer"

 

Error

parse_file: reading '/etc/udev/rules.d/99-usb-serial.rules' as rules file

udev_rules_new: rules use 197880 bytes tokens (16490 * 12 bytes), 32369 bytes buffer

udev_rules_new: temporary index used 60680 bytes (3034 * 20 bytes)

unable to open device '/sys/dev/ttyUSB0'

debian@beaglebone:~$

 

Note:

        But i am able to open this device as /dev/ttyUSB0 only by my another java application on same BBB, but not as a printer

  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 10 years ago in reply to ramanc51 +1
    Do you get the error running udevadm test /dev/ttyUSB0 ? Try udevadm test /sys/dev/char/188:0 Are you sure SUBSYSTEMS=="usb-serial" Usually they are "tty" You can also check /var/log/syslog for errors…
Parents
  • mconners
    mconners over 10 years ago

    Did you come up with that by yourself? Or did you have guidance from another source? i.e. did the device vendor provide you with that example and you just added the symlink on the end?

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ramanc51
    ramanc51 over 10 years ago in reply to mconners

    Mike, VID&PID is belongs to my device, by the guidance on other sites that are referenced i came up, for command ls -l /dev/ttyUSB0 i found the device info is stored in /sys/dev/char/188.0, the result for above command is given bellow, are you telling my udev rules is not correct?

     

    crwxrwxrwx 1 root dialout 188,  0  Feb 19 22:39 /dev/ttyUSB0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ramanc51
    ramanc51 over 10 years ago in reply to mconners

    Mike, VID&PID is belongs to my device, by the guidance on other sites that are referenced i came up, for command ls -l /dev/ttyUSB0 i found the device info is stored in /sys/dev/char/188.0, the result for above command is given bellow, are you telling my udev rules is not correct?

     

    crwxrwxrwx 1 root dialout 188,  0  Feb 19 22:39 /dev/ttyUSB0