Internet of Things
  • Technologies
  • More
Internet of Things
Forum udev rules error on BBB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 524 subscribers
  • Views 2501 views
  • Users 0 members are here
Related

udev rules error on BBB

ramanc51
ramanc51 over 10 years ago

Hi all

             In my BBB i written udev rule 99-usb-serial.rules at /etc/udev/rules.d to fix my usb-serial converter ttyUSB0 name as static(e.g printer), but this rules not create symlink as i given below, alos i saw error that unable to open '/sys/udev/ttyUSB0', is there glue to resolve this error?

 

my 99-usb-serial.rules

 

SUBSYSTEMS=="usb-serial", MODE="0666", ATTR{idVendor}=="0403", ATTR{idProduct}=="6001", SYMLINK+="printer"

 

Error

parse_file: reading '/etc/udev/rules.d/99-usb-serial.rules' as rules file

udev_rules_new: rules use 197880 bytes tokens (16490 * 12 bytes), 32369 bytes buffer

udev_rules_new: temporary index used 60680 bytes (3034 * 20 bytes)

unable to open device '/sys/dev/ttyUSB0'

debian@beaglebone:~$

 

Note:

        But i am able to open this device as /dev/ttyUSB0 only by my another java application on same BBB, but not as a printer

  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 10 years ago in reply to ramanc51 +1
    Do you get the error running udevadm test /dev/ttyUSB0 ? Try udevadm test /sys/dev/char/188:0 Are you sure SUBSYSTEMS=="usb-serial" Usually they are "tty" You can also check /var/log/syslog for errors…
Parents
  • ramanc51
    ramanc51 over 10 years ago

    Now i am able to open port using symlink name on my java app by using following line

     

           System.setProperty("gnu.io.rxtx.SerialPorts", "/dev/printer");

     

    But according to rxtx lib source, it will omit other device if we user system property method, so that i can't use more than one device using it's symlink name,

    is there any way to load more than one symlinked devices?

     

    Reference

    Trouble shooting - Rxtx

    If you wish, you can set the system properties gnu.io.rxtx.SerialPorts and gnu.io.rxtx.ParallelPorts. If either of these is set, then no scanning will be carried out and only the specified ports will be available

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to ramanc51

    Have a look at this it may help, it applies to  both RPi and BBB  http://angryelectron.com/rxtx-on-raspbian/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ramanc51
    ramanc51 over 10 years ago in reply to bwelsby

    Thanks Brain, i solved it by adding symlink names with column separated as follows 

     

       System.setProperty("gnu.io.rxtx.SerialPorts", "/dev/Printer:/dev/Display");

             

    but i think we can solve it as follows also by script

     

    java -Dgnu.io.rxtx.SerialPorts=/dev/printer:/dev/dispaly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ramanc51
    ramanc51 over 10 years ago in reply to bwelsby

    Thanks Brain, i solved it by adding symlink names with column separated as follows 

     

       System.setProperty("gnu.io.rxtx.SerialPorts", "/dev/Printer:/dev/Display");

             

    but i think we can solve it as follows also by script

     

    java -Dgnu.io.rxtx.SerialPorts=/dev/printer:/dev/dispaly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • bwelsby
    bwelsby over 10 years ago in reply to ramanc51

    Great,  Yes and I have just found this too in the FAQ - Rxtx

     

    You can specify the available ports by

     System.setProperty("gnu.io.rxtx.SerialPorts", portFileNames); 

    where the file names of the ports are separated by File.pathSeparator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ramanc51
    ramanc51 over 10 years ago in reply to bwelsby

    Brain, now i am facing another issue that, when job get done by my java app, the device is get disconnected and then appeared with new portname e.g ttyUSB1/2 automatically in /dev directory, now  i send command to that device, job is not get done because port is changed my app assign this device with same symlink that correscopnds to another ttyUSB1/2 on startup, if i restart my app then works once then same issue comes, i don't know why this behavior on BBB, my job is to print token using small thermal printer, this thermal printer is interfaced with BBB through USB-Serial converter(Prolific-PL2303), Do you have any idea or clue about this issue?